Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Labels
Top Labels
  • Alphabetical
  • Andover Continuum 2,209
  • TAC Vista 2,045
  • EcoStruxure Building Operation 1,852
  • TAC IA Series 1,825
  • TAC INET 1,459
  • Field Devices 721
  • Satchwell BAS & Sigma 474
  • EcoStruxure Security Expert 334
  • Satchwell MicroNet 252
  • EcoStruxure Building Expert 228
  • EcoStruxure Access Expert 150
  • CCTV 53
  • Project Configuration Tool 47
  • EcoStruxure Building Activate 17
  • EcoStruxure Building Advisor 12
  • ESMI Fire Detection 11
  • Automated Engineering Tool 5
  • EcoStruxure Building Data Platform 3
  • EcoStruxure Workplace Advisor 1
  • EcoStruxure for Retail - IMP 1
  • Previous
  • 1 of 2
  • Next
Top Contributors
  • Product_Support
    Product_Support
  • DavidFisher
    DavidFisher
  • Cody_Failinger
    Cody_Failinger
See More Contributors
Related Products
Thumbnail of EcoStruxure™ Building Operation
Schneider Electric
EcoStruxure™ Building Operation
4
Thumbnail of SmartX IP Controllers
Schneider Electric
SmartX IP Controllers
1
Thumbnail of EcoStruxure™ Building Advisor
Schneider Electric
EcoStruxure™ Building Advisor
1

Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

Building Automation Knowledge Base

Sort by:
Date
  • Date
  • Views
  • Likes
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend
  • « Previous
    • 1
    • 2
    • 3
    • 4
    • 5
    • …
    • 509
  • Next »

EasyLogic and SpaceLogic Controllers & RP-IO Modules as BACnet MS/TP third-party devices

Issue Can the EasyLogic range of controllers & RP-IO Modules work under Building Operation 3.2 as BACnet MS/TP third-party devices  Product Line EcoStruxure Building Operation Environment EasyLogic Controllers, EasyLogic RP-V, EasyLogic RP-C, EasyLogic MP-C EasyLogic RP-IO SpaceLogic Advanced, Pro, and Pro Plus Controllers that support native BACnet MS/TP (via a SpaceLogic RS-485 Adapters.   Standalone BACnet field controller Cause The documentation states that EasyLogic Controllers can be used as a Native BACnet MS/TP device. These devices must be configured using their respective supported Building Operation versions, such as Building Operation 2022 and above. However, there are no guidelines on whether they can be used as a third-party BACnet device, particularly in earlier versions such as Building Operation 3.2.    Resolution EasyLogic controllers can be used as BACnet MS/TP third-party devices in Building Operation 3.2 since the EasyLogic range of RP and MP controllers, and RP-IO I/O modules, natively communicate using the BACnet MS/TP protocol.  This same concept applies when using the devices as true 3rd-party devices (e.g., with Continuum and I/A systems) when older controllers fail, and these EasyLogic controllers are used as temporary replacements before a complete transition.   What MUST be understood before taking this approach is that there is no automatic conversion when migrating the site (and devices) to later Building Operation versions that support these devices natively. After the upgrade, the controller must be deleted from the database and hosted as a native EBO controller.   During this process, some programming may be lost. This risk may be mitigated by creating Custom Types for the application once engineered in Building Operation 2022 (or higher) to future-proof the site for upgrades.  Using the latest firmware for the EasyLogic range of devices is also recommended.     Furthermore, the SpaceLogic Controller Range that supports native BACnet MS/TP (via an RS-485 Adapters) can be configured in the same fashion as described for the EasyLogic range.   Refer to Hardware Overview for further details on each product line. 
View full article
Guinan RobertAndriolo Guinan
‎2023-09-21 12:45 AM

Labels:
  • EcoStruxure Building Operation
2976 Views

Collect EBO Workstation logs

Issue There is a performance issue affecting EBO Workstation and Product Support has requested logs. Product Line EcoStruxure Building Operation Environment Building Operation Workstation Cause Product Support has requested logs from EBO Workstation. Resolution The WorkStation logs and crash dumps are stored in the application data folder. The full path depends on the software installed:   EcoStruxure: %appdata%\Schneider Electric EcoStruxure\Building Operation\WorkStation\Logs %appdata%\Schneider Electric EcoStruxure\Building Operation\WorkStation\Crashes   StruxureWare: %appdata%\Schneider Electric StruxureWare\Building Operation\WorkStation\Logs %appdata%\Schneider Electric StruxureWare\Building Operation\WorkStation\Crashes     All files from the Logs folder starting with CoreLog or CrashLog must be included. All files from the Crashes folder must be included.   Perform the following to quickly access the appropriate folder above: Select link Paste into Windows Explorer Address Bar  If you can replicate an issue, perform this process to Temporarily Raise the Log Level before running the test and collecting the logs. Log in to WorkStation Click the Tools menu Click Options Hold down the left SHIFT key on the keyboard Click Apply Release the left SHIFT key on the keyboard and click OK to close the dialog The WorkStation log level is now set to INFO and will collect additional information Please note the logging level will remain at INFO while logging out and in.  To return the workstation log level to default close the Workstation and re-open.
View full article
Picard David_Purser Picard
‎2022-08-18 09:37 PM

Last Updated: Sisko GavinHe Sisko ‎2025-05-19 07:27 AM

Labels:
  • EcoStruxure Building Operation
1759 Views

Jace 9000 and NRIO Failures

Issue This issue is described in Tridium's internal case NCCB-71360. Users will notice that the default Nrio Device Manager view (Ux/web media) of the NrioNetwork driver in N4.14 looks identical to the previously existing workbench AX view; however, due to this defect, devices discovered and added through the web view will not function as expected.  Product Line TAC IA Series Environment I/A Series N4 Jace 9000 I/A Series N4.14 Framework Version Cause With the release of the Jace 9000, users may notice that the IO-R-16 and IO-R-34 devices will not function properly when discovery and configuration are performed through the web views. Resolution To tell if the device was added through the correct view, there are a few indicators. Malfunctioning devices will not show up with an Installed Version or a Sec version in either view: Working devices will display these values with no issue in either view: The malfunctioning devices' health section will read 'fail' even with a status of ok: Users in N4.14 should only use the Workbench AX Nrio Device Manager view to discover and add devices to a station. This use case is currently not supported in the browser for N4.14. All other use cases function in the UX Web Views, such as viewing devices, adding points, and commanding points.  
View full article
Guinan RandyDavis Guinan
‎2025-05-15 05:07 PM

on ‎2025-05-15 05:07 PM

Labels:
  • TAC IA Series
290 Views

System Limitations of Flex Server

  Issue This document gives guidelines on the device constraints that effect the system capabilities or the system limitations of the Flex Server.  Product Line EcoStruxure Building Activate Environment EcoStruxure Building Activate Flex Server EcoStruxure Building Activate Partner Portal Cause Understanding this document helps in efficiently designing architecture and Single line Diagrams. Identifying potential bottlenecks in a system allows for preemptive action. If you know a system parameter has limited device capacity, you can optimize the distribution methods or plan for upgrades before it becomes a critical issue. Understanding the limitations of system allows for the implementation of backup measures. Resolution Thes guidelines provide the recommended Flex Server design limits for common applications. These are the configurations that have been tested and supported by Schneider Electric. Environmental factors such as network traffic and radio interference may reduce the stated limits of these guidelines. Deviations from these guidelines may result in performance related issues or product failures.   Flex Server Capacity Parameter Maximum Number Number of total devices (all protocols combined) 50 Number of controlled points (all protocols combined) 500   BACnet Parameter Maximum Number Number of BACnet MSTP devices per RS485 port 32 a b e Number of BACnet MSTP networks per server 2 c Number of BACnet IP devices 50 d e   a. Maximum number of devices according to protocol specifications and guidelines. b. BACnet MS/TP adheres to RS485 rules for wiring, wire type, termination etc. c. There is one onboard RS485 port, an additional port can be added via USB. d. BACnet IP uses default UDP port 47808 (0xBAC0). e. The total number of devices across all protocols must not exceed 50   Modbus Parameter Maximum Number Number of Modbus RTU devices per RS485 port 32 a b e Number of Modbus RTU networks per server 2 c Number of Modbus TCP devices 50 d e   a. Maximum number of devices according to protocol specifications and guidelines. b. Modbus RTU adheres to RS485 rules for wiring, wire type, termination etc. c. There is one onboard RS485 port, an additional port can be added via USB. d. Modbus TCP uses default TCP port 502. e. The total number of devices across all protocols must not exceed 50   LoRa a Parameter Maximum Number Number of LoRa sensors per server 32 b c d Maximum number of messages per day (per server) 100   a. LoRa distances – LoRa is noted for its long range and deep penetration. LoRa transmissions can penetrate glass, metal and concrete found in most buildings. The radio’s antenna and installation can affect the range of LoRa sensors. You must test the transmission and signal strength, when installing wireless devices. b. Maximum number of devices according to protocol specifications and guidelines. c. Every LoRaWAN sensor manufacturer has their own decoder. d. The total number of devices across all protocols must not exceed 50   SNMP Parameter Maximum Number Number of SNMP devices 10 a Maximum number of messages per day (per server) 1024   a. The total number of devices across all protocols must not exceed 50   Object Limits Object Type Maximum Number Analog values 500 a Digital values 500 a Multi-state values 500 a Analog Input 500 a Multi-state input 500 a Analog output 500 a Digital output 500 a Multi-state output 500 a   a. The total number of combined points must not exceed 500
View full article
pranavkumar003 Cadet
‎2025-05-15 12:23 AM

Last Updated: Administrator CraigEl Administrator ‎2025-05-15 12:30 AM

Labels:
  • EcoStruxure Building Activate
257 Views

EBO SQL Extended Log Storage connection fail with alarm "Login failed for user"

Issue After correctly following the process outlined in Setup External Log Storage using MSSQL., EcoStruxure Building Operation (EBO) server fails to connect to the external database, generating the following System Alarms:  Unable to connect to data source Login failed for user The system alarm specifically details an issue with the ODBC SQL Driver as below: "The driver doesn't support the version of ODBC behavior that the application requested..." "Invalid connection string attribute" Product Line EcoStruxure Building Operation Environment Building Operation Enterprise Server Building Operation Enterprise Central Building Operation Automation Server Premium (AS-P) External Log Storage [MSSQL]  Cause The system alarm details indicate an issue with the ODBC SQL Driver, specifically: "The driver doesn't support the version of ODBC behavior that the application requested..." "Invalid connection string attribute" This suggests a compatibility or configuration issue with the ODBC driver or connection string.   Resolution The following has been seen to correct the issue: Verify User Credentials Ensure that the username and password used for the ODBC connection are correct. Note: SQL Server credentials are case-sensitive, so double-check for any discrepancies in letter casing. Remove any uppercase for the username. In some cases, using only lowercase letters for the username in the ODBC connection string has resolved the issue, e.g,. Instead of "My_User" use "myuser"
View full article
Commander Hernan_Urueña Commander
‎2025-05-14 10:39 PM

Last Updated: Guinan RobertAndriolo Guinan ‎2025-05-14 10:40 PM

Labels:
  • EcoStruxure Building Operation
229 Views

Embedded license activation failed - Device ID included in the banned list

Issue Cannot activate a license on an Automation Server although the entitlement works on other Automation Servers. The Device Administrator output is similar to the following:   Activate failed: ASEmbeddedAPI internal error: Binary response does not contain feature information Error status information: FNO server response: =V(BACK_OFFICE%DEBACK_OFFICE+]\fK%MDEVICEID|0}~;DEVICEID/jlSk\}K qq7!vi%DCH'~A%05pQWN]G|3^Jk+yaz_Kx/:Dy&w F7BWWN#`Ex|6S.d<Y^nV~@?*C.D0])"KO?[pS#GH|aMe+i|@4's9kNE\7gfocfVbRf$1VuH>sdp_JN6%4B.n|Zm$]wi9M|F8#Hrw~/L4%XU<?8o="P1S$uW6Fu5vAsAz|l>8.@XA|.'[v_ekh_P}c7 Product Line EcoStruxure Building Operation Environment Building Operation Automation Server Premium (AS-P) Building Operation Automation Server Bundled (AS-B) Building Operation Automation Server (AS) Cause When an Automation Server fails in the field an RMA (Return Material Authorization) request is made, and the license is returned for re-use in the replacement Automation Server. Once this occurs the serial number of the faulty Automation Server is blacklisted to ensure that it cannot be licensed and reused. Resolution If the device was mistakenly added to the blacklist please supply the Automation Server serial number to Support. If an RMA number does not exist in the licensing system for this Automation Server, the support team can make a request to have the server removed from the blacklist.
View full article
Commander Hernan_Urueña Commander
‎2025-05-14 07:42 AM

Last Updated: Administrator CraigEl Administrator ‎2025-05-14 04:06 PM

Labels:
  • EcoStruxure Building Operation
346 Views

Collect log files from Project Configuration Tool 2.0 (PCT 2.0)

Issue How to collect log files from the Project Configuration tool 2.0. Product Line EcoStruxure Building Operation Environment Project Configuration Tool Cause When contacting Product Support about issues with the PCT, log files should be provided. Resolution Collect log files through the Web interface on both Windows and Ubuntu installations: Logon to PCT server, Click Diagnostic  Click Collect logs Log starts collecting. After the log collection process is complete, the file will either be saved to the browser's default download location or a window will pop up asking where to save the ZIP file. Select the desired location then click Save   Log collector tool for PCT for Ubuntu: If the PCT web interface is unavailable, you can use the Log Collector tool to gather log files. This tool is included with the PCT installation on Ubuntu, eg. pct-2.1.1.8-log-collector-ubuntu. Give the file proper permission to be able to run as an executable either using chmod command:  chmod +x pct-2.1.1.8-log-collector-ubuntu​ or via file properties, as shown in below screenshot: Run the log collector tool. ./pct-2.1.1.8-log-collector-ubuntu​ A zip file containing the required log files will be saved in the same folder where the log collector tool is located.
View full article
Admiral StephenYang Admiral
‎2025-05-12 08:12 AM

Last Updated: Kirk Mahmoud_Sayed Kirk ‎2025-05-14 07:21 AM

Labels:
  • EcoStruxure Building Operation
  • Project Configuration Tool
363 Views

Configuration steps for Elsys LoRaWAN sensors with a Smartphone using NFC

Warning Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices. Potential for Data Loss: The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure or unfamiliar with any complex steps detailed in this article, please contact Product Support for assistance. Issue How are Elsys LoRaWAN sensors configured with a smartphone using NFC Product Line EcoStruxure Building Activate Environment EcoStruxure Building Activate Flex Server EcoStruxure Building Activate Partner Portal Cause All Elsys sensors are equipped with NFC for easy configuration with a smartphone. There is a requirement to configure these sensors using a Smartphone or tablet using Elsys 'Sensor Settings' application. Resolution Download the ELSYS “Sensor Settings” application from Google Play or the IOS App store and install it on a smartphone or tablet.     Ensure the mobile device supports NFC. Enable NFC on the device and start the application. Position the mobile device directly on the NFC antenna of the sensor. Ensure both devices remain close and stationary to maintain optimal connectivity. Remove the mobile device. The current settings will be displayed in the application. Set the 'Timebase' to 120 seconds using the application. Remember to revert it to 600 seconds after commissioning!    Make note of the following sensor keys: DevEUI: The unique ID of the sensor, found in the blue panel at the top. AppEUI: Application ID (8 bytes or 16 hex digits). Default is 0, can be changed if needed for the application. AppKey: Application unique key (16 bytes or 32 hex digits) that is the encryption key used for messages during every over-the-air activation. Tap the sensor's NFC antenna to transfer the new settings after making the desired changes. Ensure the application confirms the updated settings. Wait for the sensor to reboot, indicated by the LED flashing. The sensor settings should now be updated. Validate your settings by reading the NFC data after the sensor has restarted. Verify that settings have been applied by using the ‘Read’ functionality in the app and touching the sensor’s NFC antenna.    Remember to change the 'Timebase' back to 600 seconds after the commissioning is completed!
View full article
Ensign Mukesh_Sangwan Ensign
‎2025-05-13 03:53 PM

on ‎2025-05-13 03:53 PM

Labels:
  • EcoStruxure Building Activate
244 Views

Different options for EBO to serve data to 3rd party systems

Issue How can EcoStruxure BMS server serve data to external devices or software? Product Line EcoStruxure Building Operation Environment Building Operation Enterprise Server Building Operation Enterprise Central Building Operation Automation Server Building Operation Automation Server Premium Building Operation Automation Server Bundled Building Operation Edge Server - Standard Third party devices or software Cause The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management. In many projects, it is required that an EcoStruxure BMS server serve data to external devices or software, E.X. HMI, SCADA or power monitoring. Resolution The following is a summary of the available options to serve EcoStruxure BMS server data to the external world: BACnet:  When you create a BACnet Interface, the system automatically creates the Application and IP network folders within the BACnet Interface folder on the System Tree. If you create a BACnet Interface for a SmartX server, you can optionally create an MS/TP network. You can create BACnet objects in BACnet application folder of EcoStruxure BMS servers and these object will be visible for external BACnet clients. More information about EBO BACnet interface: BACnet Interface   Modbus Slave network:  If you configure the Modbus Slave Network (and associate it with a serial port), you can set up any external Modbus master device to communicate with the internal Modbus Interface. In this example, a Modbus Slave Network is set up on an EcoStruxure BMS Server and the external master device is configured with the same Modbus properties as the Modbus Slave Network object. The Modbus master device can also be an HMI device. More information about Modbus serial interface: Modbus Serial Networks Modbus server network: You can create a Modbus TCP Network on an Ethernet network (TCP/IP).  You can create an internal interface which acts as the server to an external client/clients. More information about Modbus TCP interface: Client and Server Networks   MQTT: MQTT is a lightweight and flexible data transfer protocol for IoT resources. EcoStruxure Building Operation, V3.2 or higher, can be configured to send data to an MQTT broker on interval or event-driven. The below are the tested brokers: Microsoft Azure IoT Hub Amazon IoT Core IBM Watson IoT Mosquitto More information about MQTT interface: MQTT Overview LonWorks Interface: EcoStruxure BMS servers can have a local node on their networks that can act as a LonWorks node. In the local node, you can create your own NVs that can be bound to external LonWorks devices using LonWorks bindings. The NVs in your local node can then be used in EcoStruxure Building Operation bindings for applications and graphics. More information about LonWorks interface: LonWorks Engineering   SNMP: Simple Network Management Protocol (SNMP) is an Internet-standard protocol for managing devices on IP networks. The EcoStruxure BMS servers support SNMP version 3. The SmartX servers support several SNMP traps. SNMP traps enable an agent to notify the management station of significant events by way of an unsolicited SNMP message. More information about SNMP: SNMP EcoStruxure Web Service (EWS) server: EcoStruxure Web Services allows seamless sharing of operational data, including alarms and historical information, between software from different Schneider Electric Business Units. When the EcoStruxure BMS server is an EcoStruxure Web Service server, it exposes objects, such as values, to another EcoStruxure system that is an EcoStruxure Web Service client. The EcoStruxure Web Service client can read and change values on the EcoStruxure BMS depending on the configuration of the EcoStruxure BMS server. More information about EBO EWS Server: EcoStruxure Web Service Server Smart Connector: A development framework that simplifies and accelerates integrations with third-party systems or other data sources. It is an open, extensible and configurable application framework that allows developers to create innovative new capabilities, applications, and solutions which extend and enhance EcoStruxure Building solutions. Ex. SmartConnector can be used to serve EBO data in a RESTful manner, refer to: Configure SmartConnector RESTful EWS Gateway to serve EBO data   For further information watch the Smart Connector explainer video or visit the Smart Connector Developer Community on the Exchange: For developers wanting to get started using the Smart Connector framework visit: https://www.smartconnectorserver.com Smart Connector at Exchange:  EcoStruxure Building Operations SmartConnector 
View full article
Kirk Mahmoud_Sayed Kirk
‎2021-12-12 05:42 PM

Last Updated: Admiral StephenYang Admiral ‎2025-05-13 02:01 PM

Labels:
  • EcoStruxure Building Operation
7027 Views

Upgrading SBO 1.x or EBO 2.x licenses to EBO 2022 v4 or later

Issue Licenses required to upgrade SBO/EBO to EBO 2022 v4.0.x Product Line EcoStruxure Building Operation Environment Building Operation Automation Server Premium - Secure boot Building Operation Automation Server Premium Building Operation Automation Server Bundled Building Operation Enterprise Server Cause Clarifying licensing upgrade requirements for EBO 2022 v4.0.x Resolution Example: Upgrading a site SBO 1.x or EBO 2.x to EBO 2022 v4.0.x or later directly. Site has an Enterprise Server (ES) the ES has 7x Automation servers AS-Ps and 2x AS-Bs attached. One AS-P has a Modbus interface, and 1 AS-B has a Modbus interface. Adding 1 additional AS-P classic (non-secure boot), 1x AS-P-S secure boot and 1 AS-B scalable. The SBO 1.x or EBO 2.x licenses need to be upgraded to EBO 3.x first. Upgrade ES licensing from SBO 1.x license to EBO 3.x.  These licenses need to be activated using License Administrator.   1 x SXWSWESUP13010 ES Upgrade from 1.X to 3.0 with 10 or less AS  Note: Upgrading ES from 1.x gives the ability to host the maximum quantity of field devices / controllers at the Enterprise Server (600). Also, when a system is upgraded from 1.x, it will be provided with an unlimited (bounded by the maximums stated in the Architectural Guidelines) client license for connections to the Enterprise Server that has been upgraded.   The following additional licenses are required for each AS-x when upgrading a site from SBO 1.x to EBO 3.x or upgrading a site from EBO 2.x that was originally installed at SBO 1.x and upgraded to EBO 2.x. These are not required if the site was originally installed at EBO 2.0 and upgrading to EBO 3.x. These licenses need to be activated using License Administrator.   7 x SXWSWASUP00001 license will be required one for each AS-P. 2 x SXWSWASUP00001 licenses will be required one for each AS-B.   Note: If the site has more than 24 AS-xs then part number SXWSWASUP00099 provides 999 licenses. EBO 3.2.x architectural guidelines allows a maximum of 250 AS-xs per ES.   Upgrade ES license from EBO 3 to EBO 4 This license needs to be activated using License Administrator.   1 x SXWSWESUP30010 ES Upgrade from 3.X to EBO 2022 or later (i.e. to the current EBO version) with 10 or less AS Upgrade AS-P/B licensing from EBO 3 to EBO 4 or later These licenses need to be activated using Device Administrator.   For each AS-P (non secure boot AS-P and AS-P-NL), one of the following bundles would be required for each AS-P.   SXWSWASPUP30SA Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Standalone SXWSWASPUP30SD Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Standard SXWSWASPUP30EN Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle - Enhanced SXWSWASPUP30FU Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Full SXWSWASPUP30BP Full Bulk pack for upgrading AS-P-XX from EBO 3.x to EBO 2022 or later, contains 125 pieces of SXWSWASPUP30FU. For the AS-P with the Modbus interface, an SXWSWX000MBRTU license is not needed as Modbus is grand-fathered for AS-P classics.   Note: Once an AS-P license is upgraded, there is no differentiation between AS-P Secure Boot and AS-P Non-Secure Boot (Classic):   If the “SXWSWASPUP30SD Upgrades an AS-P from EBO 3.x to EBO 2022 or later AS-P Bundle – Standard” license was purchased for an AS-P classic, and later it requires an enhanced or full license.   SXWSWXUP00SDEN ASP Bundle upgrade - Standard to Enhanced SXWSWXUP00SDFU ASP Bundle upgrade - Standard to Full Would need to be purchased.   If the “SXWSWASPUP30EN Upgrades an AS-P from EBO 3.x to EBO 2022 or later AS-P Bundle – Enhanced” license was purchased for an AS-P classic, and later it requires an  full license. SXWSWXUP00ENFU ASP Bundle upgrade - Enhanced to Full Would need to be purchased.   For the AS-Bs (AS-B-24, AS-B-24H, AS-B-36, and AS-B-36H), one of the following bundles would be required for each AS-B. These licenses need to be activated using Device Administrator.   SXWSWASBUP30SD Upgrades AS-B from EBO 3.x to EBO 2022 or later AS-B Bundle – Standard SXWSWASBUP30FU Upgrades AS-B from EBO 3.x to EBO 2022 or later AS-B Bundle - Full A SXWSWX000MBRTU Modbus license is not needed with AS-Bs Note: Once an AS-B license is upgraded, there is no differentiation between AS-B Scalable and AS-B (L) Non-Scalable (Classic): If the “SXWSWASBUP30SD Upgrades AS-B from EBO 3.x to EBO 2022 AS-B Bundle – Standard” license was purchased for an AS-B (L) classic, and later it requires a full license.   SXWSWXBBUPSDFU ASB Bundle upgrade - Standard to Full, would need to be purchased.   To upgrade the AS-B-L (classic) type, the SXWSWASBUP30SD ASB Upgrade – Standard license is all that is required.   For the additional AS-P classic one of the following licenses would be required. SXWSWASPUP30SA Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Standalone SXWSWASPUP30SD Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Standard SXWSWASPUP30EN Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle - Enhanced SXWSWASPUP30FU Upgrades AS-P-XX from EBO 3.x to EBO 2022 or later AS-P Bundle – Full For the AS-P with the Modbus interface, an SXWSWX000MBRTU license is not needed as Modbus is grand-fathered for AS-P classics.   For the additional AS-P secure boot one of the following licenses would be required. SXWSWXBU0000SA ASP Bundle - Standalone  SXWSWXBU0000SD ASP Bundle – Standard  SXWSWXBU0000EN ASP Bundle – Enhanced  SXWSWXBU0000FU ASP Bundle - Full  For the AS-P secure boot if a Modbus interface is to be used the SXWSWX000MBRTU Modbus license would be required. For the additional AS-B Scalable one of the following licenses would be required. SXWSWXBBU010SD ASB Bundle – Standard SXWSWXBBU050FU ASB Bundle – Full A SXWSWX000MBRTU Modbus license is not needed with AS-B scalable. If an additional AS-B classic was added one of the following licenses would be required. SXWSWASBUP30SD Upgrades AS-B from EBO 3.x to EBO 2022 or later AS-B Bundle – Standard SXWSWASBUP30FU Upgrades AS-B from EBO 3.x to EBO 2022 or later AS-B Bundle - Full A SXWSWX000MBRTU Modbus license is not needed with AS-Bs     Addition: If the site had an Enterprise Central (EC) at EBO 2.0 and was upgrading to EBO 2022 v4.0.x or later, one of the following licenses would be required to upgrade to EBO 3.x first:   SXWSWECUP23005 EC Upgrade with 5 or less ES SXWSWECUP23010 EC Upgrade with 10 or less ES Then one of the following licenses would be require to upgrade from EBO 3.x to EBO 2022 v4.0.x or later:   SXWSWECUP30005 EC Upgrade from 3.x - with 5 or less ES SXWSWECUP30010 EC Upgrade from 3.x - with 10 or less ES   For more information on the bundles, search for 'software bundles" in the  “Part Numbers and Hardware/Software User Matrix – EBO 2024”   For information on software and features that require licenses  
View full article
Gary Schneider Alumni (Retired)
‎2022-02-17 09:16 AM

Last Updated: Kirk Mahmoud_Sayed Kirk ‎2025-05-12 05:49 AM

Labels:
  • EcoStruxure Building Operation
12800 Views

Currently Supported SIM Cards in the Flex Server

Warning Hazard of Electric Shock: Remove all power from all devices before removing any covers or doors of the system. Disconnect power at the device and at the power source. Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices. Caution While removing gateway cover: Open the gateway screws and delicately remove the top cover. Take extra care during this step, as the top cover is connected to the antenna cable via a thin wire. After opening the top cover, you will be able to see the top view of the board, please insert the active SIM card in the designated slot. Once the Sim Card is properly inserted, fix the screws back and ensure that the 4G&Wi-Fi Antenna is attached properly. If the antenna cable remains disconnected from the board, then the GSM will not work.   Important Note: The SIM must not have a Username, Password, or PIN. These features are not supported. Refer to Steps to follow to unlock SIM PIN when using SIM Card under Flex server The user must ensure that no firewall is applied by the SIM provider. If a firewall exists, it may block connectivity. We recommend using SIMs without any firewall restrictions. Ensure the data plan of the SIM should not be less than 2GB per month for approximately 100-200 streams. Issue This article provides information on the SIM cards that are currently supported in EcoStruxure Building Activate and are added to the central database to support field deployment of Flex servers. Product Line EcoStruxure Building Activate Environment EcoStruxure Building Activate Flex Server EcoStruxure Building Activate Partner Portal Cause This eliminates the need for manual support for the already validated SIM operators individually on each server. Resolution Below is the list of the Network Service Providers whose APN exists in the backend and have already been added: MCC code (Country Code) Operator APN 260 play {"generic": "internet"} 260 plus {"generic": "mbb.mobi-data.com"} 732 claro {"generic": "internet.comcel.com.co"} 454 smc hk {"generic": "Smartone"} 520 ais {"generic": "internet"} 240 tele2 se {"generic": "mbb.mobi-data.com"} 260 t-mobile {"generic": "internet"} 262 t-mobile {"generic": "internet.v6.telekom"} 505 telstra {"generic": "telstra.internet"} 204 nl kpn {"generic": "matooma.m2m"} 208 208 28 {"generic": "datapro"} 234 voda uk {"generic": "wap.vodafone.co.uk"} 901 901 40 {"generic": "internet.m2mportal.de"} 208 free {"generic": "free"} 208 bouygues telecom {"generic": "mmsbouygtel.com"} 208 sfr {"generic": "sl2sfr"} 208 orange {"generic": "orange"} 268 vodafone {"generic": "internet.vodafone.pt"} 268 nos {"generic": "umts"} 405 vi india {"iot": "IOT.ZENATIX.COM"} 404 vi india {"iot": "IOT.ZENATIX.COM"} 405 ind airtel {"iot": "iot.com"} 404 ind airtel {"iot": "iot.com"} 724 tim internet {"generic": "timbrasil.br"} 724 vivo {"iot": "smart.m2m.vivo.com.br", "generic": "zap.vivo.com.br"} 724 claro {"generic": "claro.com.br"} 310 at&t {"iot": "armstrongdynm.com.attz", "generic": "NXTGENPHONE"} 440 fl1 {"generic": "soracom.io"} 302 bell {"generic": "mnet.bell.ca.ioe"} 302 rogers {"generic": "M2Minternet.apn"} 302 at&t {"iot": "armstrongdynm.com.attz", "generic": "NXTGENPHONE"} 404 idea {"generic": "Internet"} 431 etisalat {"generic": "mnet"} 430 etisalat {"generic": "mnet"} 424 etisalat {"generic": "mnet"} 424 du {"generic": "du"} 405 404 11 {"iot": "IOT.ZENATIX.COM"} 405 vodafone {"iot": "IOT.ZENATIX.COM"} 405 airtel {"iot": "iot.com"} 404 airtel {"iot": "iot.com"} 404 vodafone {"iot": "IOT.ZENATIX.COM"} 404 404 11 {"iot": "IOT.ZENATIX.COM"} 404 jio {"generic": "jionet"} 405 jio {"generic": "jionet"} Additional Information Ensure the SIM card is active and properly inserted. Verify the antenna cable is securely connected to the board. Confirm the SIM card has no firewall restrictions and meets the data plan requirements.  
View full article
pranavkumar003 Cadet
‎2025-05-12 04:59 AM

on ‎2025-05-12 04:59 AM

Labels:
  • EcoStruxure Building Activate
255 Views

Steps to follow to unlock SIM PIN when using SIM Card under Flex server

Warning Hazard of Electric Shock: Remove all power from all devices before removing any covers or doors of the system. Disconnect power at the device and at the power source. Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices. Caution While removing gateway cover: Open the gateway screws and delicately remove the top cover. Take extra care during this step, as the top cover is connected to the antenna cable via a thin wire. After opening the top cover, you will be able to see the top view of the board, please insert the active SIM card in the designated slot. Once the Sim Card is properly inserted, fix the screws back and ensure that the 4G&Wi-Fi Antenna is attached properly. If the antenna cable remains disconnected from the board, then the GSM will not work. Issue SIM card not being detected and internet is not connecting automatically when SIM card is inserted inside the Gateway.   Product Line EcoStruxure Building Activate Environment EcoStruxure Building Activate Flex Server EcoStruxure Building Activate Partner Portal Cause Some network service providers have a username, password and SIM PIN set by default when they issue the SIM to the customer. If the Gateway is using the SIM for internet, it requires any username, password and SIM PIN to be disabled before inserting the SIM inside the Gateway.  Resolution Contact the Network service provider directly to disable the username and password. The Network service provider can disable the username and password from the backend. For disabling the SIM PIN follow the below procedure: Steps to follow to unlock SIM PIN An example YouTube video on the steps detailed below can be seen at: How to unlock your SIM Card Upon receiving the SIM kit (note down the PUK number and also note down the SIM PIN if available) Insert the SIM card to a Mobile device/cellular device Type in the SIM PIN from the Step 1 and Unlock the SIM Navigate to the settings page – Network section - SIM settings - SIM PIN - Disable the SIM PIN option SIM CARD SETTINGS           SIM PIN DISABLED Reconfirm if the SIM PIN is disabled by reinserting the SIM from the SIM tray and check if it asks for PIN. If the SIM PIN is successfully disabled, it will not ask for SIM PIN at startup. If it still asks, repeat Step 4. Insert the SIM inside the Gateway SIM Slot and check for network connectivity and that the gateway goes online. After inserting the SIM card properly, power up the gateway and allow the gateway to boot up. This process may take up to 5 minutes. Once completed, the device should come online and can be provisioned through a partner portal   In case the SIM PIN is unavailable An example YouTube video on the steps detailed below can be seen at: How to Unlock Sim Card / Sim locked by Pin Code or PUK Code  Insert the SIM card into a Mobile device/cellular device Type in incorrect PIN more than 4 times till it asks to enter PUK code. Contact the Network Service Provider and perform the verification and obtain the PUK Code for the SIM from the Network provider directly Type the PUK code into the mobile device in the PUK code page Navigate to the Network settings - SIM PIN - Set a SIM PIN inside the settings Use this SIM PIN to Disable the SIM PIN lock. Reconfirm that the SIM PIN is disabled by reinserting the SIM from the SIM tray and check that it does not request a PIN.
View full article
pranavkumar003 Cadet
‎2025-05-12 12:49 AM

on ‎2025-05-12 12:49 AM

Labels:
  • EcoStruxure Building Activate
349 Views

Change Set Error

Issue The "Change set error" occurs after trying to save a LonWorks network variable binding in SmartStruxure. Product Line> EcoStruxure Building Operation Environment Workstation LonWorks Network Cause The LonWorks bindings have become corrupt and need to be rebuilt. Resolution Rebuild LonWorks Bindings Right click on the LonWorks Network. Go to Advanced > Rebuild LonWorks Bindings. Select Yes.
View full article
Picard Product_Support
‎2018-09-11 07:27 AM

Last Updated: Administrator CraigEl Administrator ‎2025-05-11 04:47 PM

Labels:
  • EcoStruxure Building Operation
1554 Views

Error activating a license using entitlement id.

Issue Attempting to add a Building Operation ES license using the entitlement ID results in an error indicating that the server cannot be contacted. Product Line EcoStruxure Building Operation Environment Building Operation License Administrator Building Operation Device Administrator Cause The ES computer does not have an Internet connection Resolution To activate a license using an entitlement ID, an Internet connection is required to validate with the Schneider Electric main license server. Follow these steps: Ensure Internet Connectivity: Verify that the ES computer has a stable Internet connection. Refer to Documentation: Consult the following resources for detailed instructions: How to activate, release and/or transfer a license in EcoStruxure Building Operation License server and port used to reach Building Operation licensing server Additional Information: For further assistance, visit the Schneider Electric Building Automation Knowledge Base or contact support.  
View full article
Picard Product_Support
‎2018-09-06 12:22 PM

Last Updated: Administrator CraigEl Administrator ‎2025-05-09 05:42 PM

Labels:
  • Andover Continuum
1946 Views

License server and port used to reach Building Operation licensing server

Issue Firewall issues when trying to reach out to the activation server for a license Product Line EcoStruxure Building Operation, Satchwell Sigma, TAC Vista Environment Building Operation Licensing Firewall Cause If the corporate network has a very restricted firewall policy or rules, the port needed to reach and activate a license may be blocked. Note: The same license server is used for EcoStruxure Building Operation, Satchwell Sigma and TAC Vista software licenses. Resolution Open Port 443 (HTTPS) for the server hosting the license server, and ensure that the routing paths to the Flexnet Licensing server URL's are all fully open. The Licensing Server URL should be opened from the site, and it is:  https://schneider-electric.flexnetoperations.com ocsp.r2m02.amazontrust.com Ocsp.r2m02.amazontrust.com Ocsp.rootca1.amazontrust.com If the site of the old server has issues with non-secure communications or communications forwarding between the previous and the new server, a tool is available to configure EBO to only use the new server. See the Exchange Community article for the download: SBO License Setup Note: From EBO V2.0 only the new license server is used, port 80 is no longer required and HTTP is redirected to HTTPS.
View full article
Picard Product_Support
‎2021-02-17 02:51 AM

Last Updated: Administrator CraigEl Administrator ‎2025-05-09 05:32 PM

Labels:
  • EcoStruxure Building Operation
  • Satchwell BAS & Sigma
  • TAC Vista
11990 Views

License activation stops at 80% or License Administrator crash

Issue Two related issues are covered in this article While attempting to activate a customer or demo license, the activation process stops at around 80%. When clicking the "Diagnostics" tab in the License Administrator it crashes with a "System.DllNotFoundException" error. System.DllNotFoundException: Unable to load DLL (Tac.Nsp.Archive.Licensing.Client.dll) Product Line EcoStruxure Building Operation Environment First detected in Windows 10 First detected with Microsoft Visual C++ Redistributable 2012 (VC++ 2012) License Administrator Cause There can be two reasons why this happens If the activation process stops at around 80%, but the License Administrator does not crash when the "Diagnostics" tab is selected, the license system needs to be completely reset. If the activation process stops at around 80%, and the License Administrator crashes when the "Diagnostics" tab is selected, Microsoft Visual C++ components need to be repaired. Refer to solutions below depending on the issue detected. Resolution Solution 1: Resetting the license system The process to reset the license server system is covered in Resetting the License Server. In some cases, a deeper reset can be required. For that, a tool called "SBO License Server Reset" can be downloaded from the Community. Solution 2: Repairing Microsoft Visual C++ components Method 1 In Control Panel, click Uninstall a program in the Programs group. In the programs list, locate Microsoft Visual C++ 2012 Redistributable (X64) - 11.0.61030 or Microsoft Visual C++ 2012 Redistributable (X86) - 11.0.61030, depending on your system architecture. Right-click the entry name, and then click Change. In the Modify Setup dialog box, click Repair. After the repair process is completed, restart the computer if you are prompted to do this. Method 2 Run the Modify Setup repair functionality for Microsoft Visual C++ Redistributable by starting the installer. VC++ installers In the Modify Setup dialog box, click Repair. After the repair process is completed, restart the computer if you are prompted to do this.
View full article
Picard Product_Support
‎2018-09-06 07:54 AM

Last Updated: Admiral StephenYang Admiral ‎2025-05-09 10:29 AM

Labels:
  • EcoStruxure Building Operation
3992 Views

SP90 Actuator alarm "BV:22 Temperature Sensors Missing or Interchanged"

Issue The SP90 Actuator alarm "BV:22 Temperature Sensors Missing or Interchanged" is triggered. Can we simply swap T1 and T2 in the configuration to fix this, instead of physically swapping the sensors? Product Line Field Devices Environment SpaceLogic SP90 Series Smart Actuator Cause The installer has installed the temperature sensors in the incorrect pipes. Resolution Firmware versions V439 (for actuators products marked V1xxx on the product label) and V539 (for actuators marked V2xx on the product label) introduced MSV:42 (T1 input) and MSV:43 (T2 input) which enable the temperature sensors to be swapped.   You are able to select each as: 1: Disabled 2: Supply temperature 3: Return temperature   If the SP90 actuator is at a lower firmware revision, it can be upgraded. Contact Product Support for the firmware files and upgrade instructions.
View full article
Administrator CraigEl Administrator
‎2025-05-08 09:15 PM

Labels:
  • Field Devices
199 Views

Card Printers supported with Security Expert

Issue What third party Card Printers are supported for use with Security Expert? Product Line EcoStruxure Security Expert Environment Security Expert Client Third-party Card Printers Cause There is no list of supported printers as there are too many devices to test.  Some testing has been done as listed in the resolution below.  If an issue should come up with a card printer then raise a support case and they will assist where possible and offer suggestions regarding the update of printer drivers, windows and printer preferences, etc. If necessary and the customer cannot resolve an issue then they may wish to supply the particular printer for testing and validation. Resolution There is currently no list of supported Card Printers, the following two printers have been tested by Engineering  with Security Expert: Datacard SD260 Datacard CD800 Indications that the HID Fargo HDP8500 and Fargo DTC4500e also work with Security Expert. In general, if the card printer presents itself in Windows as an XPS printer, then the printer should work with the Security Expert Client. This may require a printer driver to be downloaded and installed from the printer manufacturer for the printer to show up in the "Printers and Scanners" list in Windows.   Note: R&D has indicated that currently (12/19/2024) there is no list of printers or documentation as to what specific features or configurations are supported by each printer above.   Some functionality in Security Expert and within printer drivers allows the selection of landscape or portrait orientation. However, hopper selections are not currently supported. Printer testing was done with standard iso card printing using landscape and portrait using a single hopper. Any other requirements outside the above will rest fully with the partner/branch/customer to test and confirm it works as needed.    In unsupported printers it has been observed that some printer functions, such as badge orientation and hopper choice, may not work for all printers using the pop-up printer configuration window within Security Expert client. In those cases a workaround may be to manually change the default printer options in Windows to the required setting before printing badges. If specific functions or badge printers are required then a feature request can be submitted to potentially implement that in a future version of Security Expert. This will need to be raised with your local solution category management.
View full article
Guinan AdamSteele Guinan
‎2019-08-22 03:50 AM

Labels:
  • EcoStruxure Security Expert
1769 Views

Error when viewing Graphic panel in Pinpoint. "Pinpoint: Failed to call pILiveData-&gt;GetLiveData(). ACDataServices has an error."

Issue General Continuum instability is followed by the following error when viewing Graphic panels. "Pinpoint: Failed to call pILiveData->GetLiveData(). ACDataServices has an error." Product Line Andover Continuum Environment Continuum Cyberstation Cause Continuum has become unstable due to modules not starting up properly. This can be evidenced by looking at the Windows Application Event Logs for "Send Email" errors when alarms occur. This may then be followed by Continuum applications starting to crash and post errors. Resolution Remove "email" and "page" entries in Event Notifications if there has not been an Email client installed and configured to email alarms. Set Windows virtual memory settings to 4096. Ensure time synchronization between Cyber and CX. In Continuum General preferences set the Time Interval Between Requests to 100 (default is 30). Set COV increment for noncritical points to non-zero numbers (default is 0). Upgrade to 2.03. If already at 2.03, a reinstall of Continuum may be necessary or at least the pre-requisite 'Visual C++ 2005 redistributable'. Also refer to: Crash of ACCDataServices on start-up or run 
View full article
Picard Product_Support
‎2018-09-06 12:56 PM

Last Updated: Administrator CraigEl Administrator ‎2025-05-07 06:53 PM

Labels:
  • Andover Continuum
1702 Views

Esmi Ultima Media Gateway Card Firmware Update

Warning Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.   Issue Fire Panel unable to display the Media Gateway Card version in system information. Product Line ESMI Fire Detection. Environment FFSULH1007. Cause Panel message output on Media Gateway Card TCP/IP port not functioning and impacting BMS integration with the panel.  Resolution The Media Gateway Card firmware needs to be updated. Follow the steps below to update the Media Gateway Card firmware.   Prerequisites An SD card and SD card reader is required to make a bootable SD card for the firmware update files.   Prepare the SD card The first stage to update the firmware of the media gateway card is to prepare and install the firmware file onto the SD card. The media gateway card requires a micro-SD card. The firmware file is approx. 320MB, so select an SD card with suitable memory size. Format the SD card. Open up Win32Diskimager software. You should see the screen appear below. Click on the open file tab and then select the firmware file. When the firmware is selected it will populate the image file box. Click on the ‘Write’ tab and you should then get a pop-up screen shown below. Click on the ‘Yes’ tab. The firmware will now install onto the SD card. When you see the pop-up screen ‘Write Successful’ appear click on the ‘OK’ tab. The firmware is now loaded onto the SD card. Close down the Win32Diskimager software and eject the SD card form the PC. Install the Firmware Install jumper link onto the middle and top pin of X7 (as per the image below). There is a sliding cover on the socket. First slide the cover to unlock it, then hinge it up. Place the SD-Card in the socket. Hinge down the cover, then slide it to lock it as below The media gateway must be restarted to initiate the installation of firmware. This is done by pressing the reset button, shown in the picture below. The Media Gateway card has a set of 6 LEDs that indicate the status of the card. During normal operation one of the LEDs flashes regularly once each second. After a few seconds you will see a moving pattern progressing through the six LEDs. This indicates that the installation is in progress. The installation will take a few minutes to complete. Note: During this time the panel may display a fault condition that the media gateway card is not present or not working correctly. You can ignore this fault indication. When the firmware installation on the media gateway card is complete, the pattern displayed on the six LEDs will change. Instead of a moving pattern progressing through the six LEDs, all six LEDs will flash on and off together. Once you see this pattern, with all the LEDs flashing together, you should uninstall the jumper, remove the micro-SD-card, and then press the reset button. The media gateway will restart then running the newly installed firmware. It will take a few seconds for the media gateway board to achieve its normal operating state. If the panel displayed a fault indication that the media gateway board was missing, this fault should clear. The ESMI ULTIMA panel now needs to be rebooted to accept the updates from the media gateway card.13. Once the ESMI ULTIMA panel has initialised the firmware installation is now complete.  
View full article
Ensign Sandeep_Kumar006 Ensign
‎2025-05-05 10:30 PM

on ‎2025-05-05 10:30 PM

Labels:
  • ESMI Fire Detection
364 Views
  • « Previous
    • 1
    • 2
    • 3
    • 4
    • 5
    • …
    • 509
  • Next »
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.