Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

EasyLogic and SpaceLogic Controllers & RP-IO Modules as BACnet MS/TP third-party devices

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • EasyLogic and SpaceLogic Controllers & RP-IO Modules as BACnet MS/TP third-party devices
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
2 Likes
4997 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

EasyLogic and SpaceLogic Controllers & RP-IO Modules as BACnet MS/TP third-party devices

Picard RobertAndriolo Picard
‎2023-09-21 12:45 AM

Issue

Can the EasyLogic range of controllers & RP-IO Modules work under Building Operation 3.2 as BACnet MS/TP third-party devices 

Product Line

EcoStruxure Building Operation

Environment

  • EasyLogic Controllers, EasyLogic RP-V, EasyLogic RP-C, EasyLogic MP-C
  • EasyLogic RP-IO
  • SpaceLogic Advanced, Pro, and Pro Plus Controllers that support native BACnet MS/TP (via a SpaceLogic RS-485 Adapters.  
  • Standalone BACnet field controller

Cause

The documentation states that EasyLogic Controllers can be used as a Native BACnet MS/TP device. These devices must be configured using their respective supported Building Operation versions, such as Building Operation 2022 and above. However, there are no guidelines on whether they can be used as a third-party BACnet device, particularly in earlier versions such as Building Operation 3.2.   

Resolution

EasyLogic controllers can be used as BACnet MS/TP third-party devices in Building Operation 3.2 since the EasyLogic range of RP and MP controllers, and RP-IO I/O modules, natively communicate using the BACnet MS/TP protocol.  This same concept applies when using the devices as true 3rd-party devices (e.g., with Continuum and I/A systems) when older controllers fail, and these EasyLogic controllers are used as temporary replacements before a complete transition.

 

What MUST be understood before taking this approach is that there is no automatic conversion when migrating the site (and devices) to later Building Operation versions that support these devices natively. After the upgrade, the controller must be deleted from the database and hosted as a native EBO controller.

 

During this process, some programming may be lost. This risk may be mitigated by creating Custom Types for the application once engineered in Building Operation 2022 (or higher) to future-proof the site for upgrades.  Using the latest firmware for the EasyLogic range of devices is also recommended.  

 

Furthermore, the SpaceLogic Controller Range that supports native BACnet MS/TP (via an RS-485 Adapters) can be configured in the same fashion as described for the EasyLogic range.

 

Refer to Hardware Overview for further details on each product line. 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (3)
  • Find more articles tagged with:
  • RobertAndriolo23
  • RobertAndriolo24
  • RobertAndriolo25
Was this article helpful? Yes No
100% helpful (2/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.