Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Card Printers supported with Security Expert

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Card Printers supported with Security Expert
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
2097 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Card Printers supported with Security Expert

Guinan AdamSteele Guinan
‎2019-08-22 03:50 AM

Last Updated: Crewman ContentModerator ‎2025-08-11 04:13 AM

Issue

What third party Card Printers are supported for use with Security Expert?

Product Line

EcoStruxure Security Expert

Environment

  • Security Expert Client
  • Third-party Card Printers

Cause

There is no list of supported printers as there are too many devices to test.  Some testing has been done as listed in the resolution below. 

If an issue should come up with a card printer then raise a support case and they will assist where possible and offer suggestions regarding the update of printer drivers, windows and printer preferences, etc. If necessary and the customer cannot resolve an issue then they may wish to supply the particular printer for testing and validation.

Resolution

There is currently no list of supported Card Printers, the following two printers have been tested by Engineering  with Security Expert:

  • Datacard SD260
  • Datacard CD800

Indications that the HID Fargo HDP8500 and Fargo DTC4500e also work with Security Expert.

In general, if the card printer presents itself in Windows as an XPS printer, then the printer should work with the Security Expert Client. This may require a printer driver to be downloaded and installed from the printer manufacturer for the printer to show up in the "Printers and Scanners" list in Windows.

 

Note: R&D has indicated that currently (12/19/2024) there is no list of printers or documentation as to what specific features or configurations are supported by each printer above.

 

Some functionality in Security Expert and within printer drivers allows the selection of landscape or portrait orientation. However, hopper selections are not currently supported. Printer testing was done with standard iso card printing using landscape and portrait using a single hopper. Any other requirements outside the above will rest fully with the partner/branch/customer to test and confirm it works as needed. 

 

In unsupported printers it has been observed that some printer functions, such as badge orientation and hopper choice, may not work for all printers using the pop-up printer configuration window within Security Expert client. In those cases a workaround may be to manually change the default printer options in Windows to the required setting before printing badges.


If specific functions or badge printers are required then a feature request can be submitted to potentially implement that in a future version of Security Expert. This will need to be raised with your local solution category management.

Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (3)
  • Find more articles tagged with:
  • AdamSteele19
  • AdamSteele25
  • RobertAndriolo20
Was this article helpful? Yes No
0% helpful (0/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.