Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Steps to follow to unlock SIM PIN when using SIM Card under Flex server

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Steps to follow to unlock SIM PIN when using SIM Card under Flex server
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
982 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Steps to follow to unlock SIM PIN when using SIM Card under Flex server

pranavkumar003 Cadet
‎2025-05-12 12:49 AM

Last Updated: Crewman ContentModerator ‎2025-09-01 03:31 AM

Issue

SIM card not being detected and internet is not connecting automatically when SIM card is inserted inside the Gateway.  

Product Line

EcoStruxure Building Activate

Environment

  • EcoStruxure Building Activate Flex Server
  • EcoStruxure Building Activate Partner Portal

Warning

Hazard of Electric Shock: Remove all power from all devices before removing any covers or doors of the system. Disconnect power at the device and at the power source.

Electrostatic Discharge Required: Always discharge static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Caution While removing gateway cover: Open the gateway screws and delicately remove the top cover. Take extra care during this step, as the top cover is connected to the antenna cable via a thin wire. After opening the top cover, you will be able to see the top view of the board, please insert the active SIM card in the designated slot.

Once the Sim Card is properly inserted, fix the screws back and ensure that the 4G&Wi-Fi Antenna is attached properly. If the antenna cable remains disconnected from the board, then the GSM will not work.

Cause

Some network service providers have a username, password and SIM PIN set by default when they issue the SIM to the customer. If the Gateway is using the SIM for internet, it requires any username, password and SIM PIN to be disabled before inserting the SIM inside the Gateway. 

Resolution

Contact the Network service provider directly to disable the username and password. The Network service provider can disable the username and password from the backend.

For disabling the SIM PIN follow the below procedure:

Steps to follow to unlock SIM PIN

An example YouTube video on the steps detailed below can be seen at: How to unlock your SIM Card

  1. Upon receiving the SIM kit (note down the PUK number and also note down the SIM PIN if available)
  2. Insert the SIM card to a Mobile device/cellular device
  3. Type in the SIM PIN from the Step 1 and Unlock the SIM
  4. Navigate to the settings page – Network section - SIM settings - SIM PIN - Disable the SIM PIN option

    SIM CARD SETTINGSSIM CARD SETTINGSSIM CARD SETTINGS          SIM PIN DISABLEDSIM PIN DISABLEDSIM PIN DISABLED

  5. Reconfirm if the SIM PIN is disabled by reinserting the SIM from the SIM tray and check if it asks for PIN. If the SIM PIN is successfully disabled, it will not ask for SIM PIN at startup. If it still asks, repeat Step 4.

  6. Insert the SIM inside the Gateway SIM Slot and check for network connectivity and that the gateway goes online.

  • After inserting the SIM card properly, power up the gateway and allow the gateway to boot up. This process may take up to 5 minutes. Once completed, the device should come online and can be provisioned through a partner portal

 

In case the SIM PIN is unavailable

An example YouTube video on the steps detailed below can be seen at: How to Unlock Sim Card / Sim locked by Pin Code or PUK Code 

  1. Insert the SIM card into a Mobile device/cellular device
  2. Type in incorrect PIN more than 4 times till it asks to enter PUK code.
  3. Contact the Network Service Provider and perform the verification and obtain the PUK Code for the SIM from the Network provider directly
  4. Type the PUK code into the mobile device in the PUK code page
  5. Navigate to the Network settings - SIM PIN - Set a SIM PIN inside the settings
  6. Use this SIM PIN to Disable the SIM PIN lock.
  7. Reconfirm that the SIM PIN is disabled by reinserting the SIM from the SIM tray and check that it does not request a PIN.
Labels (1)
Labels:
  • EcoStruxure Building Activate
Tags (1)
  • Find more articles tagged with:
  • PranavKumar25
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.