Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Building Automation Knowledge Base
  • Label: Field Devices
Options
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
  • Alphabetical
  • Andover Continuum 2,197
  • TAC Vista 2,029
  • EcoStruxure Building Operation 1,897
  • TAC IA Series 1,688
  • TAC INET 1,444
  • Field Devices 722
  • Satchwell BAS & Sigma 402
  • EcoStruxure Security Expert 343
  • EcoStruxure Building Expert 222
  • Satchwell MicroNet 212
  • EcoStruxure Access Expert 153
  • CCTV 52
  • Project Configuration Tool 48
  • EcoStruxure Building Activate 19
  • EcoStruxure Building Advisor 13
  • ESMI Fire Detection 13
  • Automated Engineering Tool 5
  • EcoStruxure Building Data Platform 3
  • EcoStruxure Workplace Advisor 1
  • EcoStruxure for Retail - IMP 1
Top Contributors
  • Product_Support
    Product_Support
  • DavidFisher
    DavidFisher
  • CraigEl
    CraigEl
See More Contributors
Related Products
Thumbnail of EcoStruxure™ Building Operation
Schneider Electric
EcoStruxure™ Building Operation
4
Thumbnail of SmartX IP Controllers
Schneider Electric
SmartX IP Controllers
1
Thumbnail of EcoStruxure™ Building Advisor
Schneider Electric
EcoStruxure™ Building Advisor
1

Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

Label: "field devices"

View in: "Building Automation Knowledge Base" | Community

721 Posts | First Used: 2018-09-06

Building Automation Knowledge Base

Sort by:
Date
  • Date
  • Views
  • Likes
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend
  • « Previous
    • 1
    • …
    • 8
    • 9
    • 10
    • …
    • 37
  • Next »
Label: "Field Devices" Show all articles

TC900 Modbus bias, termination and number of devices

Issue What is the unit load of a TC900 thermostat and what are the bias and termination requirements when used with a SmartX Server. Product Line EcoStruxure Building Operation, Field Devices Environment TC907-3A4LMA TC907-3A4DLMSA TC907-4FMSA TC907-3A4DPMSA TC907-3A4DPMSA-24 TC903-3A4LMA TC903-3A4DLMSA TC903-4FMSA TC903-3A4DPMSA TC903-3A4DPMSA-24 SmartX Server Cause Documentation does not state the RS-485 transceiver type for the TC900 range, making it unclear how many devices can exist under a SmartX servers RS-485 serial port ComA or ComB. Resolution Use the Worksheet for Configuration of RS-485 Bus with generic RS-485 devices on Webhelp to determine the appropriate Modbus configuration. The answers to the transceiver interface attributes below can be applied to complete the worksheet. Q1 Failsafe Receiver : The TC900 uses an RS-485 transceiver with an integrated idle-state failsafe receiver. Q2 Data Transmission Speed : TC900 thermostats can be configured to communicate at 4800, 9600, 19200 or 38400 bps. Q4 Isolated Interface : The TC900 does not provide an isolated RS-485 interface. Q6a Measured Resistance : With no electrical connections to the TC900, the measured resistance between the RS-485 low-side (-) signal and the communications common is 8.2K ohms. Based on this the unit load of the TC900 is 1.46 (12.000/8,200) Bias requirements and number of devices If there are only TC900 devices on the RS-485 bus then Generic RS-485 Network Device configuration 1 applies, configuration becomes very simple and no node or distance reductions are called for. The failsafe receivers can typically operate with no added bias resistors. Connect a 120 ohm termination resistor across the + and - data lines at the head end of the bus (typically at the SmartX server). Connect another 120 ohm termination resistor across the + and - data lines on the last node at the far end of the bus. Connect the shield drain wire to earth ground terminal rail in the panel with the SmartX server. This is the only ground connection of the shield for the complete cable segment. Connect the RET/Shield terminal (see the figure below) on the SmartX server to the ground rail in the panel using a 12 AWG (3.31 mm²) to 18 AWG (0.82 mm²) wire. Since the TC900 has a unit load of 1.4 the maximum number of devices that can be placed under each comm port using this configuration is 21 (31.5 / 1.46 = 21.5) Also check out the SmartStruxure-RS485-Controller Unit Load Quick-Help video on the Exchange. Note:  Adding an RS-485 Repeater at this point provides another 32 Units Loads to the Network which can be continued up to the Architectural Maximum defined for the hosting controller.
View full article
Administrator CraigEl Administrator
‎2020-07-14 06:58 PM

Last Updated: Admiral David_Kendrick Admiral ‎2024-11-18 06:56 AM

Labels:
  • EcoStruxure Building Operation
  • Field Devices
5737 Views

Extending EBO Zigbee Wireless Mesh Using Repeaters

Issue When a SED-TRH-G-5045 sensor is positioned outside the range of the main EBO Zigbee wireless mesh, what is the recommended method or product to extend the wireless coverage? Product Line EcoStruxure Building Operation Environment Building Operation Automation Server Premium Cause The SED-TRH-G-5045 is a Zigbee pro sleepy end device. Resolution Any Zigbee router within the system can function as a repeater to extend the radio communication. The router should be positioned within the radio range of the sensor and within the range of the RPx or another router. If a Zigbee device is powered by mains, it typically operates as a router. While there are currently no SE products designed solely with "repeater capability," several SE products possess router capabilities in addition to other capabilities, SE8000 SpaceLogic room controller Wiser plug CCTFR6500 Wiser Power Micromodule CCTFR6730 Wiser Room Thermostat with display CCTFR6400 or CCTFR6401. We have not officially tested any 3rd party Zigbee routers, however the IKEA TRÅDFRI repeater is known to work effectively.
View full article
Guinan MikaelKrantz Guinan
‎2024-09-11 06:21 PM

on ‎2024-09-11 06:21 PM

Labels:
  • EcoStruxure Building Operation
  • Field Devices
1930 Views

How to identify what ports are being used on a PC

Issue How to identify what ports are being used on a PC. Product Line All product Lines. Environment Any Windows OS Cause Running multiple applications on the same PC without managing TCP/UDP port assignments can lead to conflicts. Resolution TCPView will help you identify all ports and services to each application. Download from Microsoft's website http://technet.microsoft.com/en-us/sysinternals/bb897437.aspx Detailed instructions are available at the site.
View full article
Picard Product_Support
‎2018-09-10 01:28 PM

Last Updated: Kirk Mahmoud_Sayed Kirk ‎2024-05-22 01:21 AM

Labels:
  • Andover Continuum
  • CCTV
  • EcoStruxure Building Operation
  • Field Devices
  • Satchwell BAS & Sigma
  • Satchwell MicroNet
  • TAC IA Series
  • TAC INET
  • TAC Vista
2253 Views

Galvanic isolation for SHD2/SCD2

Issue Does SHD2/SCD2 have galvanic isolation? Product Line EcoStruxure Building Operation Environment Building Operation SmartX Living Space Sensor Cause Galvanic isolation is a principle of isolating functional sections of electrical systems to prevent current flow; no direct conduction path is permitted. Resolution The SHD2XP2A/SCD2XPXAVX does not have galvanic isolation.
View full article
Guinan MikaelKrantz Guinan
‎2024-04-24 04:18 AM

Last Updated: Janeway PeterEdvik Janeway ‎2024-04-24 04:19 AM

Labels:
  • EcoStruxure Building Operation
  • Field Devices
3360 Views

SLP BACnet Setpoint limits

Issue SLP BACnet Setpoint limits Product Line EcoStruxure Building Operation, Andover Continuum, Field Devices Environment SpaceLogic SLP Series Cause The BACnet Object "Temperature Setpoint" includes properties Minimum and Maximum values These can be used to limit the setpoint, however the values are not saved in non volatile memory, thus the value revert to default after a power cycle (0 and 50 degC). The Setpoint object needs to be manually downloaded from EBO following a power cycle to set these properties. These properties cannot be written to individually. Thus changing these properties is unlikely to be good practice. Resolution A script program can be used to set limits to the Temperature Setpoint. Example below Note the "Value transfer settings" need changing to "Transfer value each time..." as below
View full article
Dave_Shore Schneider Alumni (Retired)
‎2024-02-07 08:53 AM

on ‎2024-02-07 08:53 AM

Labels:
  • Andover Continuum
  • EcoStruxure Building Operation
  • Field Devices
4651 Views

Replacement for SPA1505 – SPA1506

Issue Information for replacement for the SPA1505 and SPA1506 Product Line Field devices Environment Pressure sensors Cause "PA-00167 Sensors and Input Devices New SPP930 Relative Pressure Switch" suggests SPP930 replaces SPA 1505 and SPA 1506. The link provided for the SPP930’s manufacturer’s data sheet, no longer works Resolution SPP930 Part number 004701160 replaces the SPA 1505 SPP930 Part number 004701170 replaces the SPA 1506 The site wiring should be checked, to ensure it complies with replacement switches reduced current ratings.   SPA 1505/1506 data sheet Huba Controls type 620/625 data sheet.
View full article
Gary Schneider Alumni (Retired)
‎2024-01-16 05:22 PM

on ‎2024-01-16 05:22 PM

Labels:
  • Field Devices
5597 Views

Insight Sensor/Multi sensor Ambient Light Sensor Calibration

Issue The Insight Sensor and Multi Sensor Ambient Light Sensor require calibration before they can be effectively used. Product Line EcoStruxure Building Operation. Environment Insight Sensor. Multi Sensor Cause When setting up a new Insight Sensor or Multi Sensor device, the default settings for Gain and offset may result in inaccurate readings. Calibration is necessary to ensure accurate data collection based on the specific installation area. Resolution To perform the calibration, the following two tasks need to be carried out manually: Calibrate the Light Sensor: Conduct the calibration process in an environment without any daylight for optimal results. Set the light to 100%. Measure the lux level at the reference point using a lux meter. Adjust the gain settings on the sensor to match the measured lux level. Linearize the Feedback Signal: In some cases, lights may not provide a linear feedback (lux level) as the output increases. To compensate for this non-linearity, the signal from the controller is linearized before being sent to the output. During the optimization phase, the controller incrementally increases the output in 10% steps, measuring the adjacent lux levels for each step. The maximum lux supplement is calculated by subtracting the lux level at 100% output from the lux level at 0% output. After the optimization phase, breakpoints are determined and verified by re-running the test. If the results fall within the maximum difference limit compared to a linear signal, the calibration test is considered valid. Remember, performing the calibration process without any daylight present will yield the best results.  
View full article
Guinan MikaelKrantz Guinan
‎2023-11-29 04:43 PM

on ‎2023-11-29 04:43 PM

Labels:
  • EcoStruxure Building Operation
  • Field Devices
5257 Views

Offer Creation Roadmap

Issue What new features are planned for inclusion in future product releases? Product Line Andover Continuum, EcoStruxure Building Operation, Field Devices, Satchwell BAS & Sigma, Satchwell MicroNet, TAC IA Series, TAC INET, TAC Vista, EcoStruxure Access Expert, EcoStruxure Security Expert Environment All product ranges Cause Information required on future Product Marketing plans. Resolution This document is no longer published on the Download Center by Product Management. For further information on the future product planning please contact the Product Manager for the specific product in your region. Americas: Americas.EcoStruxureBuilding@schneider-electric.com EMEA: EMEA.EcoStruxureBuilding@schneider-electric.com Asia Pacific & India: AsiaPac.EcoStruxureBuilding@schneider-electric.com
View full article
Picard Product_Support
‎2018-09-06 10:23 AM

Last Updated: Administrator CraigEl Administrator ‎2023-08-20 05:37 PM

Labels:
  • Andover Continuum
  • EcoStruxure Access Expert
  • EcoStruxure Building Operation
  • EcoStruxure Security Expert
  • Field Devices
  • Satchwell BAS & Sigma
  • Satchwell MicroNet
  • TAC IA Series
  • TAC INET
  • TAC Vista
3460 Views

TC300 thermostat cooling only operation

Issue In applications where heating is not required is it possible to change the thermostat operation to cooling only? Product Line Field Devices Environment TC300 thermostat Cause By default the TC300 thermostat is configured for heating and cooling. It should be possible to lockout operation of heating in cooling only applications so that the user cannot inadvertently change modes. Resolution In thermostat model TC303-3A2DLS parameter item 7 allows selection of cooling or heating only mode.
View full article
Picard Product_Support
‎2018-09-07 10:59 AM

Last Updated: Administrator CraigEl Administrator ‎2023-07-10 07:38 PM

Labels:
  • Field Devices
1962 Views

What is the Output of a STR300

Issue Confusion in documentation of the output type of an STR300 temperatire transmitter Product Line Field Devices Environment STR300 series transmitter Cause The STR300 is an electronic living space transmitter that converts a measured temperature into an electric current signal. The transmitter is delivered as a complete unit, comprising a Pt100 classB sensing element and an amplifier mounted in a housing. STR300 is intended either for surface mounting on a wall or installation in a standard switch box in dry, dust free rooms.   The HVAC Sensors Catalogue incorrectly shows that the STR300 Series has an Output of 0-10V while  the datasheet correctly shows the output as 4-20ma. Resolution The STR300 has an output signal of 4 to 20 mA corresponding to a temperature range of 0-40°C
View full article
Picard Product_Support
‎2018-09-11 04:25 AM

Last Updated: Administrator CraigEl Administrator ‎2023-07-10 07:34 PM

Labels:
  • Field Devices
2580 Views

What is pneumatic actuator spring range shift and how can it be eliminated?

Issue What is pneumatic actuator spring range shift and how can it be eliminated? Product Line Field Devices Environment Pneumatic Actuator Cause Spring range shift is an inherent feature of all spring return pneumatic actuators without positive positioners. The nominal published spring range of a pneumatic actuator without a positive positioner is the air pressure required to fully stroke the actuator WITH NO EXTERNAL LOAD. In the extend direction against an opposing load as provided by a damper or a valve, the supply air pressure must be increased above the spring range of the actuator to overcome the spring and the opposing force. In the retract direction against an opposing load as provided by a damper or a valve, the supply air pressure must be decreased below the spring range of the actuator so that the spring can overcome the air pressure and the opposing force. Under constant load conditions, the range of the actuator is offset by the amount of air pressure required to provide close-off of the damper or the valve. Resolution When is "Spring Range Shift" a concern? It is a concern when two or more pneumatic controlled devices should be sequenced from one pneumatic signal without an overlap. An example would be a normally open heating valve and a normally closed cooling valve being sequenced from a direct acting thermostat, In this example the spring range of the normally open valve will shift upward and the normally closed valve will shift downward which means the two valves may overlap. Another area of concern is that pneumatic control signal provides proper pressure span to operate the control device and provide "tight" close-off of damper or valve. Examples of limited pressure change would be: pneumatic controllers maximum output which is limited by main air pressure; the low pressure output capability of a pneumatic controller; and electronic to pressure transducer which can have a limited output such as 3 to 15 psig.   What can be done to overcome "Spring Range Shift" when sequencing devices? Sequencing can be accomplished in a pneumatic system by selecting actuators with appropriate spring ranges, utilizing positive positioners (AK-42309-500 or N800-0555) or ratio relays with bias adjustment (2378-501) or controllers with separate outputs for each actuator. Positive positioners on damper and valve actuators provide the versatility of start point and span adjustment plus the availability of full pneumatic power for positioning. This is the ideal way to provide precision sequencing, since variable loading on the actuator will not effect the sequencing. Biased start ratio relays may be used to provide a method of sequencing by amplifying or shifting the pneumatic signal. For applications involving sequencing a pressure to electric (P.E.) switch with a pneumatic actuator, the P.E. can often be adjusted to operate outside the operating range of the actuator. Sometimes larger actuators will help the sequencing problem. Using full actuator stroke to rotate the damper less than 90 degrees increases the force delivered to the damper and therefore reduces control signal change required to control the actuator. Rotating the damper 60 degrees usually provides almost full flow through the damper. If the actuator has an adjustable start point, adjusting the start points can help prevent sequencing problems. Normally open valves or dampers should have start point adjusted to the minimum and normally closed adjusted to the maximum. Sequencing problems can be eliminated by providing controllers with separate outputs for each actuator and do the sequencing in the controller. What can be done to increase the close-off of a damper or valve actuator due to limited or insufficient pneumatic control pressure to the control device? Proper control and close-off of the control device can be accomplished by selecting actuators with appropriate spring ranges, utilizing positive positioners (AK-42309-500 or N800-0555) or ratio relays with bias adjustment ( 2378-501). Positive positioners on damper and valve actuators provide the versatility of start point and span adjustment plus the availability of full pneumatic power for positioning (0 to main air pressure to the actuator). Biased start ratio relay provide a method of amplifying or shifting the pneumatic signal. Selecting larger actuators will increase close-off pressure. Using full actuator stroke to rotate the damper less than 90 degrees increases the force delivered to the damper. Rotating the damper 60 degrees usually provides almost full flow through the damper. If the actuator has an adjustable start point, proper adjustment of the start points will increase close-off. Normally open valves or dampers should have start point adjusted to the minimum and normally closed adjusted to the maximum. Provide electronic to pneumatic transducers with sufficient input span to obtain maximum or sufficient pneumatic output.
View full article
Picard Product_Support
‎2018-09-06 02:29 PM

Last Updated: Administrator CraigEl Administrator ‎2023-07-10 07:13 PM

Labels:
  • Field Devices
5761 Views

TC303 Time and Day of the Week Settings

Issue TC303 Time and Day of the Week Settings Product Line Field Devices Environment TC303 Series Fan Coil Thermostat Cause The time and day displayed on the thermostat is incorrect Resolution Press and hold the M button on the thermostat for approximately 3 seconds and the time's hour will start to blink. Use the Up/Down arrows to change the value. Press the M button again to switch the focus to minutes and the day of the week. 
View full article
Picard Product_Support
‎2018-09-06 07:29 AM

Last Updated: Administrator CraigEl Administrator ‎2023-07-10 07:25 PM

Labels:
  • Field Devices
2336 Views

What are the sensor temperature vs resistance values of the TC range of thermostats.

Issue Resistance against temperature Product Line Field Devices Environment TC300 thermostat range TC900 thermostat range RS-03 remote sensor Cause Remote sensor compatibility Resolution The TC thermostat range use a 10K type 3 (3950) Negative Temperature Coefficient (NTC) thermistor. Whilst this is similar to the 10K type 3 thermistor used in the other BMS field device sensors such as the SpaceLogic SLA range, it has a different resistance curve and the temperature read will be different.   The table below shows that at typical room temperatures the error is 0.6°C or less. T(°C) RS-03 R(KΩ) SPA R(KΩ) Error % Error °C 0 31.77 29.575 6.91% 1.736 5 24.94 23.504 5.76% 1.366 10 19.68 18.809 4.43% 1.052 15 15.62 15.146 3.03% 0.812 20 12.47 12.271 1.60% 0.63 25 10 10 0.00% 0 30 8.064 8.195 -1.62% 0.3872 35 6.538 6.752 -3.27% 0.3052 40 5.327 5.592 -4.97% 0.2422 45 4.363 4.655 -6.69% 0.1928 50 3.592 3.893 -8.38% 0.1542   Click here to view the TC thermostat's RS-03 remote temperature against resistance chart. Click here to download the chart that provides the temperature against resistance reading for the TC thermostat's RS-03 remote temperature sensors.
View full article
Picard Product_Support
‎2018-09-11 07:51 AM

Last Updated: Administrator CraigEl Administrator ‎2023-06-08 12:06 AM

Labels:
  • Field Devices
4080 Views

PM5340 does not update values via BACnet in EBO

Issue Values in EBO from a PM5000 series energy meter do not update Product Line EcoStruxure Building Operation, Field Devices Environment Building Operation Server BACnet PM5000 series energy meter Cause The EBO trace log shows a lot of BACnet related error messages, such as:   nsp.pin.BACnet.VariableProperty Subscription to ~/BACnet Interface/IP Network/PM 5340/Application/THD Current - Ph G attempted COV, but will POLL due to BACnet error: 0x00030013 (resources,no_space_to_add_list_element)   This error indicates that a Change of Value (COV) subscription is being attempted but has failed. This is due to a resource issue with the device, i.e., error class 0x0003 from error code 0x00030013. The error is no space to write property (0013 part) which suggests the subscription limit of the device has been reached. Refer to the Decoding BACnet Errors Knowledge Base article for further information on decoding the error code.   Reviewing the PM5300 series user manual reveals that the device only supports 20 COV subscriptions.     Resolution Remove BACnet objects that are not required in EBO, it is unlikely that fewer than 20 values will be practical. Disable COV for the device in EBO. This can be done via the service_blacklist as noted in the BACnet RULES implementation to disable features such as readPropertyMultiple, COVs etc How to disable RPM (readPropertyMultiple), COVs etc services in AS/ES BACnet interface. Knowledge Base article. The following is an example service_blacklist for the PM3450 <blacklist> <rule> <vendor>10</vendor> <model>PM5340</model> <no-cov/> <no-rpm/> </rule> </blacklist> Polling can put an unintended load on the polling device and the polled device. The polling intervals should be adjusted using the settings on the BACnet Interface. This is available from BACnet Interface -> Properties -> Advanced and scroll all the way to the bottom as shown below for an ES. If looking at the option for an Automation Server it will also have additional options for the RS485 communication ports. Minimum polling intervals in the range of 5,000 to 10,000ms are a good starting point.  
View full article
Administrator CraigEl Administrator
‎2023-05-30 05:51 PM

on ‎2023-05-30 05:51 PM

Labels:
  • EcoStruxure Building Operation
  • Field Devices
3177 Views

Viconics VT7600x1000x exceeding the set 3 Cool Cycles Per Hour (CPH)

Issue Tested the Viconics VT7600x1000x for Cool CPH set to 3.  Manually heated the thermostat and let it cool to cycle the cool stages and it cycled on and off 7 times before stopping the test.  According to the documentation it should have stopped after 3 on/off cycles. Product Line Field Devices Environment SSL SE7000 Cause Cooling/heating has to be within 15-85% of the proportional band. Resolution With the Viconics VT7600x1000x series products, the CPH only works when the cooling/heating demand is within 15 to 85% of the proportional band. The thermostat has a 2 degree proportional band (fixed) so at a setpoint of 72 and CPH of 3 (cooling CPH adjustable 3-4), if the temperature stays between 72.3 and 73.7 the CPH is at 3. Outside of that band the cooling/heating is allowed to cycle as often as needed.
View full article
Picard Product_Support
‎2018-09-06 02:33 PM

Last Updated: Administrator CraigEl Administrator ‎2023-03-31 07:45 PM

Labels:
  • Field Devices
1429 Views

How do you reset the Viconics VT7200, VT7300, &amp; VT7600 LON series thermostats back to factory default values?

Issue How do you reset the Viconics VT7200, VT7300, & VT7600 LON series thermostats back to factory default values? Product Line Field Devices Environment SSL SE7000 Cause There's no button or command that sets the thermostat to its default parameter settings. Resolution Either set them manually or through the snvts available via a LON integration.  The Viconics Lon Integration Manual will help with identifying the proper snvts to use.
View full article
Picard Product_Support
‎2018-09-06 02:29 PM

Last Updated: Administrator CraigEl Administrator ‎2023-03-29 04:57 PM

Labels:
  • Field Devices
3772 Views

BACnet/MSTP communication to Viconics VT thermostats is intermittent.

Issue BACnet/MSTP communication to Viconics VT thermostats is intermittent. Product Line Field Devices Environment SE7000 Room Controller Cause Possible cause is physical layer and device addresses. Resolution Verify the physical layer (i.e. wire, end of line resistors and bias resisters) is installed as recommended.  A common wiring error is landing the trunk cable shield to the "REF" terminal at the thermostat. The shield should be carried through but not landed at the thermostat and the trunk shield should be grounded in one place. Duplicate device addresses can cause this type of issue as well. Verify each controller has a unique "Com addr" which is part of its instance number. This can be viewed and modified from the display panel of the thermostat. To enter the configuration parameter menu: VT7200 series press and hold the button(OVERRIDE) for 8 seconds VT7300 series press and hold the middle button(°C/F or OVERRIDE)for 8 seconds. VT7600 series press and hold the button(MENU)for 8 seconds
View full article
Picard Product_Support
‎2018-09-06 02:44 PM

Last Updated: Administrator CraigEl Administrator ‎2023-03-28 09:20 PM

Labels:
  • Field Devices
1753 Views

SLPSXC2 CO2 sensor calibration using both ABC standard and Fresh Air process

Issue Can SLPSXC2 CO2 sensor calibration be used with both methods (ABC standard and Fresh Air process) at the same time? Product Line Field Devices. Environment Building Operation SmartX Living Space Sensor. Cause SLPSXC2 CO2 can be calibrated using two different methods. Automatic Baseline Calibration(ABC) The ABC algorithm constantly keeps track of the sensor’s lowest reading over a pre-configured time interval and slowly corrects for any long-term drift detected when compared to the expected fresh air value of 400 ppm. ABC calibration is enabled/disabled through coil 4 (invoke = enable ABC). Manual Calibration Coil 11 triggers the manual calibration (FRC 400ppm) => this will tell the sensor that the current level of CO2 should be interpreted as 400ppm. When setting this register to 1, it automatically goes back to 0 a couple of seconds later. Setting Coil 11 to value 1 is the same as pressing the calibration button. Resolution The both methods of calibration can be used simultaneously since one method is for correcting drift over time (1 week intervals), the other is a manually executed reset.   The only error would come if the unit was exposed to high CO2 concentrations at night, inducing abnormal averages. If ABC is disabled, manual calibration would need to be performed more frequently.
View full article
Guinan MikaelKrantz Guinan
‎2023-03-07 03:48 PM

on ‎2023-03-07 03:48 PM

Labels:
  • Field Devices
3729 Views

SE8xxx Room Controller Password

Issue Unable to access the SE8xxx or SER8xxx Room Controller configuration parameters menu - displays an error code. Product Line EcoStruxure Building Expert, Field Devices  Environment SE8xxx and SER8xxx Room controller SE8000 and SER8000 Series Ex. Viconics branding VT8000 Series Cause The PswrdSet parameter sets a protective access password to prevent unauthorized access to the configuration menu parameters. An error code is displayed whenever the password lockout is active and an incorrect password is used. Resolution Contact your region's Customer Care Center for a temporary password. The error code which is unique to that controller will be required by the Customer Care Center to calculate the temporary password.
View full article
Sisko DavidChild Sisko
‎2020-03-13 08:26 AM

Last Updated: Administrator CraigEl Administrator ‎2023-02-14 03:36 PM

Labels:
  • EcoStruxure Building Expert
  • Field Devices
2929 Views

How to read the accuracy and repeatability on CO2 sensors

Issue How to read and understand the accuracy and repeatability on CO2 sensors. The sensors shows 380 ppm, is it defect? Product Line Field Devices Environment CO2 Sensors Cause Accuracy +- 30ppm +-2% of measured value Repeatability +- 20ppm +-1% of measured value Resolution   Accuracy The accuracy of a unit is defined as the tolerance between the actual absolute gas concentration and the measured value. For example, if a unit has a specified accuracy of ±30ppm, this implies that the displayed value will be within 30 parts‐per‐million of the actual gas concentration under standard ambient operating conditions. If the gas concentration in a room is 400ppm, then the sensor is operating within rated parameters if it reads anywhere between 370ppm and 430ppm on average.   Repeatability Repeatability is closely related to precision. Repeatability is defined as the variance in measured values of a known, unchanging gas sample upon repeat measurements. To put it another way repeatability is the range of acceptable values the sensor will read, relevant to a previous measurement, when measuring a gas, independent of the actual gas concentration.  For example, if the gas concentration in a room is 400ppm and the sensor has a rated repeatability of ±10ppm, then if originally the sensor reads 420ppm, upon future measurements the sensor will read between 410ppm and 430ppm.  Repeatability is generally specified as having a tighter tolerance than accuracy. Even if a sensor is reading a value that is slightly high when compared to the actual gas concentration, it is likely that it will read close to the same slightly higher value upon repeat measurements.   How to understand the accuracy and repeatability Accuracy +- 30ppm +-2% of measured value Repeatability +- 20ppm +-1% of measured value Accuracy at 400ppm:                     Min =  – (30 + 400*0.02) = -38                     Max = + (30 + 400*0.02) = 38 Repeatability at 400pm:                     Min = - (20 + 400*0.01) = -24                     Max = (20+400*0.01) = 24   This means that in a 400ppm environment, the sensor output can vary between                     400-38-24 = 328 ppm                     400+38+24 = 462 ppm Finally, based on the explanation given above, 380ppm would still be in spec. However, another reason could be that the calibration was done in an environment that was not the “purest” and by doing so, an offset was created on the 400-baseline explaining why values below 400ppm are reported.   As said 380ppm is still in spec but the customer could try to recalibrate the CO2 sensor to see if it changes anything.
View full article
Guinan MikaelKrantz Guinan
‎2022-11-24 01:44 AM

on ‎2022-11-24 01:44 AM

Labels:
  • Field Devices
2538 Views
  • « Previous
    • 1
    • …
    • 8
    • 9
    • 10
    • …
    • 37
  • Next »
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.