Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

How to read the accuracy and repeatability on CO2 sensors

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to read the accuracy and repeatability on CO2 sensors
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • PeterEdvik
    PeterEdvik
  • MikaelKrantz
    MikaelKrantz

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2544 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to read the accuracy and repeatability on CO2 sensors

Guinan MikaelKrantz Guinan
‎2022-11-24 01:44 AM

on ‎2022-11-24 01:44 AM

Issue

How to read and understand the accuracy and repeatability on CO2 sensors.

The sensors shows 380 ppm, is it defect?

Product Line

Field Devices

Environment

CO2 Sensors

Cause

Accuracy +- 30ppm +-2% of measured value

Repeatability +- 20ppm +-1% of measured value

Resolution

 

Accuracy

The accuracy of a unit is defined as the tolerance between the actual absolute gas concentration and the measured value. For example, if a unit has a specified accuracy of ±30ppm, this implies that the displayed value will be within 30 parts‐per‐million of the actual gas concentration under standard ambient operating conditions. If the gas concentration in a room is 400ppm, then the sensor is operating within rated parameters if it reads anywhere between 370ppm and 430ppm on average.

 

Repeatability

Repeatability is closely related to precision. Repeatability is defined as the variance in measured values of a known, unchanging gas sample upon repeat measurements. To put it another way repeatability is the range of acceptable values the sensor will read, relevant to a previous measurement, when measuring a gas, independent of the actual gas concentration. 

For example, if the gas concentration in a room is 400ppm and the sensor has a rated repeatability of ±10ppm, then if originally the sensor reads 420ppm, upon future measurements the sensor will read between 410ppm and 430ppm. 

Repeatability is generally specified as having a tighter tolerance than accuracy. Even if a sensor is reading a value that is slightly high when compared to the actual gas concentration, it is likely that it will read close to the same slightly higher value upon repeat measurements.

 

How to understand the accuracy and repeatability

Accuracy +- 30ppm +-2% of measured value
Repeatability +- 20ppm +-1% of measured value

Accuracy at 400ppm:

  •                     Min =  – (30 + 400*0.02) = -38
  •                     Max = + (30 + 400*0.02) = 38

Repeatability at 400pm:

  •                     Min = - (20 + 400*0.01) = -24
  •                     Max = (20+400*0.01) = 24

 

This means that in a 400ppm environment, the sensor output can vary between

  •                     400-38-24 = 328 ppm
  •                     400+38+24 = 462 ppm

Finally, based on the explanation given above, 380ppm would still be in spec.

However, another reason could be that the calibration was done in an environment that was not the “purest” and by doing so, an offset was created on the 400-baseline explaining why values below 400ppm are reported.

 

As said 380ppm is still in spec but the customer could try to recalibrate the CO2 sensor to see if it changes anything.

Labels (1)
Labels:
  • Field Devices
Tags (1)
  • Find more articles tagged with:
  • MikaelKrantz22
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.