New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 04:19 AM
📖 Home
everything you needed to know about alarms, events and using SQL lists to interrogate the system
ClearSCADA logs all occurrences on your system, creating an audit trail for system operation and reporting. Events are the records of these occurrences on your system. ClearSCADA logs events, for example, for each user interaction with the system, and for automatic system occurrences such as alarms, point updates, scheduled archiving, and so on. ClearSCADA logs the events in the Event Journal. These occurrences can be viewed by displaying an Events List.
ClearSCADA raises alarms when an indication of an abnormal condition detected. ClearSCADA will raise an alarm, for instance, if communications with an outstation fails, or if a scheduled dial in window is missed. Additionally, items in your database may be configured to operate within certain limits, and if such an item returns values that are outside those limits, ClearSCADA may be configured to raise an alarm to indicate that occurrence. When an alarm is raised, it is added to the Alarms List and the Alarm Banner.
A ClearSCADA provides mechanisms to query and list different aspects of the system including alarm activity, event activity, database object information and historical point data. When a list queries is performed, ClearSCADA uses SQL to query the database and retrieve the data that is required. The entries in the List are then returned and displayed in colours that define their state and status.
Home
More Links:
Display Alarm Related Events
Generating Custom Alarms and Events
When do the Point Alarm Limits Get Processed
Control Failed Alarm not Clearing until Successful Control Action
Displaying a List of Disabled Alarms
Monitoring Alarm Active and Alarm Received Times
Excessive Event Journal Logging
Area of Interest Filtering of Events and Alarms
SMS Alarm Redirection
How queries are optimised and executed by ViewX
Restarting Alarm Redirection
Recording an Alarm Response for Multiple Alarms
Enforce Alarm Acknowledge With Comment
Redirecting Alarms to Applications
Designing Queries for GIS Map Markers
Redirect alarms with messages referring to other objects
Configuring the Alarm & Event Printer Service
Embedded Mimic in Email Alarm Redirection
Disabling and Enabling Alarms
Querying CDBPoint for a Single Data Type
SQL Join Optimization
Changing Alarm Limit Does Not Immediately Raise an Alarm
Object Menu on Embedded Lists in ViewX and the Web Client
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.