Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 11:55 PM
HKEY_LOCAL_MACHINE\Software\Serck Controls\SCX6\AEPrinter
| Value Name (type) | Details |
|---|---|
| System (REG_SZ) | System Name to connect to. There is no default. |
| TerminalWidth (REG_DWORD) | Width of the terminal, in characters. The default is 0 (no terminal width used). |
| Enabled (REG_DWORD) | Specify 1 to enable this connection, 0 to disable. The default is 1. |
| InitialRefresh (REG_DWORD) | Setting to 1 will output the current active Unacknowledged alarms on the system when AEPrinter first connects to a system. Before the alarms are printed, the line "*** Start of current system alarms" will be output, and after the last alarm is output, the message "*** End of current system alarms" will be printed. If this is not specified, the default is 0. |
| FormatString (REG_SZ) | This format string determines the output format of the message. The format characters are listed in the table at the bottom of this page. The default for this key is "%**%**%A %E1 %D %T- %>%S, %M (%C0)". |
| WrapOnChars (REG_SZ) | A string containing all the characters on which the formatting code should perform a word-wrap break. Default is " ". |
| EOLString (REG_SZ) | This value specifies what combination of CR/LF should be used on the end-of-line sent to the printer. C is used to designate CR and L is used for LF. The default is "CL". |
| UserName (REG_SZ) | Username to use to log into ClearSCADA. |
| Password (REG_SZ) | Password to use to log into ClearSCADA. |
| Format Character | Description |
|---|---|
| %* | If the current alarm/event is an alarm, print to the output, otherwise print a space. Example: %*# would print "#" if alarm, " " otherwise. |
| %A | Print the word "Alarm" if the alarm/event is an alarm, otherwise print the word "Event". |
| %a | Print the letter "A" if alarm, "E" otherwise. |
| %E0 %E1 | Print the alarm severity description for the alarm/event. If %E1 is specified, pad out after the severity with spaces to the width of the longest severity, to maintain correct formatting. |
| %e0 %e1 | Print the alarm severity of the alarm/event as a number. If %e1 is specified, pad out after the number with spaces to the width of the longest possible number (4 characters). |
| %D | Print the date of the alarm/event in the form DD-MMM-YYYY, the month is in the form "JAN", "FEB" etc. |
| %T | Print the time of the alarm/event in the form HH:MM:SS. |
| %S | Print the object name that generated the alarm/event. |
| %M | Print the alarm/event message. |
| %I | Print the unique cookie associated with the alarm. |
| %C0 %C1 | Print the category description of the alarm. If %C1 is specified, pad out after the severity with spaces to the width of the longest category, to maintain correct formatting. |
| %> | Set this point in the message as a left-justification margin. If a terminal width is specified in the registry, the message is word-wrapped and a new line is started at this margin. |
| %% | Print the "%" character. |
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.