Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Load Events Using LoadRecord and LoadRecords

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Load Events Using LoadRecord and LoadRecords
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
AdamWoodland
AdamWoodland Schneider Alumni (Retired)
Schneider Alumni (Retired)
‎2024-03-25 01:52 AM
0 Likes
0
1315
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
‎2024-03-25 01:52 AM

Load Events Using LoadRecord and LoadRecords

Originally published on Geo SCADA Knowledge Base by AdamWoodland | March 25, 2024 09:52 AM

📖 Home   Back  

 

Overview

Event data can be loaded into the Geo SCADA historian using some database methods:

  • LoadRecord - One event at a time with any freeform/custom text as the event message
  • LoadRecords - Multiple events at a time, supporting multiple objects at the same time, with any freeform/custom text for the event message

The only difference in parameters between these two methods are LoadRecords takes an array of values (even if an array size of 1) whereas LoadRecord just takes a singular value from each parameter.

LoadEncodedRecord and LoadEncodedRecords also exist, the only difference with these is the message parameter for these two methods must be a defined encoded message that allows backend support for internationalisation. The encoded message can be extracted from CDBEventJournal using the EncodedMessage column. Using the encoded message is typically better for moving events between two Geo SCADA systems, whereas the non-encoded messages will be necessary when bringing in event data from other systems.

 

Parameters

Parameter Maps to CDBEventJournal Column Details
Timestamp (Time) RecordTime The time in UTC of the event message for the source of the event (e.g. timestamp from RTU if event is originally sourced from an RTU)
ClassName (String) Category The event category name of the event based on the category name in the table DBEventCategoryDef, not the friendly description seen by users in CDBEventJournal (do a SQL JOIN between those tables if necessary to extract in one go)
ObjectId (Long) Id / Source The valid database object id that the event is to be loaded into
Severity (Long) Severity / SeverityDesc / SeverityValue Database severity between 1 and 1000, ideally should match a valid severity on the target system but will round down to the nearest severity if not matched. Will error if 0 is used.
OPCType (Long) None Bitmask for the OPC-AE event type:

 Bit 1 - Simple

 Bit 2 - Tracking

 Bit 3 - Condition

Bitmask cannot be 0, so unless you specifically need to set the event type suggest just using a value of 1 for the imported events

SCXType (Long) AlarmStateDesc

Shows the alarm state causing the event:

  1. Blank entry
  2. "Alarm Raised"
  3. "Alarm Cleared"
  4. "Alarm Accepted with Comment"
  5. "Alarm Accepted"
  6. "Alarm Removed with Comment"
  7. "Alarm Removed"
  8. "Alarm Disabled"
  9. "Alarm Enabled"
  10. "Alarm Response"
  11. "Alarm Unaccepted with Comment"
  12. "Alarm Unaccepted"
Message (String) Message / EncodedMessage The message shown for the event entry, see above for details on EncodedMessage. Cannot be blank.
UserName (String) User Can be any valid string, including blank.
SeqNo (Long) None Doesn't currently import anything, use Null/Nothing depending on your coding language. A new SeqNo will be generated by the server automatically
CommentNo (Long) None Use 0, no other value supported
ReceiptTime (Time) ReceiptTime The timestamp for the event that the server receives it, for the import typically the same as RecordTime or the current time depending on need
ClientAddress (String) ClientAddress

The IP address of the user that generated a source using string (dotted quads) or as 32-bit unsigned representation of the IP address.

Cannot be blank, use "0" for a blank entry in the event journal else provide a valid IP address

AreaOfInterest (Long) AreaOfInterest Use 0 for "World", else a valid Id for an AOI. Parameter still required if AOI is disabled on your system (just use 0 in this case)
SuppressionType (Byte) SuppressionDesc
  1. Blank entry
  2. "None"
  3. "Consequential"
  4. "Maintenance"

Doesn't cause any suppression to occur, just cosmetic.

 

📖 Home    Back  

Labels:
  • SCADA

  • Telemetry

  • Tags:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA

Author

Biography

AdamWoodland

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.