Geo SCADA 2025 Known Issues

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Geo SCADA 2025 Known Issues
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
sbeadle
Kirk sbeadle Kirk
Kirk
‎2025-10-13 05:41 AM
0 Likes
0
379
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
‎2025-10-13 05:41 AM

Geo SCADA 2025 Known Issues

Originally published on Geo SCADA Knowledge Base by sbeadle | October 13, 2025 02:41 PM

Home  Back  
Please read the information below prior to installing Geo SCADA Expert 2025 for important information on any known issues.

 

Running ViewX on Windows Server 2025

  1. When running ViewX directly on Windows Server 2025, the default bell sound will not be heard. This is because the Windows SystemSoundsService task is disabled by default. Both this task and the Windows Audio service need to be enabled for the bell sound to function. Alternatively, use the Geo SCADA custom bell sound feature configured in ViewX | File | Options | Alarms and Events, or the configured alarm severity sounds within the Server Configuration tool.
  2. When running ViewX directly in Windows Server 2025, Mimic scripts written using JScript will not run if you switch the Mimic display from Design mode to Run mode. To run the Mimic script, close and then reopen the Mimic in Run mode. This restriction applies only to JScript and this particular operating system.

Python Program Arguments

When calling the Run method, for example Run(Arg1, Arg2) on a Python program in the Geo SCADA database, its program arguments in "geo_scada_args: dict" are in reverse order, such that geo_scada_args["Arg2"] is the first argument. This will be addressed in the next update.

 

Selection of Aveva Enterprise Licensing

Please do not select the Aveva Enterprise Licensing option in the Server Icon Licensing dialog tool if you are not going to use this option, as it may invalidate your license or stop Geo SCADA if the pre-requisite has not been installed. Then you may need to install the pre-requisite to continue.

 

Upgrading a Server Also Running Virtual ViewX Server

If an existing server is running the Geo SCADA Server and the Virtual ViewX Server, you must upgrade both. If you omit to upgrade Virtual ViewX then you will see issues when starting ViewX or creating a Virtual ViewX session.

 

OPC Registration

On a clean installation, the classes for OPCDA, OPCAE and OPCHDA servers are not registered. The user would need to open the Client Configuration dialog and click OK on the configured connection for the OPC classes to be registered. This was changed in 2015 to add support for the Systems.xml file.

 

Web Client Licensing

Licensing for Virtual ViewX Web clients changed in Geo SCADA 2019 and remains the same for Geo SCADA 2025. This note is relevant if you are upgrading from ClearSCADA. Please read the Release Notes of Geo SCADA 2019 for a full explanation of Virtual ViewX licensing.

In brief, Virtual ViewX requires a separately installed Virtual ViewX license for the number of clients per web server. Also the web server itself requires a client license for the database connections - this is sold as a Virtual ViewX web server license.

 

Blurry Maps and/or Lists on high DPI displays using Text Scaling


High resolution displays that are configured to use Text Scaling can result in displays of Geo SCADA's Map Displays and Lists to be noticeably pixelated and blurry. The impact for Map Displays is aesthetic only and should not impact usability, however applying non-standard scaling impacts the display of Lists because the table content becomes too wide for the column width, obscuring some content from view.

 

Home  Back  

  • Tags:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
  • Telemetry and SCADA

Author

Biography

sbeadle

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.