Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 06:42 PM
Geo SCADA Expert 2025 - Schneider Electric, Remote Operations, announces the release of EcoStruxure Geo SCADA Expert 2025, the newest version of our successful SCADA Host software. Geo SCADA Expert 2025 has support for new features in Realflo software. There's a new MQTT Sparkplug Publisher historian feed to any Sparkplug host application and a new Python programming and run-time system for extending Geo SCADA functionality. New security features include TLS and DTLS encryption and authentication for DNP3, Modbus and IEC60870 protocols. Our Geo SCADA Mobile application has been extended to support the same mimic and trend graphics as ViewX. We also have a new web component designed for use within AVEVA UOC (OMI Web) systems.
There are smaller changes, including to ViewX mimic editing and new embedded trend sparklines.
Ethernet/IP Driver -- supporting Allen Bradley devices with tag browsing
Extended Mobile Functionality -- adding Search, execute Methods such as RTU refresh
Realflo -- support 6.96 and 7
SCADAPack
SCADAPack E -- Support more SCADAPack E functions
New Networking Features
Configurable Tab names -- for mimic and trend displays
Automatic Database Backup - on upgrade
Database Performance Displays -- enable customers to find 'noisy' data sources
Virtual ViewX File Download -- document download from web clients
Permissions for Permanent Standby Servers -- enhanced security
Redirect Alarm to Method by User
Independent Communications (for IP devices)
IIS WebX Server Separation
Security Certificates
ClearSCADA 2017 Bringing increased efficiency in remote asset management, ClearSCADA 2017 is a major release that delivers a new level of functionality for geographically dispersed infrastructure, helping customers to unlock the geo-locational power of their SCADA assets, with the introduction of innovative location services and mapping integration.
SCADA Expert ClearSCADA 2015 R2 Game-changing Performance & Scalability. ViewX Enhancements for Improved Usability. Improved Driver Functionality. Trending Options & Enhancements.
SCADA Expert ClearSCADA 2015 R1.1 New ribbon buttons to easily locate the active document/object within the Database or OPC Explorer bar. Improved mimic load times, including improvements to embedded mimics and object references. Improved user interface responsiveness whilst loading a mimic. Improved behavior of embedded mimic cache.
SCADA Expert ClearSCADA 2015 R1 New WebX User Interface. Increased Template Efficiency via Expressions. Client Access Control Lists. Enhanced Alarm Summary Information. Enhanced Support for O&G Flow Computers. Enhanced User Account Security. Direct Mapping of DNP3-to-Modbus Master/Slave Addresses on SCADAPack E RTUs. Enterprise Software Integration to Wonderware Historian.
SCADA Expert ClearSCADA 2014 R1.1 Added the ability for ViewX users to disable Client Side Automation. Expanded list of object References to include Data References. Implemented forced log-off of active users when their User Account is disabled. Client translations for French and Chinese are now available within the installer. SCADAPack Realflo 6.90 (Liquids).
SCADA Expert ClearSCADA 2014 R1 New User Interface ClearSCADA 2014 R1 delivers a completely redesigned User Interface, leveraging the latest technology to improve the user experience and increase overall efficiency. Internal point calculations have been simplified, providing an alternative to the complexity of logic for simple calculations or internal data transfer. A Bulk Editing tool has been included that interfaces with ClearSCADA to simplify mass changes to the database, including template property overrides. ClearSCADA 2014 R1 adds another dimension to trending, providing a new 3D (X-Y-Z) plot. ClearSCADA 2014 R1 provides a new data set (like a table or grid) that works with your templates, delivering automated expansion as your database grows. ClearSCADA 2014 R1 continues its close integration with the rest of the Telemetry family, providing support for the new SCADAPack535E Smart RTU, and the SCADAPack50 Wireless Data Logger. ClearSCADA's SNMP driver has been enhanced to Version 3
SCADA Expert ClearSCADA 2013 R2.2 Improved historic data synchronization. Enhanced system diagnostics. More secure signing algorithm for self-signed certificates. Diagnostics information removed from WebX for increased security. Selected of minimum supported HTTPS protocol for increased security.
SCADA Expert ClearSCADA 2013 R2.1 Faster mimic load times because of batched loading of embedded mimics from the server. Alarm bell can now be sounded by embedded alarm lists. Improvements to the request timeout settings on OPC driver. Support for parameter trip sequences in Crystal Reports. Support for SQL Server 2008 in the OLE DB driver
SCADA Expert ClearSCADA 2013 R2 Enhanced Data Visualization - automated data collection management, XYZ Plots. Enhanced Security - restricted access to sensitive system information, configurable listen ports when performing 'Server Browse', confirmation on ViewX close. Enhanced Operational Intelligence - Aquis Integration, SCADAPack 50 driver, T-Box driver, enhancements to DNP3 driver, support for version 3 in the SNMP driver, bulk modification of historic data.
SCADA Expert ClearSCADA 2013 R1.1 Ability to use Windows Authentication with usernames that do not follow SCADA Expert ClearSCADA user naming conventions (allowing dots, numeric only usernames etc.). Ability to display graphs on server that is still in "Synchronising History" state. Support for passwords with semicolons in the ODBC connection string. Improved diagnostics in historian file handling. New "Thread Exec Count" field in 'Standby Links' to monitor thread activity. New fields added to IEC60870-5 Slave Outstation to control data returned with timetag.
SCADA Expert ClearSCADA 2013 R1 ClearSCADA is now part of the StuxureWare software applications and suites - to drive business performance while conserving enterprise resources. Continued value in WWW - new wastewater starter application project and best-practices design guide. Improved engineering efficiency through simplicity and productivity - support for SCADAPack E IEC61131-3 Target 5, new TRSS device symbol library. Improved operational efficiency through increased system performance - ClearSCADA Mobile, integrated server backup, improved mimic drawing performance, historian scalability and trending. Continued value in O&G - Dynacard Export tool, Schneider Electric Pump off Controller driver.
ClearSCADA 2010 R3.2 Enabled alarm bell for alarm list windows outside the alarm banner. Introduced additional filter indicator for alarm banner and made both indicators configurable, allowing users to see if the banner is filtered, has had its filter modified, or both, or neither. Added extended database lock diagnostics. Updated the SAP Crystal Reports runtime for .NET Framework 4 to support pack 10. Updated Microsoft Visual C++ 2010 redistributables from version 10.0.40219.1 to version 10.0.40219.325. Updated Signing Algorithm for Self-Signed Certificates.
ClearSCADA 2010 R3.1 Alarm Bell added to embedded alarm lists. Historic capabilities added to Schneider Electric Wade 310 driver points. Editable trace line width for ad hoc trends in WebX. Configurable timeout fields added to the OPC driver for control and refresh requests. Options added to CFX Export object to enable user to export partial hour records and daily data.
ClearSCADA 2010 R3 The limit on User Groups and Areas of Interest removed, use of special characters, case sensitive User Names optional. Maintenance Themes -- use of intermediate web certificates now possible, support for Crystal Reports 2011, new methods for client-side scripting. Data Access Improvements -- support for new SQL 2008 expression and numeric functions, new EcoStruxure Web Services interface, query processor enhancements. Driver Developments -- new Advanced Modbus driver, Lufkin SAMS Pump off Controller added, greater flexibility with On-Demand Support in Advanced Modbus, improvements in the IEC 60870 driver. User Interface -- Embedded Web Pages, Chinese added as a supported language, French translation upgraded.
ClearSCADA 2010 R2.1 This release of ClearSCADA contains a number of product enhancements, including: Improved processing of replies to E-Mail redirections. Improved support for SMS messages sent across carriers. Configurable settings for trace line width of new traces. New function added to client-side scripting to navigate to a document on another head. New command line option added to configure ViewX registry settings. Extended use of Dictionary file translations to custom menus, tooltips, extra alarm columns etc.
ClearSCADA 2010 R2 - ClearSCADA has been rebranded under Schneider Electric in this new version. This version also includes numerous performance, scalability and security improvements, support for the Water Industry Telemetry Standard (WITS - available in the UK only) for DNP3, support in the E-Series RTU driver for new features in the 7.82 firmware version, conformance tested DNP3 slave driver etc.
ClearSCADA 2010 R2.1 - service pack containing fixes and improvements to the product.
ClearSCADA 2010 R1 - this major version adds support for new features such as Linked Database tables, Autosol integration, SQL Export capability, Crystal Reports 2008 support, Database Change Auditing, DNP3 security, Windows authentication, a new Trio Diagnostics driver, consequential alarms support and much more...
ClearSCADA 2010 R1.1 - service pack containing fixes and improvements to the product.
ClearSCADA 2010 R1.2 - service pack containing fixes and improvements to the product.
ClearSCADA 2009 R2 - this minor version contains support for new features such as facilities for creating ad-hoc trends in both ViewX and WebX, an SMS command processor, native OLE DB provider, support for Control Microsystems SP330E/SP334E RTUs and Trend Data Recovery in SCADAPack E-Series, support for Eavesdrop operation in SCADAPack Modbus driver, Multi-Site aware WebX hyperlinks, support for up to 5 Partner servers and more...
ClearSCADA 2009 R2.1 - service pack containing numerous improvements to security and performance.
ClearSCADA 2009 R2.2 - service pack containing numerous fixes, performance improvements and adds support for Windows 7, Windows Server 2008 R2 and Internet Explorer 8.
ClearSCADA 2009 R2.3 - service pack containing numerous fixes and improvements.
ClearSCADA 2009 R2.4 - service pack containing some improvements and fixes to the product.
ClearSCADA 2009 R1 - this version contains numerous new features such as 64 Bit Operating System Support, Integration of Kepware OPC Driver, new .Net API, Pager SMS and UCP Support, E-Series Configuration Download support, FloCal Export object, Read only Permanent Standby, Dynamic Metadata etc.
ClearSCADA 2009 R1.1 - service pack containing fixes and improvements to the product to provide improved performance, stability and compatibility with non-English operating systems.
ClearSCADA 2009 R1.2 - service pack containing fixes and improvements to the product.
ClearSCADA 2009 R1.3 - service pack containing numerous improvements to security and performance.
ClearSCADA 2009 R1.4 - service pack containing numerous fixes and improvements.
ClearSCADA 2007 R1 - this version contains support for Windows Vista, Crystal Reports XI Release 2, a new command executor, native custom table support and numerous enhancements to performance, security, user interface and communications drivers.
ClearSCADA 2007 R1.1 - service pack allowing upgrades of redundant servers without system shutdown.
ClearSCADA 2007 R1.2 - service pack for ClearSCADA 2007 R1 containing numerous fixes and improvements.
ClearSCADA 2007 R1.3 - service pack for ClearSCADA 2007 R1 containing numerous fixes and improvements in security.
ClearSCADA 2007 R1.4 - service pack containing numerous improvements to security and performance.
ClearSCADA 2007 R0 - a major ClearSCADA release containing new drivers (RealFLO support for SCADAPack Modbus Driver, IEC 60870-5-101 and 104, Siemens S7), localization support and numerous performance improvements. Also includes many other new features and general product improvements.
ClearSCADA 2007 R0.1 - a service pack for ClearSCADA 2007 R0
ClearSCADA 2005 R1 - This release includes improvements to the SCADAPack Modbus driver, emf image support and general performance improvements.
ClearSCADA 2005 R0 - ClearSCADA is launched with the release of ClearSCADA 2005 R0. Along with all the expected features of a high end SCADA software, ClearSCADA 2005 R0 contains native support for Control Microsystems SCADAPack hardware through the SCADAPack Modbus Driver.
Go: Home Back
More Links:
SCADA Expert ClearSCADA 2013 R1.2
ClearSCADA 2007 R0
ClearSCADA 2007 R0.1
ClearSCADA 2007 R1.2
ClearSCADA 2007 R1.1
SCADA Expert ClearSCADA 2014 R1
SCADA Expert ClearSCADA 2013 R1.1a
ClearSCADA 2009 R2.4
ClearSCADA 2010 R1
SCADA Expert ClearSCADA 2013 R1.1
ClearSCADA 2005 R1
ClearSCADA 2005 R0
ClearSCADA 2007 R1
SCADA Expert ClearSCADA 2014 R1.1
ClearSCADA 2007 R0.2
ClearSCADA 2009 R2.2
SCADA Expert ClearSCADA 2015 R1
ClearSCADA 2009 R1.4
ClearSCADA 2009 R2.3
ClearSCADA 2009 R2.1
ClearSCADA 2009 R1.3
ClearSCADA 2010 R2
SCADA Expert ClearSCADA 2015 R2
ClearSCADA 2010 R3
ClearSCADA 2017
ClearSCADA 2007 R1.4
SCADA Expert ClearSCADA 2013 R2.1
SCADA Expert ClearSCADA 2013 R2.2
ClearSCADA 2010 R1.1
ClearSCADA 2009 R2
ClearSCADA 2010 R2.1
ClearSCADA 2009 R1
SCADA Expert ClearSCADA 2013 R2
ClearSCADA 2010 R1.2
ClearSCADA 2009 R1.1
ClearSCADA 2010 R3.2
ClearSCADA 2007 R1.3
ClearSCADA 2009 R1.2
ClearSCADA 2010 R3.1
SCADA Expert ClearSCADA 2015 R1.1
SCADA Expert ClearSCADA 2013 R1
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.