Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Modbus

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Modbus
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 09:41 AM
0 Likes
0
1036
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
‎2021-06-09 09:41 AM

Modbus

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 06:41 PM

📖 Home  Back  

 

How Fast can I Scan Modbus?

Problem

  • I’d love to use a modern protocol like DNP3 with its intelligent report on change, but I’m stuck with Modbus which I must scan quickly to make sure I catch changes.
  • How fast can I scan the devices – what are the limitations?
  • I read that there are limits to data rates caused by the size of historic files, such as 15 second data, but I need to read data quicker than that.

Response

We are careful to state limits because there are so many variables. It’s useful to review our Software Performance Guidelines document to help understand the process. Please see the Geo SCADA Expert Performance Guidelines document for details. Link.

 

Driver Scan Rate

An important point is that the driver itself has few limitations on how fast the scanning is set up for. You can set it fast, and it becomes self-limiting because it can’t start a new scan until the old one has completed. The scan interval is the time between the end of the last scan and the start of the next. Therefore, the scan times of 1 second or shorter are possible.

For Advanced Modbus, the scan times are defined with the term 'Retrieval Interval' and are defined on the outstation object, with the selection of interval on the points:

sbeadle_0-1741104374696.png

 

For fast scanning to be useful, what we want to do is limit the data coming out of the driver process and into the server’s database. This is where the database gets potentially overloaded with non-useful data, and by the same reason the users are overwhelmed with it too. Note also that the Promoted scan rates may need to be changed, depending on whether you wish to enable 'Promote when displaying points', a feature which can accelerate scanning for devices on displayed mimics. This feature is enabled on the outstation object's 'Direct' tab.

Point and Device Configuration

To stop the driver from reporting no-change or little-change of analogues to the server, which then gets to the historian for processing, you can use the Advanced driver’s Deadband setting:

sbeadle_1-1741104429156.png

 

This will filter noise from the signal. You can also use the Hysteresis setting (and Persistence below it) to reduce the affect of noise causing alarm transitions which are load-intensive for value and event history:

sbeadle_2-1741104446526.png

 

Confidence Polling

The other area for consideration is the Confidence Poll. These are timed polls which ALWAYS cause data processing and storage. These MUST be configured for their real purpose, which is to provide a value to the database when not much change is happening to give operators confidence that the values are OK. However, you have device alarms and point quality (colour) to tell operators that devices are not healthy, so a good time interval for confidence polling is no more than HOURLY – which may also then be useful for report queries. Configure this on the Channel and the points. The default options for this shown here are very likely to be too fast for good system performance when a large system is set up. In this example use Group 8 which is set up for hourly updates.

sbeadle_3-1741104468838.png

 

 

The screenshot above also shows how the channel configuration has communication statistics update timing, which you may wish to increase for large numbers of devices.

Historian Compression

While it’s possible to use the historian’s compression feature to reduce the number of historic values stored, that does not stop data from being processed into the database as current values. Doing a lot of that will load up the database with noise. But historian compression may still be needed.

sbeadle_4-1741104486877.png

 

The above configuration will help to reduce the amount of noise stored by the historian and affecting historic query and trend display times.



Go: Home Back

More Links:

   Modbus RTU via Terminal Server

   Modbus Dual Ethernet Communications

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.