Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Modbus Dual Ethernet Communications

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Modbus Dual Ethernet Communications
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 02:58 PM
0 Likes
0
1240
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
‎2021-06-09 02:58 PM

Modbus Dual Ethernet Communications

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 11:58 PM

📖 Home  Back  
Modbus can be configured such that two communications paths to a PLC can be configured on a "switched" scheme, meaning that all of the attached scanners (on a channel) will either use the first configured path or the second.

The driver architecture that the Modbus driver is built on uses one thread per channel. Scanners attached to a channel are scanned in sequence, one scan must end before the next can start. Even if the Modbus scanners on a single channel in the configuration had the connections spread between addresses one and two, the scans would still be synchronized, this meaning that even though requests are being shared between two connections, the overall time it takes to complete all the scans would be unchanged. The network usage would look something like this:

'#' means in use'.' means idle1: ##...#..##...2: ..###.##..###


Bandwidth is shared between the two links, but overall Modbus scan performance is not improved.

To improve the performance and throughput to a PLC, there are a couple of things that can be done. The first option involves using multiple channels. This immediately allows multiple concurrent connections to the PLC allowing more data to be transferred between the SCADA and PLC.

To allow load sharing on the network, for every second channel to a PLC, switch the primary and secondary IP addresses around on these scanners, so that address 1 becomes address 2. This way one channels primary address would be on one link, the other on the other link. So by default, the scanning load would be shared between the two networks. On link failure, all of the scanners would switch onto the same link, it would then be a manual exercise (or a FBD or ST Logic program to perform this automatically) to switch the channel back to primary when the network issues have been resolved.

Using 2 channels as described above will give the following:

Channel 1 path A (Address 1): ##########Channel 1 path B (Address 2): ..........Channel 2 path A (Address 2): ##########Channel 2 path B (Address 1): ..........


You can have scanners for different PLC's on one channel. A channel will make one TCP connection for every unique address configured in it's scanners, scanners with the same address sharing the same connection.

To get multiple connections to the same PLC, split the scanners between multiple channels. This will give one connection per PLC per channel. The more channels you have, the more connections you get.

Path switching is determined by how many scanners on a channel have failed. This is configurable in the channel as "Switch after n scanners have failed", zero meaning that only switch if all scanners fail. Switching doesn't care what IP addresses the scanners are connecting to, it just goes from A to B (or back) when N have failed. The idea was that N PLC's may be configured on just two physical networks, and if one network fails, all the PLC's need to be switched to the other network. Finer granularity of switching can be achieved by introducing more channels and splitting the PLC's between them.

Automatic switching will only occur if at least one of the paths was determined "healthy". This is determined as "More scanners were polled successfully than the "Switch after n scanners have failed" of the channel". This is to prevent the link continuously switching between the two links.

Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.