Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
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
  • About Sven_Ortmann
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Sven_Ortmann
Sven_Ortmann
Schneider Alumni (Retired)
‎2023-10-09
487
Posts
53
Likes Received
41
Likes Given
3
Solutions

Community Badges

Open Hailing Frequencies - L7
Resistance is Futile - L7
Open Hailing Frequencies - L6
Resistance is Futile - L6
+19
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

Difference between cumulated and normal energy?

Hello, I was wondering about the difference between cumulated and normal energy at some Meters? Maybe there is a quick and possible answere 🙂
EcoStruxure Power & Grid icon_circle Metering & Power Quality
3383 0 3

2020-01-07 06:54 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

ION7650 https certificate / disable http

Customer needs to disable http on ion 7650. Is it possible to switch to https with certificate?Any documentation? Thanks
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1063 0 1

2019-10-30 07:26 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

PM8000 Standalone sending Alarm E-Mails

Hello, a customer wants to configure several pm8000 devices to send alarm emails through smtp server to a local e-maiil adress. We didn't find where t...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1112 0 1

2019-09-30 03:08 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

ComX 510 IP or Slave routing - remote device connection

Hello, Is it possible to forward IP or Slaves remote device connection with the help of an ComX510. With the old EGX300 it was possible to forward Sla...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
860 0 1

2018-12-19 05:19 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

PM5563 IP Range Problem

Hello, I do have problems setting an IP adress with in the END 255 e.g. 192.168.254.255 This could not be set and the meter sends an error "unsupporte...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
984 0 1

2018-11-14 10:42 PM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

PM5320 no Ping an no changes in ION Setup possible

Hello,customer does have many PM5320 Meters. For the network team it is not possible to ping the devices.PROBLEM 1: static ip address will only be app...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2288 0 4

2018-08-30 05:02 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

Problems with PM8000 using as a Modbus Master Gateway for Serial devic...

Customer wants to use 3x PM8000 device as a master gateway for different slave meters. The problem is we cant get a connection to the modbus slaves.Al...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1980 0 1

2018-03-02 02:59 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

Is it possible to configure a Com'X510 like a ION meter in case of com...

Hello,by using a ion meter with internal storage the historical data is first stored on the device and always visible in case there is a communication...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1249 0 3

2018-02-26 05:09 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

PM5560 Digital Input & Digital Output Problems

Hello,I need to read the DI of some PM5560 devices and implement it to DCEBut it seems there are some troubles.1) Web status and software status is no...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1256 0 1

2018-01-09 03:30 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

ion8650 periodically lan network reset

Hello,we have problem with ion8650 and periodically lan network reset. The meter works as it should but since 2 weeks the network connection is lost ....
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1092 0 1

2018-01-08 06:05 AM

Sven_Ortmann
Sven_Ortmann Schneider Alumni (Retired)

EGX 150 Pin occupancy RJ 45 to RS-485

Hello,with the change from EGX100 to EGX150 RJ45 also the connection port changes. A customer wants to connect a symmetra mw with modbus serial. Which...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1751 0 6

2017-11-14 12:35 AM

Activity Feed
  • Liked Re: Difference between cumulated and normal energy? for DanL. ‎2020-01-07 11:10 PM
  • Liked Re: Difference between cumulated and normal energy? for Romain_Polette. ‎2020-01-07 11:10 PM
  • Posted Re: Difference between cumulated and normal energy? on Metering & Power Quality. ‎2020-01-07 06:54 AM
  • Posted Difference between cumulated and normal energy? on Metering & Power Quality. ‎2020-01-07 06:54 AM
  • Posted ION7650 https certificate / disable http on Metering & Power Quality. ‎2019-10-30 07:26 AM
  • Posted PM8000 Standalone sending Alarm E-Mails on Metering & Power Quality. ‎2019-09-30 03:08 AM
  • Posted ComX 510 IP or Slave routing - remote device connection on Gateways and Energy Servers. ‎2018-12-19 05:19 AM
  • Posted PM5563 IP Range Problem on Metering & Power Quality. ‎2018-11-14 10:42 PM
  • Posted Re: PM5320 no Ping an no changes in ION Setup possible on Metering & Power Quality. ‎2018-08-31 12:22 AM
  • Posted PM5320 no Ping an no changes in ION Setup possible on Metering & Power Quality. ‎2018-08-30 05:02 AM
  • Posted Re: How to upgrade PM5320 firmware on Metering & Power Quality. ‎2018-08-29 09:07 AM
  • Posted Re: PM8000 V2 firmware available!! on Metering & Power Quality. ‎2018-03-20 02:35 AM
  • Liked Re: PM8000 V2 firmware available!! for Abdel. ‎2018-03-20 02:31 AM
  • Posted Re: PM8000 V2 firmware available!! on Metering & Power Quality. ‎2018-03-06 02:47 AM
  • Posted Problems with PM8000 using as a Modbus Master Gateway for Serial devices in PME on Metering & Power Quality. ‎2018-03-02 02:59 AM
  • Posted Re: PM8000 V2 firmware available!! on Metering & Power Quality. ‎2018-03-01 11:32 PM
  • Posted Re: Is it possible to configure a Com'X510 like a ION meter in case of communication loss on Gateways and Energy Servers. ‎2018-02-26 05:19 AM
  • Posted Is it possible to configure a Com'X510 like a ION meter in case of communication loss on Gateways and Energy Servers. ‎2018-02-26 05:09 AM
  • Got a Like for How can i set E-Mail notification when Voltage is +-10?. ‎2018-02-19 01:44 AM
  • Posted PM5560 Digital Input & Digital Output Problems on Metering & Power Quality. ‎2018-01-09 03:30 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.