Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84783members
354228posts

PM5560 Digital Input & Digital Output Problems

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Sven_Ortmann
Commander Commander
Commander
0 Likes
1
269

PM5560 Digital Input & Digital Output Problems

Hello,

I need to read the DI of some PM5560 devices and implement it to DCE

But it seems there are some troubles.

1) Web status and software status is not the same at digital Input

2) I installed newest firmware 2.4.3 but suddenly all DIs are "off"

and DOs are "on"  -> but nothing is connected to DOs

by reading the modbus registers starting at 8915 the result is:

from the modbus register list:


Accepted Solutions
Ramasamy_N
Commander Commander
Commander

Re: PM5560 Digital Input & Digital Output Problems

Hello @Sven_Ortmann , 

 

Is this query still open?

 

If Yes, can you please suggest to upgrade the latest firmware and check this behavior? 

 

Firmware download path: https://www.se.com/ww/en/download/document/PM5560_PM5563_V2.7.4_Release/

 

Regards, 

Ramasamy N

See Answer In Context

1 Reply 1
Ramasamy_N
Commander Commander
Commander

Re: PM5560 Digital Input & Digital Output Problems

Hello @Sven_Ortmann , 

 

Is this query still open?

 

If Yes, can you please suggest to upgrade the latest firmware and check this behavior? 

 

Firmware download path: https://www.se.com/ww/en/download/document/PM5560_PM5563_V2.7.4_Release/

 

Regards, 

Ramasamy N