• About Robert_Lee
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Robert_Lee
Robert_Lee
Admiral
‎2025-11-27
369
Posts
201
Likes Received
1
Like Given
108
Solutions

Community Badges

Open Hailing Frequencies - L7
Mind Meld - L7
Live Long and Prosper - L6
Open Hailing Frequencies - L6
+23
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Helpful Links for ION Setup, templates, firmware, etc.

Most files should be available via search from the main Schneider Electric web site using: Download Schneider Electric Alternatively, you might find u...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2565 2 2

2015-08-04 08:54 AM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Advanced Security Password Updater for ION devices

A new feature has been implemented in the past few builds and I think it is now ready to be rolled out (get the latest version from here in the Instal...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1454 0 0

2014-03-31 10:41 AM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

How to change PM8xx data log file mode

The default setup file doesn't support the modification of the data log file mode but this functionality can be manually added to the file using the f...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1521 0 0

2014-01-29 12:32 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Why does my ION Setup run so slow now?

I've recently been getting reports of the newest versions of ION Setup having some performance issues to the point where its taking minutes sometimes ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1605 1 0

2013-09-18 01:32 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Using the Modbus Tester User Interface within ION Setup

ION Setup V3.0 now has a built-in Modbus Tester interface allowing reading/writing of a device's Modbus registers using the standard Modbus RTU comman...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1730 0 0

2013-02-28 10:13 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Modifying an external module output using ION Setup

The three external class modules (Boolean/Pulse/Numeric) have certain outputs which can be used to control ION framework operation. Previously, users...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1220 1 0

2013-02-28 09:24 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

How to get ION Setup to allow a serial COM port higher than 16

By default, ION Setup allows users to select serial COM ports between 1 and 16. If required, users can modify the IONSETUP.INI file to allow access t...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1161 0 0

2013-02-28 07:44 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

USB to isolated RS-485 converters for use with ION Setup/SPM

B&B Electronics USOPTL4-LS Inline USB to Serial Converters - B&B Electronics Note: Ensure DIP Switch 2 is ON (Echo OFF) for proper operation. Nationa...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1821 0 1

2013-02-28 07:06 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

How to connect an ION module's input to a setup register using ION Set...

Certain ION modules will allow inputs to be connect to another module's setup register (ex. Nominal Voltage in the Sag/Swell module). Most common app...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1951 0 2

2013-02-28 06:49 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

ION Setup introduces transmit delay throttling to decrease ION firmwar...

ION Setup 3.0 Build 13052.01 introduces measured comm performance which will periodically decrease the specified transmit delay in an attempt to decre...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
4418 0 10

2013-02-28 04:28 PM

Robert_Lee
/html/rank_icons/Admiral.png Robert_Lee /html/rank_icons/SE-Employee.png

Using ION Setup to collect ION logged data for SPM/ION EEM

In instances where automated (either direct or via modem) communication channels between the SPM server and the remote device isn't available, ION Set...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
7842 5 17

2013-02-28 03:46 PM

Activity Feed
  • Posted Re: How to update firmware for multiple PQMs on Metering & Power Quality. ‎2025-11-18 01:45 PM
  • Got a Like for Re: PowerLogic Ion 8650 Offline Meter Data Report. ‎2025-10-23 09:34 PM
  • Posted Re: EPC communications test report on Metering & Power Quality. ‎2025-08-07 01:58 PM
  • Posted Re: PM5560 Connection Issue with ION Setup on Metering & Power Quality. ‎2025-08-07 01:50 PM
  • Got a Like for Re: PM5560 Connection Issue with ION Setup. ‎2025-08-06 09:29 PM
  • Posted Re: PM5560 Connection Issue with ION Setup on Metering & Power Quality. ‎2025-08-05 04:19 PM
  • Posted Re: i Remote PM800 comm issue on Metering & Power Quality. ‎2025-08-05 04:12 PM
  • Posted Re: ION Setup Waveform Log Timestamp Issue on Metering & Power Quality. ‎2025-08-05 04:03 PM
  • Posted Re: DLF3000 Install error on Metering & Power Quality. ‎2025-05-29 12:55 PM
  • Got a Like for Re: ION9000 VT wiring and meter config Question. ‎2025-02-25 04:27 PM
  • Posted Re: ION9000 VT wiring and meter config Question on Metering & Power Quality. ‎2025-02-25 09:51 AM
  • Posted Re: PM5320 Modbus TCP on Metering & Power Quality. ‎2025-02-12 10:19 AM
  • Posted Re: EM1000 meter communication on Metering & Power Quality. ‎2025-01-28 11:36 AM
  • Got a Like for Re: Load Profile Clock always in GMT, how to change?. ‎2024-11-15 08:01 AM
  • Posted Re: conzerv EM6436 energy meter not communicating with Modbus on Metering & Power Quality. ‎2024-11-13 10:17 AM
  • Posted Re: IEM3255 and KepServer EX setup on Metering & Power Quality. ‎2024-11-07 09:56 AM
  • Got a Like for Re: iEM3555 : set Wiring command number 2000. ‎2024-11-05 04:13 PM
  • Posted Re: iEM3555 : set Wiring command number 2000 on Metering & Power Quality. ‎2024-11-05 12:31 PM
  • Posted Re: IEM3255 and KepServer EX setup on Metering & Power Quality. ‎2024-11-05 12:26 PM
  • Got a Like for Re: ION9000T HSTC Settings warning in ION Setup when using PTs. ‎2024-10-10 08:46 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.