Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Advanced Security Password Updater for ION devices

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Advanced Security Password Updater for ION devices
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2014-03-31 10:41 AM . Last Modified: ‎2020-04-22 01:51 AM

0 Likes
0
1646
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
‎2014-03-31 10:41 AM

Advanced Security Password Updater for ION devices

A new feature has been implemented in the past few builds and I think it is now ready to be rolled out (get the latest version from here in the Installers/Updated Versions folder):

 

Advanced Secuirty Password Updater

 

This feature allows for complete updating of all Advanced User passwords within all ION devices defined in the system if the user chooses to update them.  Primarily targetting utility applications, I believe it is also applicable for any customer with cyber security concerns/policies in place.

 

The updater can be accessed using the following steps:

 

1.  Highlight the System icon in the network viewer.  Press either the stethoscope icon on the toolbar or select Tools -> Diagnostics from the menu.

2.  Click on the Tools tab and click on the "Advanced Security Password Updater" in the listbox and select Open.

 

A full list of all ION devices defined in the network viewer will be shown.

 

Select all device(s) you wish to update passwords for making sure they are checked and set the user#/password of the super-user for each of those device(s) (the super-user has security rights to modify passwords).  Once all that information has been set, press Start to proceed to entering the new passwords.

 

Next for each defined user, you may enter a new password which will apply to all new devices.

 

NOTE: This feature is meant to only update existing advanced ION security users/passwords.  It will not update their rights/create new users or turn on/off Advanced Security  Use the setup assistant security wizard to accomplish this.

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.