New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Using the Modbus Tester User Interface within ION Setup
Metering & Power Quality
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
2013-02-2810:13 PM
Using the Modbus Tester User Interface within ION Setup
ION Setup V3.0 now has a built-in Modbus Tester interface allowing reading/writing of a device's Modbus registers using the standard Modbus RTU commands.
Commands presently supported are:
Read Input Status (Function code 0x02)
Read Holding Registers (Function code 0x03)
Read Input Registers (Function code 0x04)
Preset Single Register (Function code 0x06)
Preset Multiple Registers (Function code 0x10)
Read General Reference (Function code 0x14)
Read Scattered Registers (Function code 0x64)
Read Device Identification (Function code 0x2B)
Most read functions will display register values only as 16-bit unsigned integers values presently.
To access the tester:
Highlight a device that communicates using Modbus RTU protocol in the network viewer.
Either select from the menu, Tools -> Diagnostics or click on the stethoscope icon on the toolbar.
Click on the Troubleshooting tab and if the device uses Modbus protocol, the first available option should be "Modbus Tester Interface".
Click on the Open button, then select from the droplist the function code you want to perform. Fill out any of the required information and click on the Send button.