Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Modifying an external module output using ION Setup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Modifying an external module output using ION Setup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
526
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2013-02-28 09:24 PM . Last Modified: ‎2020-04-22 01:57 AM

1 Like
0
1242
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
‎2013-02-28 09:24 PM

Modifying an external module output using ION Setup

The three external class modules (Boolean/Pulse/Numeric) have certain outputs which can be used to control ION framework operation.  Previously, users would need to create either a Vista diagram with a linked control object or a custom ION Setup table view to allow control of these outputs, which during framework design/testing is very cumbersome and time consuming.

 

ION Setup V3.0 allows users to directly control these external module outputs using the Advanced ION setup view.

 

  1. Exit any table/dialog and at the network view, display the device properties (either via the Edit menu or right clicking on the device icon).
  2. Click on the Tools tab and switch the Device Setup to "Show Advanced ION Setup" then click on OK.  This should show all the ION module types if viewing the device setup type.
  3. Find the desired external module type and after all the modules are displayed, double click on the one you want to control to bring up the module configuration dialog.
  4. When the module dialog appears, click on the Output Registers tab.  Next, hold down the <Shift> and left click on the first item in the list, a popup menu should then appear.  For External Pulse modules, clicking on the pop-up menu item will pulse the output. External Boolean modules will display a two menu item popup (one with a check mark indicating the present state), clicking on the non-checked menu item will toggle the Boolean state.  External Numeric modules will display the present output value within square brackets and clicking on the menu item will allow you to enter a new value.
Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.