Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM5320 no Ping an no changes in ION Setup possible

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PM5320 no Ping an no changes in ION Setup possible
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Sven_Ortmann
Sven_Ortmann Leader
Leader

Posted: ‎2018-08-30 05:02 AM

0 Likes
4
2643
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
‎2018-08-30 05:02 AM

PM5320 no Ping an no changes in ION Setup possible

Hello,

customer does have many PM5320 Meters. For the network team it is not possible to ping the devices.

PROBLEM 1: static ip address will only be applied after a power off - power on

PROBLEM 2: It is not possible to open ftp://IPAdress  or http://IPAdress

PROBLEM 3: Windows Explorer shows the device at network but the information is strange:

PROBLEM 4: in ION Setup it is not possible to set the ip adress because this point is not visible.

And it is not possible to change the serial parameter from odd to even

With this barcode you can see further informations:

this is the serial number of one of these devices:

firmware seems to be newest one:

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2018-08-31 01:39 AM

1 Like
0
2610
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
‎2018-08-31 01:39 AM

Hello Sven,

Please refer my comments in green,

PROBLEM 1: static ip address will only be applied after a power off - power on

The static IP address will be stored once after configure the IP,sub net,Gateway. It does not required to power off. It may take some time (1 to 2 minutes) to stored the configuration depending on the network traffic. 

-> we were waiting more than 2 minutes but it was not possible to connect, after a power off and on it works with several devices.

-->Please check and update this condition in one meter with a standalone system in same IP settings

PROBLEM 2: It is not possible to open ftp://IPAdress  or http://IPAdress

PM5320 does not support HTTP or FTP protocol

-> how to upgrade firmware for PM5320 without FTP?    

-->PM53xx series meters can be upgrade the firmware using DLF3000 tool.

PROBLEM 4: in ION Setup it is not possible to set the ip adress because this point is not visible.

And it is not possible to change the serial parameter from odd to even

PM5340 com link must be configured as Ethernet devices in ION setup and enter the IP address of device in insert device -> new device page. Serial parameters are applicable only for Serial RS485 devices.

-> so if we need to implement to PME Software, the devices are always IP Adress and ID 255 ?

--> Yes.

Regards,

Ramasamy N

See Answer In Context

Reply
Replies 4
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2018-08-30 08:33 PM

1 Like
2
2610
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
‎2018-08-30 08:33 PM

Hello Sven,

Please refer my comments below,

PROBLEM 1: static ip address will only be applied after a power off - power on

The static IP address will be stored once after configure the IP,sub net,Gateway. It does not required to power off. It may take some time (1 to 2 minutes) to stored the configuration depending on the network traffic.  

PROBLEM 2: It is not possible to open ftp://IPAdress  or http://IPAdress

PM5320 does not support HTTP or FTP protocol

PROBLEM 3: Windows Explorer shows the device at network but the information is strange:

This is know error ans escalated to product owner for fixing in the upcoming release.

PROBLEM 4: in ION Setup it is not possible to set the ip adress because this point is not visible.

And it is not possible to change the serial parameter from odd to even

PM5340 com link must be configured as Ethernet devices in ION setup and enter the IP address of device in insert device -> new device page. Serial parameters are applicable only for Serial RS485 devices.

Regards,

Ramasamy N

Reply
Sven_Ortmann
Sven_Ortmann Leader
Leader

Posted: ‎2018-08-31 12:22 AM

0 Likes
1
2610
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
‎2018-08-31 12:22 AM

Hello Ramasamy N​,

thanky for your comments:

se my new comments

PROBLEM 1: static ip address will only be applied after a power off - power on

The static IP address will be stored once after configure the IP,sub net,Gateway. It does not required to power off. It may take some time (1 to 2 minutes) to stored the configuration depending on the network traffic.  

-> we were waiting more than 2 minutes but it was not possible to connect, after a power off and on it works with several devices.

PROBLEM 2: It is not possible to open ftp://IPAdress  or http://IPAdress

PM5320 does not support HTTP or FTP protocol

-> how to upgrade firmware for PM5320 without FTP?

PROBLEM 3: Windows Explorer shows the device at network but the information is strange:

This is know error ans escalated to product owner for fixing in the upcoming release.

-> thanks

PROBLEM 4: in ION Setup it is not possible to set the ip adress because this point is not visible.

And it is not possible to change the serial parameter from odd to even

PM5340 com link must be configured as Ethernet devices in ION setup and enter the IP address of device in insert device -> new device page. Serial parameters are applicable only for Serial RS485 devices.

-> so if we need to implement to PME Software, the devices are always IP Adress and ID 255 ? 

Regards,

Sven

Reply
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2018-08-31 01:39 AM

1 Like
0
2611
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
‎2018-08-31 01:39 AM

Hello Sven,

Please refer my comments in green,

PROBLEM 1: static ip address will only be applied after a power off - power on

The static IP address will be stored once after configure the IP,sub net,Gateway. It does not required to power off. It may take some time (1 to 2 minutes) to stored the configuration depending on the network traffic. 

-> we were waiting more than 2 minutes but it was not possible to connect, after a power off and on it works with several devices.

-->Please check and update this condition in one meter with a standalone system in same IP settings

PROBLEM 2: It is not possible to open ftp://IPAdress  or http://IPAdress

PM5320 does not support HTTP or FTP protocol

-> how to upgrade firmware for PM5320 without FTP?    

-->PM53xx series meters can be upgrade the firmware using DLF3000 tool.

PROBLEM 4: in ION Setup it is not possible to set the ip adress because this point is not visible.

And it is not possible to change the serial parameter from odd to even

PM5340 com link must be configured as Ethernet devices in ION setup and enter the IP address of device in insert device -> new device page. Serial parameters are applicable only for Serial RS485 devices.

-> so if we need to implement to PME Software, the devices are always IP Adress and ID 255 ?

--> Yes.

Regards,

Ramasamy N

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2018-08-31 07:43 PM

0 Likes
0
2610
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
‎2018-08-31 07:43 PM

ION Setup is unable to program IP information as it is not readily available via Modbus.

As for the "Unable to gain device setup access" error dialog, this likely indicates someone has setup access via the front panel (or thru communications by obtaining the setup semaphore).
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.