Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84784members
354230posts

PM8000 V2 firmware available!!

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Daniel_Brandao
Lt. Commander Lt. Commander
Lt. Commander
15
1883

PM8000 V2 firmware available!!

Hello everyone,

It’s our pleasure to announce that we have officially released the PM8000 V2 firmware!  As a reminder, this firmware update is bringing the following main features:

  • Waveform on webpages
  • IPV6 and DHCP support
  • 10MB logging limit removal
  • Cyber security enhancements

The firmware files and "what's new" document is available in the "Firmware Releases" community space.

The PM8000 guidebook is being updated with the new tehnical and marketing documentation to support this release. Please allow us until early next week to finish this task.

Please let me know if any questions. We count on you to keep growing the Advanced Metering business!!

Daniel

15 Replies 15
Sven_Ortmann
Commander Commander
Commander
0 Likes
0
1598

Re: PM8000 V2 firmware available!!

Hello Daniel,

I didn't find the download for V2 ?

Can you please send me the download link?

Thank you

Fabricio
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0
1598

Re: PM8000 V2 firmware available!!

Hi Sven,

The actual firmware version is 1.4.1, The V2 naming came out as a second major release of meter functionalities. All the new features are described on Daniel's posting and the What's new document on the page you just highlighted.

Please let us know if you have any issue downloading or using the new firmware release.

Fabricio

Daniel_Brandao
Lt. Commander Lt. Commander
Lt. Commander
0
1598

Re: PM8000 V2 firmware available!!

AmyRizner
Ensign Ensign
Ensign
9
1598

Re: PM8000 V2 firmware available!!

Sven_Ortmann
Commander Commander
Commander
0 Likes
8
1598

Re: PM8000 V2 firmware available!!

Hello Sorry what is the difference between meter framework510 and PQ ?

An which one should I use?

Why is all the meter data deleted with the firmware upgrade?

AmyRizner
Ensign Ensign
Ensign
0 Likes
4
1598

Re: PM8000 V2 firmware available!!

Hi Sven,

You should probably contact Technical Support so they can help you.

Sven_Ortmann
Commander Commander
Commander
0 Likes
3
1598

Re: PM8000 V2 firmware available!!

I do have a case since last year:

Case 44623062

Tom_Stevenson
Picard Picard
Picard
0 Likes
0
1598

Re: PM8000 V2 firmware available!!

Hi Sven - the 519 framework would be used if you want to utilize the "Harmonics Compliance" report in PME.  It does IEEE519 at the expense of EN50160, however, so if you need the latter, use the PQ framework (and the default one).

Meter data is not persisted upon a firmware upgrade, hence the recommendation to ensure your logs are caught up prior to the upgrade.


Tom

Abdel
Lieutenant Lieutenant
Lieutenant
1
1598

Re: PM8000 V2 firmware available!!

Hi Sven,

as we could find out last friday. the Problem was that the Pm8000 was not configured properly.

As is remotely change only two settings we got the PM8000 working.

It was your mistake.

Sven_Ortmann
Commander Commander
Commander
0 Likes
0
1598

Re: PM8000 V2 firmware available!!

very productive input - thank you Abdelatif

engineer_langfo
Lieutenant JG
Lieutenant JG
0 Likes
2
1598

Re: PM8000 V2 firmware available!!

I can't seem to find the .dcf files. 

Is there a link?

engineer_langfo
Lieutenant JG
Lieutenant JG
0 Likes
0
1598

Re: PM8000 V2 firmware available!!

Oh; I found V1.4.3 - All here:

PM8000 Firmware 1.4.3.zip

Robert_Lee
Captain Captain
Captain
0 Likes
0
1598

Re: PM8000 V2 firmware available!!

The DCFs are embedded in the firmware zip file in the links in Daniel Brandao's post above.

Otherwise you can use the following link:

https://schneider-electric.box.com/v/IonSetup

Most DCFs should be available in the ION Templates sub-folder and if there are additional ones you need uploaded, let me know.

Arneil_Dalope
Lt. Commander | EcoXpert Master Lt. Commander | EcoXpert Master
Lt. Commander | EcoXpert Master
1
1574

Re: PM8000 V2 firmware available!!

Hello,

 

I am monitoring this link for any new ION meter firmware release:

 

https://schneider-electric.app.box.com/v/IONFirmware/folder/1251922932

 

I found out from my colleague here that the PM8000 V2.1.0 is now released and can be found here:

 

https://www.schneider-electric.com/en/product/METSEPM8240/powerlogic-pm8000---pm8240-panel-mount-met...

 

Would be good if we have one location for all firmwares and maybe announce it here in the commuinity if there is a new one. 

 

Anyway, we see in "What's New?" that there is a lot of enhancements in this firmware. Good job team!

 

Regards,
Arneil

Matt_Curry
Administrator Administrator
Administrator
0 Likes
0
1559

Re: PM8000 V2 firmware available!!

Thanks for the feedback Arneil.  We are currently looking at improving this aspect and your feedback is valuable as a consumer of this information.  Our current plan is that we would package FW releases with the associated documentation and post on SE.com.  We would then announce via the Exchange Community to point to the latest release.  If you have recommendations on this please let us know.