Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About engineer_langfo
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
engineer_langfo
engineer_langfo
Explorer
‎2023-05-10
52
Posts
6
Likes Received
7
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies - L4
Open Hailing Frequencies - L3
Resistance is Futile - L3
Live Long and Prosper - L2
+8
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
engineer_langfo
engineer_langfo

COM'X 510 WiFi Antenna

We have an application where a customer wants to install the COM'X 510 inside a steel enclosure because the metering point is located in an harsh indu...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
938 0 1

2017-05-25 12:18 PM

engineer_langfo
engineer_langfo

Manager and module list of ION meter in ION Setup

How can a complete list of ION Modules and managers be printed using ION Setup? The objective would be to print a list of modules in ION Setup. Not...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1843 0 4

2017-05-15 07:00 PM

engineer_langfo
engineer_langfo

All register search of ION modules in Meter?

When linking the input to an ION module in Advanced Mode the user needs to search through the modules for the specific input they are looking for. If...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1425 0 2

2017-05-15 06:57 PM

engineer_langfo
engineer_langfo

ION Setup - Enhancement Suggestions

Rob,I have received feedback from some customers with the following suggestions:1. is it possible to sort the Sites in Alphabetical order? 2. Is it po...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1098 0 1

2016-06-07 07:58 AM

engineer_langfo
engineer_langfo

View .XML data from ION Setup?

this question was partially answered in another thread :"Scripting ION Setup for downloading..." However, is there any way to view or extract the .XML...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2101 1 1

2016-06-03 04:30 AM

engineer_langfo
engineer_langfo

USB Driver for ION7400 and ION Setup

I want to connect to the ION7400 via USB port with ION Setup.I am running IONSetup V3.0.16008. - Windows 10 OS.There doesn't appear to be a USB Driver...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1500 0 1

2016-03-23 01:42 PM

engineer_langfo
engineer_langfo

CM4250- ECC21 and PM5000 (PM5330)

Can the ECC21 on an existing CM4250/CM3350 support RS485 communications to the PM5000 series?Customer has existing CM4250 with ECC21 integrated to PME...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2248 0 4

2016-02-01 03:05 PM

engineer_langfo
engineer_langfo

COM'X - serial server??

Does the COM'X 510 or Link150, or one of the gateway devices support a "serial server" mode. Traditionally, with ION meters that we wish to integrate...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1067 0 1

2016-01-18 04:34 PM

engineer_langfo
engineer_langfo

ION8650 clock drift.

Elsewhere It is mentioned: accuracy of the crystal for the ION8600 is 20 parts per million accuracy rated crystal (typical for these types of parts)...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1573 0 1

2015-05-20 12:36 PM

engineer_langfo
engineer_langfo

PM8000 web page

Is there a document that describes how to configure the Web Pages in the PM8000? I notice there is no longer a Web Page Module in the PM8000. Also, ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1858 0 2

2015-05-19 09:32 AM

engineer_langfo
engineer_langfo

QR Code Reader / Scanner

I am having problems scanning the QR Code in the PM5560.I am running: Android V5.1Phone: Nexus 5. I have tried a few different QR Reader apps with n...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
6287 0 9

2015-04-16 09:04 AM

Activity Feed
  • Got a Like for View .XML data from ION Setup?. ‎2021-10-03 09:24 PM
  • Posted Re: PM8000 V2 firmware available!! on Metering & Power Quality. ‎2018-04-09 09:11 AM
  • Posted Re: PM8000 V2 firmware available!! on Metering & Power Quality. ‎2018-04-09 09:04 AM
  • Liked ION 8650 PASSWORD for engenharia_memt. ‎2018-01-15 03:13 PM
  • Posted Re: Manager and module list of ION meter in ION Setup on Metering & Power Quality. ‎2017-05-26 11:21 AM
  • Posted COM'X 510 WiFi Antenna on Gateways and Energy Servers. ‎2017-05-25 12:18 PM
  • Posted Manager and module list of ION meter in ION Setup on Metering & Power Quality. ‎2017-05-15 07:00 PM
  • Posted All register search of ION modules in Meter? on Metering & Power Quality. ‎2017-05-15 06:57 PM
  • Posted ION Setup - Enhancement Suggestions on Metering & Power Quality. ‎2016-06-07 07:58 AM
  • Posted View .XML data from ION Setup? on Metering & Power Quality. ‎2016-06-03 04:30 AM
  • Tagged View .XML data from ION Setup? on Metering & Power Quality. ‎2016-06-03 04:30 AM
  • Posted Re: ION8650 certification for IEC62053-22(Class 0,2) and IEC62053-23 (Class 2.0) on Metering & Power Quality. ‎2016-03-28 09:45 AM
  • Posted USB Driver for ION7400 and ION Setup on Metering & Power Quality. ‎2016-03-23 01:42 PM
  • Posted Re: Latest Version ION Setup 3.0.15338.01 Installation Issues on Metering & Power Quality. ‎2016-03-23 01:29 PM
  • Liked Re: Latest Version ION Setup 3.0.15338.01 Installation Issues for sesa56562_bridg. ‎2016-03-23 01:29 PM
  • Posted Re: Latest Version ION Setup 3.0.15338.01 Installation Issues on Metering & Power Quality. ‎2016-03-09 02:03 PM
  • Got a Like for Re: Latest Version ION Setup 3.0.15338.01 Installation Issues. ‎2016-03-05 06:27 AM
  • Posted Re: Latest Version ION Setup 3.0.15338.01 Installation Issues on Metering & Power Quality. ‎2016-03-04 01:12 PM
  • Posted Re: Latest Version ION Setup 3.0.15338.01 Installation Issues on Metering & Power Quality. ‎2016-03-04 11:29 AM
  • Posted Re: PowerLogic Answer to Fluke / Dranetz on Metering & Power Quality. ‎2016-03-02 08:40 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.