Manager and module list of ION meter in ION Setup
How can a complete list of ION Modules and managers be printed using ION Setup? The objective would be to print a list of modules in ION Setup. Note this is different than the Meter Configuration Report via Setup Assistant.
- Labels:
-
ION Setup
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
Assuming you are viewing the device using the Advanced ION module view, simply press the Print button on the toolbar (or select File -> Print from the menu) and it will print out the Inputs/Setups/Output of every single module of every single manager. There is no option to just list managers/modules without the inputs/setups/outputs.
WARNING: This operation will take a very long time and will consume a very large amount of paper or generate a very large file if you print to a file instead.
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
Thanks Rob. This is great.
Seems to work fine for ION8600...but not working for ION8650. Any ideas?
File: entire device configuration.pdf is blank.
ION Setup 3.0.17125
ION8650 V407 & V420.
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
Looks like I've overlooked adding the more recent meters to the printing function as almost nobody uses/knows about it. I'll add it to the next version (in the mean time just switch your meter type to one that works prior to printing and switch back after your done).
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
The issue with ION8650 should now be resolved in the latest release (v3.0.17160.01) available on Box.