Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
How can a complete list of ION Modules and managers be printed using ION Setup? The objective would be to print a list of modules in ION Setup. Note this is different than the Meter Configuration Report via Setup Assistant.
Link copied. Please paste this link to share this article on your social media post.
Assuming you are viewing the device using the Advanced ION module view, simply press the Print button on the toolbar (or select File -> Print from the menu) and it will print out the Inputs/Setups/Output of every single module of every single manager. There is no option to just list managers/modules without the inputs/setups/outputs.
WARNING: This operation will take a very long time and will consume a very large amount of paper or generate a very large file if you print to a file instead.
Link copied. Please paste this link to share this article on your social media post.
Thanks Rob. This is great.
Seems to work fine for ION8600...but not working for ION8650. Any ideas?
File: entire device configuration.pdf is blank.
ION Setup 3.0.17125
ION8650 V407 & V420.
Link copied. Please paste this link to share this article on your social media post.
Looks like I've overlooked adding the more recent meters to the printing function as almost nobody uses/knows about it. I'll add it to the next version (in the mean time just switch your meter type to one that works prior to printing and switch back after your done).
Link copied. Please paste this link to share this article on your social media post.
The issue with ION8650 should now be resolved in the latest release (v3.0.17160.01) available on Box.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.