Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 and EN50160:2010 or EN50160:2000

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000 and EN50160:2010 or EN50160:2000
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
swil
swil
Mentor

Posted: ‎2019-03-19 11:03 PM . Last Modified: ‎2019-03-19 11:17 PM

0 Likes
2
2018
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
‎2019-03-19 11:03 PM

PM8000 and EN50160:2010 or EN50160:2000

There are two PM8000 meters at a site connected to PME.

* One can run the EN50160:2010 report. It can't run EN50160:2000 reports. It has firmware 1.03.01 and template 8000_FAC-PQ_V1.1.0

* One can run the EN50160:2000 report. It can't run EN50160:2010 reports. It has firmware 1.04.03 and template 8000_FAC-PQ_V1.4.0.0.0

 

What might be the reason for the difference?

Is it typical that PM8000 meters can run one of these EN50160 reports and not the other?

Tags (2)
  • Tags:
  • en50160
  • pm8000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-20 09:45 AM

1 Like
1
2011
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
‎2019-03-20 09:45 AM

Hello,

 

Be sure to backup the database before making any modifications.

 

No this is not typical, possibly not an issue with the meter itself. In the ION_Network database there is a table that records what versions of meter templates can run the EN501660:2010 rereport. In ION_Network, uder Views, there is one for cfg_ItemValues, if you edit this view you can search for 'EN50160_V2010_Frameworks'  and append the template name of the V1.4. Remeber that the name will need the special character between names, examples of names for the V1.1 framework are below.

 '8000_FAC-PQ_V1.1.0.0.0·8000_FAC_V1.1.0.0.0·

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-03-20 09:45 AM

1 Like
1
2011
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
‎2019-03-20 09:45 AM

Hello,

 

Be sure to backup the database before making any modifications.

 

No this is not typical, possibly not an issue with the meter itself. In the ION_Network database there is a table that records what versions of meter templates can run the EN501660:2010 rereport. In ION_Network, uder Views, there is one for cfg_ItemValues, if you edit this view you can search for 'EN50160_V2010_Frameworks'  and append the template name of the V1.4. Remeber that the name will need the special character between names, examples of names for the V1.1 framework are below.

 '8000_FAC-PQ_V1.1.0.0.0·8000_FAC_V1.1.0.0.0·

L4 Prime for Advanced metering and Utilities
Reply
swil
swil
Mentor

Posted: ‎2019-03-20 08:48 PM

0 Likes
0
2005
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
‎2019-03-20 08:48 PM

Hi Charles.


Thanks for that answer. You are a legend.

Changing that one value in CFG_ItemValue table fixed it. The relevant ItemID was found in the CFG_Item table.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.