Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About swil
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
swil
swil
Mentor
‎2023-10-06
371
Posts
32
Likes Received
177
Likes Given
7
Solutions

Community Badges

Resistance is Futile - L7
Open Hailing Frequencies - L6
Resistance is Futile - L6
Open Hailing Frequencies - L5
+17
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
swil
swil

Device type - IFM Module for Breakers - Com'X and Panel Server

Looking at https://www.se.com/ww/en/faqs/FA285178/, it appears that there is several types of IFM devices for similarly named breaker models. Regardi...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1702 0 2

2022-10-23 06:42 PM

swil
swil

Com'X configuration - adding Panel Server as an ethernet device

Hi,Is it possible to add a PAS600 (or PAS800) as a downstream ethernet device in a Com'X 510 / Com'X 210 Configuration? Although the Panel server is n...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
2340 0 4

2022-10-23 03:32 PM

swil
swil

PM8000 V3.1.0 firmware upgrade and compatible frameworks

Several questions about PM8000 firmware.1. Is FW version 3.1.0 the most recent?2. Is there a variety of frameworks offered at another Schneider link, ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2788 0 3

2022-10-04 11:01 PM

swil
swil

PAS800 Custom Device Model (for firmware 001.004.000)

Q1. Does PAS800 support end users having the ability to create/use custom device models?Q2. Please provide any documentation on requirements for conf...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
6491 1 14

2022-09-23 07:19 PM

swil
swil

EPC on WS2019 - Node Server UI is not running. Please try again

Can Ecostruxure Power Commission be installed and open successfully on Windows Server 2019? I ran the latest .25(?) version EPC installer as administ...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1638 0 2

2022-09-23 06:00 PM

swil
swil

Network Topology - Concurrent connections for ION7350

Hi,A site has Ethernet connection to multiple ION7350s being read by the BMS Using Modbus TCP/IP. The objective is to read all meters into the BMS, a...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1105 0 0

2022-06-25 01:28 AM

swil
swil

PM8000 DCF FIle for standard meter type

There is a standard meter framework in place on a site. It is running in a PM8000 with FAC1 Revision 3.0.0 and FAC1 Template 8000 V2.2.0.0.0. I have a...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
3086 0 5

2022-05-02 06:17 AM

swil
swil

LUFP7 Profibus DP / Modbus Gateway Software

I'd like to map modbus RTU addresses to Profibus DP using a LUFP7 Gateway.1. Can I map custom modbus-RS485 registers to custom Profibus addresses with...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
4072 0 2

2022-03-15 09:20 PM

swil
swil

Old Com'X 510 firmware upgrade question, FTP file push issue

Hi,A Com'x 510 firmware upgrade may take place. The device is configured with data logging.Questions:1. Can firmware upgrades delete data or configura...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1182 0 1

2022-02-24 05:49 AM

swil
swil

Log into Com'X webserver

I'm trying unsuccessfully to log into a Com'X webserver. Last time it was logged into was last year. Please provide an explanation for what is occurri...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
5746 0 11

2022-02-22 02:03 AM

swil
swil

How many meters can be comfortably interfaced to a Com'X

Q1a. If using a Com'X210 / Com'X510 as a datalogger with F/W 6.8.4, how many metering devices can be comfortably interfaced to without causing hardwar...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1134 0 2

2022-02-17 01:02 PM

Activity Feed
  • Got a Like for PM5560 Changed IP address, Can't save new IP address. ‎2023-06-22 04:23 AM
  • Got a Like for Re: PAS800 Custom Device Model (for firmware 001.004.000). ‎2023-04-03 12:11 PM
  • Got a Like for PAS800 Custom Device Model (for firmware 001.004.000). ‎2022-11-15 05:23 PM
  • Got a Like for Re: PAS800 Custom Device Model (for firmware 001.004.000). ‎2022-11-02 04:57 PM
  • Posted Re: Com'X configuration - adding Panel Server as an ethernet device on Gateways and Energy Servers. ‎2022-10-24 07:39 PM
  • Posted Device type - IFM Module for Breakers - Com'X and Panel Server on Gateways and Energy Servers. ‎2022-10-23 06:42 PM
  • Posted Com'X configuration - adding Panel Server as an ethernet device on Gateways and Energy Servers. ‎2022-10-23 03:32 PM
  • Liked Re: PM8000 V3.1.0 firmware upgrade and compatible frameworks for Tom_Stevenson. ‎2022-10-06 06:21 PM
  • Liked Re: PM8000 V3.1.0 firmware upgrade and compatible frameworks for Tom_Stevenson. ‎2022-10-06 06:20 PM
  • Posted Re: PM8000 V3.1.0 firmware upgrade and compatible frameworks on Metering & Power Quality. ‎2022-10-06 04:41 PM
  • Got a Like for Re: Refreshed eBrochure, Flyer and Presentation for Advanced Meters. ‎2022-10-05 03:13 PM
  • Posted PM8000 V3.1.0 firmware upgrade and compatible frameworks on Metering & Power Quality. ‎2022-10-04 11:01 PM
  • Posted Re: PAS800 Custom Device Model (for firmware 001.004.000) on Gateways and Energy Servers. ‎2022-09-27 04:05 AM
  • Posted Re: PAS800 Custom Device Model (for firmware 001.004.000) on Gateways and Energy Servers. ‎2022-09-26 03:29 PM
  • Posted Re: PAS800 Custom Device Model (for firmware 001.004.000) on Gateways and Energy Servers. ‎2022-09-26 03:25 PM
  • Liked Re: PAS800 Custom Device Model (for firmware 001.004.000) for Guillaume_Evrard. ‎2022-09-26 01:28 AM
  • Posted Re: PAS800 Custom Device Model (for firmware 001.004.000) on Gateways and Energy Servers. ‎2022-09-24 01:49 PM
  • Posted PAS800 Custom Device Model (for firmware 001.004.000) on Gateways and Energy Servers. ‎2022-09-23 07:19 PM
  • Posted EPC on WS2019 - Node Server UI is not running. Please try again on Gateways and Energy Servers. ‎2022-09-23 06:00 PM
  • Liked PAS800 - Data logging interval defaults for Sam_Vosch. ‎2022-08-17 05:42 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.