Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
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
  • About danielbarrantes
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
danielbarrantes
danielbarrantes
Lieutenant JG
‎2024-09-11
65
Posts
11
Likes Received
7
Likes Given
3
Solutions

Community Badges

Open Hailing Frequencies - L4
Resistance is Futile - L4
Live Long and Prosper - L3
Open Hailing Frequencies - L3
+11
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
danielbarrantes
Lieutenant JG danielbarrantes

High Speed Data Recording with ION 8650 B

Hello, I have previously performed high speed measurements with an ION 7650 and with an ION9000, however, currently a client needs to perform these me...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1889 0 4

2024-05-15 08:50 AM

danielbarrantes
Lieutenant JG danielbarrantes

DNP 3.0 setup with ION meter

Hello, I would like to open a case that happen when editing the analog values of a DNP map for an ION7550. When selecting a deadband of 5 or 1 instead...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1989 0 3

2024-04-30 10:47 AM

danielbarrantes
Lieutenant JG danielbarrantes

Cant read real time values PM8000

Hello, I have a problem with a PM8000 power quality meter, the meter communicates well using ION Setup and PME, however the real time values ​​on the ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
5622 1 11

2024-03-21 01:12 PM

danielbarrantes
Lieutenant JG danielbarrantes

PM5560 meter swap

Hello, currently a client has a PM5560 meter with a completely blank screen, however the meter does communicate to the PME. This meter is going to be ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2236 0 3

2024-02-22 07:06 AM

danielbarrantes
Lieutenant JG danielbarrantes

ION7650 Modbus COMM

Hello, I have 2 ION7650 meters whose values ​​via Modbus only give me 65535, I would like to ask if this answer is typical in any specific case, such ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
4956 0 8

2023-12-26 09:32 PM

danielbarrantes
Lieutenant JG danielbarrantes

Monitoring of multiple connections in energy meter

Hello, I would like to know if there is to know the connections (queries) that a meter has at any given time. For example:2 masters consulting via ION...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1462 0 3

2023-07-17 01:28 PM

danielbarrantes
Lieutenant JG danielbarrantes

ION9000 boot problem

Hi, I am trying to set up a new ION9000, however when I turn it on the rear "On/Off" LED just flashes green and red for hours. Checking the manual, it...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1594 0 1

2023-07-04 03:57 PM

danielbarrantes
Lieutenant JG danielbarrantes

Selection of suitable fuses for energy meters

Hello, reading the manual for the ION9000 meter and some other Schneider Electric equipment, they recommend using fuses for the meter power and for th...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
3752 0 3

2023-06-15 08:01 AM

danielbarrantes
Lieutenant JG danielbarrantes

Increase the size of data extracted from ION Setup

Hello, I have been testing the high speed reading module with an ION7650. The readings are given at correct intervals, however in ION Setup it only le...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2150 0 5

2023-06-06 03:14 PM

danielbarrantes
Lieutenant JG danielbarrantes

ION 9000 Calibration

Hello, a client needs to perform a calibration on an ION9000 energy meter, however, the factory told us that the optical port is disabled for these de...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1938 0 4

2023-02-23 10:19 AM

danielbarrantes
Lieutenant JG danielbarrantes

Communication problems of 7550 and 8650 energy meters ION Setup

Currently I do not have communication with 7550 and 8650 energy meters which are connected by ethernet. The curious thing is that the same meter can b...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
3370 1 4

2021-09-07 12:08 PM

Activity Feed
  • Posted Re: Two IP addresses Ion9000 on Metering & Power Quality. ‎2024-08-09 12:23 PM
  • Liked Re: DNP 3.0 setup with ION meter for Charles_Murison. ‎2024-05-28 04:09 PM
  • Posted Re: High Speed Data Recording with ION 8650 B on Metering & Power Quality. ‎2024-05-27 10:28 AM
  • Posted Re: High Speed Data Recording with ION 8650 B on Metering & Power Quality. ‎2024-05-15 11:04 AM
  • Posted High Speed Data Recording with ION 8650 B on Metering & Power Quality. ‎2024-05-15 08:50 AM
  • Tagged High Speed Data Recording with ION 8650 B on Metering & Power Quality. ‎2024-05-15 08:50 AM
  • Posted DNP 3.0 setup with ION meter on Metering & Power Quality. ‎2024-04-30 10:47 AM
  • Tagged DNP 3.0 setup with ION meter on Metering & Power Quality. ‎2024-04-30 10:47 AM
  • Got a Like for Cant read real time values PM8000. ‎2024-04-03 01:27 AM
  • Posted Re: Cant read real time values PM8000 on Metering & Power Quality. ‎2024-04-01 03:16 PM
  • Posted Re: Cant read real time values PM8000 on Metering & Power Quality. ‎2024-03-22 11:29 AM
  • Posted Re: Cant read real time values PM8000 on Metering & Power Quality. ‎2024-03-22 11:26 AM
  • Posted Re: Cant read real time values PM8000 on Metering & Power Quality. ‎2024-03-21 04:08 PM
  • Posted Cant read real time values PM8000 on Metering & Power Quality. ‎2024-03-21 01:12 PM
  • Tagged Cant read real time values PM8000 on Metering & Power Quality. ‎2024-03-21 01:12 PM
  • Posted PM5560 meter swap on Metering & Power Quality. ‎2024-02-22 07:06 AM
  • Tagged PM5560 meter swap on Metering & Power Quality. ‎2024-02-22 07:06 AM
  • Posted Re: ION7650 Modbus COMM on Metering & Power Quality. ‎2024-02-08 02:54 PM
  • Posted Re: ION7650 Modbus COMM on Metering & Power Quality. ‎2024-01-19 02:14 PM
  • Posted Re: ION7650 Modbus COMM on Metering & Power Quality. ‎2024-01-12 10:13 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.