Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Monitoring of multiple connections in energy meter

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Monitoring of multiple connections in energy meter
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
526
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
danielbarrantes
Lieutenant JG danielbarrantes
Lieutenant JG

Posted: ‎2023-07-17 01:28 PM

0 Likes
3
1456
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
‎2023-07-17 01:28 PM

Monitoring of multiple connections in energy meter

Hello, I would like to know if there is to know the connections (queries) that a meter has at any given time. For example:


2 masters consulting via ION protocol: IP 1.1.1.1 and 1.1.1.2
1 master consulting via DNP3: IP 1.1.1.3
1 master consulting via RS-485: IP 1.1.1.4

 

Context: Currently in a project there are multiple connections due to network permissions that had been authorized long ago without any control. Currently, many people (different SCADAs or masters) consult the meters simultaneously and this causes the main SCADA to lose data due to excessive connections when the limit of simultaneous users is reached. What I would like is to know if I can consult the IPs or protocols that the meter is consulting to be able to track and block them, so that only authorized personnel can consult the energy meter.

 

I hope I have explained myself correctly, if you have any other questions regarding the application, please let me know.

 

Greetings.

 

@Charles_Murison @Sanjeet_Sahota 

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-07-26 11:41 AM . Last Modified: ‎2023-08-15 10:29 AM

0 Likes
2
1448
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
‎2023-07-26 11:41 AM

Hello @danielbarrantes ,

 

Depending on the meter and firmware version, you may be able to get some of this information via terminal session. One item to note, the terminal session will drop a connection if meter is full so not always able to tell if meter is using all connections or 1 less than all.

For ION meters, connect to the meter with Telnet or SSH, this may need to be enabled on the meter. Then issue command EDS . The result should be a table of all the current connections to the meter including port numbers. 

Hope this is able to give you what you need.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 3
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-07-26 11:41 AM . Last Modified: ‎2023-08-15 10:29 AM

0 Likes
2
1449
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
‎2023-07-26 11:41 AM

Hello @danielbarrantes ,

 

Depending on the meter and firmware version, you may be able to get some of this information via terminal session. One item to note, the terminal session will drop a connection if meter is full so not always able to tell if meter is using all connections or 1 less than all.

For ION meters, connect to the meter with Telnet or SSH, this may need to be enabled on the meter. Then issue command EDS . The result should be a table of all the current connections to the meter including port numbers. 

Hope this is able to give you what you need.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
danielbarrantes
Lieutenant JG danielbarrantes
Lieutenant JG

Posted: ‎2023-07-28 04:16 PM

0 Likes
1
1441
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
‎2023-07-28 04:16 PM

Hello Charles, I tried what you indicate, I did it through the PuTTY console, however when I enter the console it shows me what you can see in the following image:

 

danielbarrantes_0-1690586046516.png

 

I assume that I have to enter the access credentials, which, according to the following link, are "8650" if I have standard security or "UserXX" if I have advanced security, however when entering those credentials it does not allow me access and therefore, I can't execute the "n" command you suggested.

 

https://www.se.com/ca/en/faqs/FA414545/

 

I currently have firmware V4.40.1, as the above link suggests.

Reply
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-07-31 09:32 AM

0 Likes
0
1433
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
‎2023-07-31 09:32 AM

Hello @danielbarrantes ,

I will admit that I do not use PUTTY much, my preferred program is Tera Term. In the meter, to able to connect with ION Setup, you will need to enable SSH terminal.

Charles_Murison_0-1690820977913.png

If you are able to connect to the meter, you would see something like the following, (this was after the Tera term login screen):

Charles_Murison_1-1690821126537.png

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.