Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:08 PM
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
Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:08 PM
Hi Steve. i did not open them. i think any one is able to see the color on the cable that a associate with the pin. my doubt are there with the color. is it any difference between them? or to better under stand my question, can you please send me a photo with i can differ one cable to another instead of the reference..
(CID:124521516)
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
Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:08 PM
Hi Dolêncio,
I guess my point is that this info should not matter. I can look to see if I can find one when I'm back in the office (or anyone else monitoring this post can) but how will this help you? If you're having an issue that needs troubleshooting this info likely won't help you.
Steve
(CID:124521525)
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
Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:08 PM
i have two cable doing the same job, there are connected as contact dry. but there are different (the cable), and one of them sometimes use to loose its config. on the appliance.
and i had to config it again. that why i wanted to know the physical difference between the cable, because i ma suspecting that one of the cable is the wrong one of cause the one that uses to have problem is the one.
(CID:124521545)
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
Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:08 PM
Hi Dolêncio,
As I mentioned, I don't have access to these cables at the moment but what I would first ask is are they both the same color on the device side? Black/green, black/red?
You asked about what color they should be at the RJ45, are you seeing that yours are different colors there?
When you say it changes it's config, what exactly changes? Does your configuration change or does the cable change from reporting as a dry contact to something else? If something else, what?
How often does it change?
How many cables connected totally? To the device itself? To a sensor pod?
What device?
If you swap the cables, does the issue follow the cable or the port?
Basically, if the troubleshooting finds that the cable itself is faulty, you'll have to contact tech support and get an RMA.
Steve
(CID:124521577)
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
Posted: 2020-07-03 10:18 PM . Last Modified: 2024-04-07 11:07 PM
1.yes, they are the same on divice side.
2.yes, they are different in color.
3. the config. changes (like name, and the relay contact config.) , the threshold too.
4. it takes about 30 minutes sometimes less then that.
5. IT has been connected 4 cable on Pod150
6. follow the cable.
(CID:124521581)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
What device?
(CID:124521583)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
Levato |
BG091A |
2 |
Andeli |
XJ5 |
2 |
The Levato devices one of them is connected with that cable.
(CID:124521587)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
Is this a NetBotz 250? Is this a 455?
What NetBotz device?
(CID:124521589)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
it is Netbotz 570 but the those sensores are plugged on netbotz sensor pod150
(CID:124521593)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
Understood ... I just wanted to verify it wasn't a 250 as there is a slightly different issue but still a connection issue soon to be resolved on that device / firmware.
There are no known issues with the 570 where this happens. There are no known dry contact cable issues.
I'm going to have someone closer to your region work with you and potentially replace the sensor. If it is mis-wired, we need to know.
Thanks, Steve
John Thompson, since you're more regional to this, can you please look into it?
(CID:124521611)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
Hi d.langa,
I sent you a private message earlier today. Can you reply to me, so that I can follow up on this.
Thanks
(CID:124521961)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2024-04-07 11:07 PM
hi. sorry. i was not at the office. i my from Mozambique, at Maputo
(CID:124521991)
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
Posted: 2020-07-03 10:19 PM . Last Modified: 2023-10-22 01:54 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.