Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Data Center Expert 7.9.1 release notes
Data Center Expert release notes
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
If the DCE update files are not available in EcoStruxure IT Entitlements, contact yourlocal technical supportto verify your support contract and get access to the update file(s) you need.
The DCE console is a stand-alone Java application that runs on systems that meet the following requirements:
A PC with a 1-GHz or better AMD/Intel processor running a 64-bit operating system: Microsoft® Windows® Server 2012 or 2016, Windows 10; Red Hat® Enterprise Linux® version 6.0; CentOS 6
At least 2 GB of RAM and 20 GB disk space
Screen resolution should be set to at least 1024 x 768
Supported browsers: Edge; Mozilla® Firefox®; Google Chrome™ See Known issues in DCE for details about support for Internet Explorer and Edge
New features in v7.9.1
HTTP support removed
The desktop client and the web client now support HTTPS communication only.
The following steps are necessary to update DCE v7.9.0 to DCE v7.9.1.
You must have a valid software support contract to receive the DCE v.7.9.1 update. If you do not, then you will need to purchase one to receive the update.
DCE must be at a minimum of v7.9.0 to update to DCE v7.9.1. If you are downloading DCE v7.9.1, you will need access to the Internet.
IMPORTANT: Do not reboot the server during the update.
The DCE 7.9.1 update performs a data migration that takes under an hour for most systems. The data migration can take longer if the system has thousands of devices and years of history, and varies based on several factors:
Number of devices
Number of sensors connected to those devices
Polling interval
Frequency at which sensor values change. For example, input voltage to UPSs can fluctuate throughout the day vs. temperature sensors in a strictly controlled environment that almost always report the same value.
You can see the status of the update on the Data Center Expert web client Home page.
NOTICE: Before beginning an update, remember to run a full backup on your DCE by going to System > Server Administration Settings > Server Backup/Restore, create a backup entry and then click Start.
Download the upgrade.zip file, or contact Technical Support for assistance. Note: The restore.iso file may be needed for later use if a re-installation is required. See Restoring using ISO Format for instructions for restoring your data from a restore.iso file from the ISO format.
Extract/expand the upgrade zip file into a separate directory on the hard drive of the system that will be running the DCE Console.
Login to your DCE v7.9.0 server with full server access. Now select Updates from the menu bar then Apply Server Update.
Click Import and look into the subdirectory where extracted files are placed. The structure of the extracted fields should contain two folders, "BW" and "NBCCore", and an index file, "nbcpkg.lst"
Select the "nbcpkg.lst" file and click "Open".
The Upgrade/New Packages table will update indicating there is an update available for the DCE server. Check the "Install/Upgrade" option for the package(s) you want to upgrade. Click the Install Selected button to start the upgrade for the selected package(s). You will be prompted to confirm you want to proceed with the update. Click Install Update to start the update process. Do not reboot the server during the update process.
When the file transfer completes, DCE will restart and disconnect your console connection. You can point a web browser to the DCE server for status.
When the update is complete, point a web browser to the DCE server, and select Install DCE Client.
Restoring Data Center Expert using ISO Format
Warning: Only perform the steps in this section if directed to do so by a Technical Support technician.
Before You Restore: A system restore will erase all data and restore the DCE hardware server to its factory default settings. Make sure you have a copy of all installed license keys and network settings prior to restore.
Download the restore.iso file to create a bootable USB key, or contact Technical Support for assistance.
Place the USB key in the USB port of your DCE appliance.
Reboot DCE.
When the appliance restarts the system restore process begins automatically. This process takes approximately 10 minutes for the 1U DCE Basic, 15 minutes for 1U DCE Standard or 25 minutes for 2U DCE Enterprise. When the restore is complete, you will be prompted to remove the USB key and hit enter to reboot the server. Note: If the system boots into the existing DCE version, reboot the server and access the BIOS settings. Adjust the boot sequence to boot from USB first.
Once DCE has restarted, configure the DCE network settings.
Migrating a Data Center Expert hardware server to a virtual appliance
Before You Migrate: To migrate a DCE hardware server to a virtual appliance, you must purchase and apply an activation key. Additionally, you must contact APC Support for new node license keys and application license keys for the virtual appliance.
Perform a back up of the DCE hardware server, using the Server Backup/Restore option, accessed from the Server Administration Settings option in the System menu.
Deploy the demo version OVA, and configure it using the hardware equivalents for the DCE Basic, Standard, or Enterprise server from which you are migrating. The available disk space for the virtual appliance must be greater than the disk space used by the hardware server. You cannot restore to a virtual appliance with fewer CPU, fewer network adapters, less RAM, or less available disk space than the hardware server. See help for Deploying and configuring a DCE virtual appliance, and DCE virtual appliance equivalent configurations.
Perform a restore on the virtual appliance, using the Server Backup/Restore option, accessed from the Server Administration Settings option in the System menu. You cannot restore to a virtual machine other than the DCE virtual appliance.
Apply the activation key to the virtual appliance.
Log in to the DCE client. In the "License Keys" display, accessed from the Server Administration Settings option in the System menu, apply the new node license keys and application license keys you received from APC Support.
InsertUSBkey (no larger than 4GB) into your system.
Extract the following file to a temporary directory: DCExpertUsbFlashRestore_Win_7.9.1_b.zip
Open a command prompt to the temporary directory and run mkDCExpertRestoreUsbKey.bat <iso image filename>. For example: mkDCExpertRestoreUsbKey.bat c:\tmp\restore.iso
Answer the prompts as appropriate.
Instructions for a Linux machine:
Insert a 2GB (or larger) USB key into your system.
Extract the following file to a temporary directory: DCExpertUsbFlashRestore_Linux_7.9.1_b.tar.gz
Open a command prompt to the temporary directory and run mkDCExpertRestoreUsbKey.sh <iso image filename>. For example: mkDCExpertRestoreUsbKey.sh /tmp/restore.iso
Answer the prompts as appropriate.
Third-party USB key scripts:
The scripts used to create USB keys use the following software:
You can now choose to compress a backup. The compressed backup is a single tar.gz file with a .dce file extension for easier filename filtering. More..