Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
DCE server backup and restore
DCE configuration
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Automatically schedule or manually create backup files for your server's configuration data, or its configuration and repository data, and use a backup file to manually restore the server data, if needed.
Note: If a server backup fails, an email is sent to the Data Center Expert Administrator users that include an email address as part of their user credentials.
Backup entries are listed by Destination Server, with information about each entry.
Backup Type: what data will be saved in backup files:
Full: all server data (configuration and repository) will be saved in every backup file.
Synchronized: only changes to server data (configuration and repository) will be saved after the initial backup file.
Configuration: only server configuration data will be saved in every backup file.
You can add a backup to the list, or edit, remove, or manually start the backup entry selected in the list.
Click Stop Backup to stop a manually-started backup. An backup-cancelled email will be sent to the Data Center Expert Administrators that include an e-mail address as part of their user credentials.
Add backup
At least one backup entry should be defined and used to create scheduled backup files for the configuration data on the server, or its configuration and repository data.
Select System > Server Administration Settings > Server Backup/Restore.
Select to edit or add a backup entry. To edit a backup entry, select the listed entry and click Edit Backup. To add a backup entry, click Add Backup and select Windows Repository or NFS.
Configure the Windows Share or NFS Share settings. If no subdirectory is specified, data will be stored in the share's root directory.
For Windows Share, specify the NT LAN Manager authentication level: NTLM, NTMLi, NTLMv2, NTLMv2i, NTLMSSP, or NTLMSSPi. For NFS, select the transport protocol, UDP or TCP, and the NFS version: v2.0, v3.0, v4.0, or v4.1.
Select whether you want to backup all server configuration and repository data for each backup (Full), just the changes to the server configuration and repository data for each backup (Synchronized) or just the configuration data (Configuration). Click Test Mount. An error message will occur if the share settings are defined incorrectly.
Click Next to edit the schedule used to automatically backup the server data, or Finish. Note: The default schedule settings will cause a backup to occur every Friday at 1:00 AM.
In the "Backup Schedule" display, select the days on which a backup will occur, and the time it will occur on those days.
Note: To delete a backup entry, select it in the list and click Remove Backup.
You use the Restore from Backup wizard to select a backup file to be used to restore the Data Center Expert server.
Choose the backup location type. Select Existing Backup Location to locate a backup file at a location that has been used to save your Data Center Expert server data, and select the location of the backup file from the list. Select New Backup Location to locate a backup file from an archived location, a location where the current backup files are not being saved.
For Windows Share, specify the NT LAN Manager authentication level: NTLM, NTMLi, NTLMv2, NTLMv2i, NTLMSSP, or NTLMSSPi. For NFS, select the transport protocol, UDP or TCP, and the NFS version: v2.0, v3.0, v4.0, or v4.1.
Select whether you want to backup all server configuration and repository data for each backup (Full), just the changes to the server configuration and repository data for each backup (Synchronized), or just the configuration data (Configuration).
In the Restore from Backup display, select the backup file you want to use to restore the server.
The server will restart as a result of the restore process. You can log on after the server finishes rebooting, which can take a few minutes.