Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About POPE3909
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
POPE3909
POPE3909
Explorer
‎2026-06-28
23
Posts
1
Like Received
2
Likes Given
0
Solutions

Community Badges

Resistance is Futile - L3
Open Hailing Frequencies - L2
Resistance is Futile - L2
Live Long and Prosper
+4
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
POPE3909
POPE3909

Upgrading a project from SoMachine HVAC to ESME HVAC

Hi Guys,I'm trying to upgrade an old project written in SoMachine/FreeStudio (I'm using Eliwell version in this case) to the ESME HVAC/ Free Studio Pl...
Industrial Automation icon_circle HVAC and Pumping Forum
138 0 1

2026-06-22 10:37 PM

POPE3909
POPE3909

Need help with using PIDAutoTuning FB

Hi Guys,Trying to use PIDAutoTuning block for the first time but rKp and UiTi both output '0' after 3 oscillations. uiMessageID shows '2' which I don'...
Industrial Automation icon_circle HVAC and Pumping Forum
365 0 2

2026-05-21 08:42 PM

POPE3909
POPE3909

TM172 Modbus Register Bit Allocation

Hi Guys,I have a question regarding Status Variables/ Modbus Registers creation in M172.On ESME HVAC, under Status Variables, Starting from address 89...
Industrial Automation icon_circle HVAC and Pumping Forum
754 0 2

2025-07-30 07:49 PM

POPE3909
POPE3909

TM172E28R analog outputs 4-20mA configuration

Hi Guys,I'm trying to configure the Analog outputs (AO1,AO2) of TM172E28R expansion module to 4-20mA output (current modulation) but having problems w...
Industrial Automation icon_circle HVAC and Pumping Forum
1919 0 1

2025-01-22 10:45 PM

POPE3909
POPE3909

M172 HMI Simulation

Hi Guys,I'm detecting HMI user activity/last key pressed by using sysBackLight and it works fine with the actual controller but in the Sim mode sysBac...
Industrial Automation icon_circle HVAC and Pumping Forum
1227 0 1

2024-11-29 07:58 PM

POPE3909
POPE3909

Creating Arrays in ESME HVAC

Hi Guys,I'm stuck while trying to create an Array with its size (Upper bound) being a EEPROM variable instead of a set constant value.Here, Num_Units ...
Industrial Automation icon_circle HVAC and Pumping Forum
1013 0 1

2024-11-20 10:01 PM

POPE3909
POPE3909

Ecostruxure Machine Expert HVAC

Hi, I have ESME HVAC 1.6.0 installed on my Windows 10 PC, and it’s been working fine until recently. The tab at the bottom that shows ‘EDIT Mode,’ ‘CO...
Industrial Automation icon_circle HVAC and Pumping Forum
1997 0 2

2024-11-14 04:11 PM

POPE3909
POPE3909

HMI development on TM172DCLFG

Hi,I'm developing HMI screens on the TM172DCLFG (touch screen version), largely based on the HMI screens from the M172 built-in B/W display. Except f...
Industrial Automation icon_circle Machine and Motion Control Forum
2396 0 3

2024-07-10 05:13 PM

POPE3909
POPE3909

PAS800 Server Virtual Devices

Hi Guys,I have 3 meters (lets say Meter B,C,D) feeding from the mains. I want to create a 'virtual' mains (addition of B,C,D) meter on PAS800 instead ...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1038 0 1

2024-05-21 09:20 PM

POPE3909
POPE3909

M172 losing PLC file

Hi Guys,I have a M172 on site that has been running fine for at least 2-3 years without any issue. One day the controller stops doing its function and...
Industrial Automation icon_circle HVAC and Pumping Forum
1395 0 2

2024-02-14 10:54 PM

POPE3909
POPE3909

M172 EEPROM Variables

Hi Guys,I've got M172 on the site which would randomly lose its default EEPROM variables values with some random numbers taking place instead. For exa...
Industrial Automation icon_circle HVAC and Pumping Forum
1773 0 1

2023-10-31 03:29 AM

Activity Feed
  • Posted Upgrading a project from SoMachine HVAC to ESME HVAC on HVAC and Pumping Forum. ‎2026-06-22 10:37 PM
  • Tagged Upgrading a project from SoMachine HVAC to ESME HVAC on HVAC and Pumping Forum. ‎2026-06-22 10:37 PM
  • Posted Need help with using PIDAutoTuning FB on HVAC and Pumping Forum. ‎2026-05-21 08:42 PM
  • Tagged Need help with using PIDAutoTuning FB on HVAC and Pumping Forum. ‎2026-05-21 08:42 PM
  • Posted Re: TM172 Modbus Register Bit Allocation on HVAC and Pumping Forum. ‎2025-07-31 04:43 PM
  • Posted TM172 Modbus Register Bit Allocation on HVAC and Pumping Forum. ‎2025-07-30 07:49 PM
  • Tagged TM172 Modbus Register Bit Allocation on HVAC and Pumping Forum. ‎2025-07-30 07:49 PM
  • Posted Re: OPC UA and M172 on HVAC and Pumping Forum. ‎2025-06-18 10:13 PM
  • Posted TM172E28R analog outputs 4-20mA configuration on HVAC and Pumping Forum. ‎2025-01-22 10:45 PM
  • Tagged TM172E28R analog outputs 4-20mA configuration on HVAC and Pumping Forum. ‎2025-01-22 10:45 PM
  • Posted M172 HMI Simulation on HVAC and Pumping Forum. ‎2024-11-29 07:58 PM
  • Tagged M172 HMI Simulation on HVAC and Pumping Forum. ‎2024-11-29 07:58 PM
  • Posted Creating Arrays in ESME HVAC on HVAC and Pumping Forum. ‎2024-11-20 10:01 PM
  • Tagged Creating Arrays in ESME HVAC on HVAC and Pumping Forum. ‎2024-11-20 10:01 PM
  • Liked Re: Ecostruxure Machine Expert HVAC for Bastian_Schmitz. ‎2024-11-17 11:24 PM
  • Posted Re: Ecostruxure Machine Expert HVAC on HVAC and Pumping Forum. ‎2024-11-17 11:23 PM
  • Posted Ecostruxure Machine Expert HVAC on HVAC and Pumping Forum. ‎2024-11-14 04:11 PM
  • Tagged Ecostruxure Machine Expert HVAC on HVAC and Pumping Forum. ‎2024-11-14 04:11 PM
  • Got a Like for Re: HMI development on TM172DCLFG. ‎2024-07-16 12:07 AM
  • Posted Re: HMI development on TM172DCLFG on Machine and Motion Control Forum. ‎2024-07-14 11:47 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.