HMI development on TM172DCLFG

Machine and Motion Control Forum

Support forum for Machine and Motion Control solutions, including Lexium MC12 and robotics, PacDrive, Modicon PLCs and I/Os, EcoStruxure Machine Expert Twin, … - from design, implementation to troubleshooting and more, by Schneider Electric
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
  • Industrial Automation
  • Machine and Motion Control Forum
  • HMI development on TM172DCLFG
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Bastian_Schmitz
Admiral Bastian_Schmitz Admiral
9
FernandoRodrigues
FernandoRodrigues Support
7
Francesco_Begnoni
Francesco_Begnoni Support
5
LeTomas
Lt. Commander LeTomas Lt. Commander
5
View All
Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert - HVAC

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Machine and Motion Control Forum
Start a Topic
Solved
POPE3909
Ensign POPE3909
Ensign

Posted: ‎2024-07-10 05:13 PM

0 Likes
3
1498
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
Posted: ‎2024-07-10 05:13 PM

HMI development on TM172DCLFG

 

Hi,

I'm developing HMI screens on the TM172DCLFG (touch screen version), largely based on the HMI screens from the M172 built-in B/W display. Except for changes in font size and buttons (from physical to touch-based), the base HMI code and structure are the same.

 

However, the performance on the DCL screen is very laggy, especially on pages with a lot of information. For example, the alarms page uses 'Sets' with 'Set_AlarmsName' and 'Set_AlarmsStatus,' totaling 70 variables in each set (see screenshots attached).

 

Please refer to the attached video for reference. Notice the lack of lag on the M172 PLC for the same 'Alarms' page compared to the very laggy performance on the DCL touch screen.

 

On simpler pages like the clock adjust page, the DCL performs quite fast as shown in the video.

 

What do you think is causing the laggy performance? Is it the RS485 speed or the processor? Upon checking the hardware, the DCL touchscreen has the same speed ARM Cortex M3 processor with up to 120MHz, so it should be able to handle what the M172 PLC does. I'm using the touchscreen as the master and the M172 as the only slave on the RS485, so the network load is minimal.

Attachments
Labels
  • Labels:
  • Connectivity
  • HVAC
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
FedericoM
Captain FedericoM Captain
Captain

Posted: ‎2024-07-11 11:49 PM

0 Likes
1
1472
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
Posted: ‎2024-07-11 11:49 PM

I usually define a CASE linked to a different modbus read, every 0.5sec I managed a different read.

If a write is required from Display, I set a trigger which will manage the write.

In case of R/W set, if you want to keep the @PLC.variable syntax, you have to limit the number of parameters shown per page.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 3
FedericoM
Captain FedericoM Captain
Captain

Posted: ‎2024-07-11 11:45 PM

0 Likes
0
1472
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
Posted: ‎2024-07-11 11:45 PM

Hello,

 

the delay is caused by modbus communication, each @PLC.variable read by the M172 requires a modbus message.

If you want to optimize the speed you should manage all the modbus part from programming, using multiple R or W messages.

If you define a global variable in the Display part (only for this target), the variable can be used both in programming and display.

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
Captain FedericoM Captain
Captain

Posted: ‎2024-07-11 11:49 PM

0 Likes
1
1473
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
Posted: ‎2024-07-11 11:49 PM

I usually define a CASE linked to a different modbus read, every 0.5sec I managed a different read.

If a write is required from Display, I set a trigger which will manage the write.

In case of R/W set, if you want to keep the @PLC.variable syntax, you have to limit the number of parameters shown per page.

Reply

Link copied. Please paste this link to share this article on your social media post.

POPE3909
Ensign POPE3909
Ensign

Posted: ‎2024-07-14 11:47 PM

In response to FedericoM
1 Like
0
1407
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
Posted: ‎2024-07-14 11:47 PM

Hi Federicom,

As you suggested, I limited the number of variables per page and it works fine. Thanks for your explanation and clarification.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.