Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About Parlindungan_Sitorus
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Parlindungan_Sitorus
Parlindungan_Sitorus
Contributor
‎2026-07-12
56
Posts
2
Likes Received
0
Likes Given
2
Solutions

Community Badges

Resistance is Futile - L4
Open Hailing Frequencies - L3
Resistance is Futile - L3
Open Hailing Frequencies - L2
+9
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Substitute Products Gateway PowerLogic G3200

Hi Expert,Can you please provide information on a replacement for the PowerLogic G3200 gateway to convert Modbus RTU to IEC61850? Thank you in advance...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
441 0 1

2025-10-20 12:25 AM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Are our Power Meters and ION Meters equipped with H2S Certification?

Hi all,Are our Power Meters and ION Meters equipped with H2S Certification?We have a tendering documentation that apply this requirement subject to En...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1620 0 2

2025-09-23 11:38 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

How to setup and configure ION8650 to send alert (voltage disturbance ...

Hi Expert,I kindly need advice how to setup and configure the ION8650, when there is a sag/swell (voltage disturbance detection), will send notificati...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1452 0 2

2024-06-24 03:48 AM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

How to find out Modbus Register address or Output Register for TDD on ...

Hi Expert, We kindly need your help.We have requirement from a tender specification for PQ meter.The point that we still do not know is, the TDD on bo...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1135 0 1

2024-03-04 01:30 AM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Error Filesys Offline on display ION8650 Meter

ear Expert,Kindly need your help for problem that we have here.There is an ION8650 meter that shows error on display: Err: Filesys Offline What should...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1815 0 1

2023-07-17 08:39 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Ask: Accuracy on PowerTag Flex 160A (A9MEM1580) if installed on MCB 32...

Dear Expert,We kindly need your valuable support (urgent) for our question below: Question 1,On the datasheet PowerTag Flex 160A, there is information...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
964 0 0

2023-06-12 06:44 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

How to reset password ION7600 (customer forgot the password)

Dear All Expert, One of our customer that has ION7600 meter forgot the password.They want to change the parameter and also want to create the custom f...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2070 0 2

2022-03-23 07:18 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Interoperability Test for ION8650 meter on DC Auxiliary Power Supply

Dear All Expert, We will face a testing on Interoperability Test for ION8650 meter which will be carried out by the research and development center of...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2406 0 3

2022-03-23 02:19 AM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Setup and Configure ION8650 using DLMS protocol

Dear All,I have problem related to setup and configure ION8650 on retrieving data to other software application via DLMS protocol.Could you help me ho...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1446 0 1

2018-08-07 09:50 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

Case on Network Setup ION 8600

Dear All,I have a case regarding to network setup on ION8600 meter.I cannot access the network setup via front panel ION8600 meter and here the screen...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1978 0 3

2016-07-31 09:50 PM

Parlindungan_Sitorus
Parlindungan_Sitorus Contributor

How to connect and setup communication setting on CM3000 using EGX300?

Dear All,How can I connect and setup for communication setting on EGX300 into CM3000?Once I have tested before, I used 2 wire cable to connect seriall...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1164 0 1

2016-01-29 01:29 AM

Activity Feed
  • Posted Substitute Products Gateway PowerLogic G3200 on Gateways and Energy Servers. ‎2025-10-20 12:25 AM
  • Tagged Substitute Products Gateway PowerLogic G3200 on Gateways and Energy Servers. ‎2025-10-20 12:25 AM
  • Posted Are our Power Meters and ION Meters equipped with H2S Certification? on Metering & Power Quality. ‎2025-09-23 11:38 PM
  • Tagged Are our Power Meters and ION Meters equipped with H2S Certification? on Metering & Power Quality. ‎2025-09-23 11:38 PM
  • Posted How to setup and configure ION8650 to send alert (voltage disturbance detection) to handphone via short text messages on Metering & Power Quality. ‎2024-06-24 03:48 AM
  • Posted How to find out Modbus Register address or Output Register for TDD on PM8240 and ION7400 on Metering & Power Quality. ‎2024-03-04 01:30 AM
  • Posted Error Filesys Offline on display ION8650 Meter on Metering & Power Quality. ‎2023-07-17 08:39 PM
  • Tagged Error Filesys Offline on display ION8650 Meter on Metering & Power Quality. ‎2023-07-17 08:39 PM
  • Posted Ask: Accuracy on PowerTag Flex 160A (A9MEM1580) if installed on MCB 32A and recommendation for HMI Display? on Metering & Power Quality. ‎2023-06-12 06:44 PM
  • Tagged Ask: Accuracy on PowerTag Flex 160A (A9MEM1580) if installed on MCB 32A and recommendation for HMI Display? on Metering & Power Quality. ‎2023-06-12 06:44 PM
  • Posted How to reset password ION7600 (customer forgot the password) on Metering & Power Quality. ‎2022-03-23 07:18 PM
  • Tagged How to reset password ION7600 (customer forgot the password) on Metering & Power Quality. ‎2022-03-23 07:18 PM
  • Posted Re: Interoperability Test for ION8650 meter on DC Auxiliary Power Supply on Metering & Power Quality. ‎2022-03-23 06:52 PM
  • Tagged Re: Interoperability Test for ION8650 meter on DC Auxiliary Power Supply on Metering & Power Quality. ‎2022-03-23 06:52 PM
  • Posted Interoperability Test for ION8650 meter on DC Auxiliary Power Supply on Metering & Power Quality. ‎2022-03-23 02:19 AM
  • Tagged Interoperability Test for ION8650 meter on DC Auxiliary Power Supply on Metering & Power Quality. ‎2022-03-23 02:19 AM
  • Got a Like for Re: Apakah ada list register untuk PM5000?. ‎2022-01-06 07:38 PM
  • Posted Re: Apakah ada list register untuk PM5000? on Expert on Demand for Standards & Regulations. ‎2022-01-06 07:02 PM
  • Tagged Re: Apakah ada list register untuk PM5000? on Expert on Demand for Standards & Regulations. ‎2022-01-06 07:02 PM
  • Posted Setup and Configure ION8650 using DLMS protocol on Metering & Power Quality. ‎2018-08-07 09:50 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.