Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi Expert,
We kindly need your help.
We have requirement from a tender specification for PQ meter.
The point that we still do not know is, the TDD on both PM8240 and ION7400.
We check on excel file for PM8240 and ION7400, only on PM8240 there are several list like:
| TDD Current A 10 Minute | 34681 |
| TDD Current B 10 Minute | 34683 |
| TDD Current C 10 Minute | 34685 |
| I-TDD Z Comp | 43756 |
| PO I-TDD Z Cmp | 43788 |
From this register, which one related to show the TDD?
On ION7400, still could not find the Modbus Register for this TDD parameter.
Please help,
Best regards,
Link copied. Please paste this link to share this article on your social media post.
Hello @Parlindungan_Sitorus ,
When looking at the ION7400 V4.5.0 Modbus mapping excel file I see the same TDD registers as PM8000 meter. One item to note is that this TDD is from the IEE519 framework. You will need to configure IEEE519 or at least the External numeric 519_I_L in meter for the TDD calculations. The modules performing the TDD are Harmonic Measurement Modules.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @Parlindungan_Sitorus ,
When looking at the ION7400 V4.5.0 Modbus mapping excel file I see the same TDD registers as PM8000 meter. One item to note is that this TDD is from the IEE519 framework. You will need to configure IEEE519 or at least the External numeric 519_I_L in meter for the TDD calculations. The modules performing the TDD are Harmonic Measurement Modules.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.