Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Dear All,
I have a case regarding to network setup on ION8600 meter.
I cannot access the network setup via front panel ION8600 meter and here the screenshots:



Here is the serial number of this meter:
M8600B4E0H5C7B1B
I need advice from all of you.
Thank you in advance.
Regards,
Link copied. Please paste this link to share this article on your social media post.
Dear Parlindungan SITORUS PANE,
could you please log a support request through your local Schneider Electric Customer Care Center (SE Website --> Support --> Contact). They. will help you with your request.
Thank you
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Your device has hardware lock option you have to set it to test mode.
Open cover press Test switch
Link copied. Please paste this link to share this article on your social media post.
The "Not Available" being displayed when attempting to access the network setup indicates some type of Ethernet module issue. One thing you can try is to find a working TCP connection and plug into the 10Base-T connector to see if the LEDs begin blinking (one should go solid ON, the other blink if there is TCP traffic). If the LEDs are not working (and you know that the connection is working), then it is likely some type of issue with the device's comm card.
You could also try to plug a PC into the RS-232 port to try and communicate using ION Setup to see if the Ethernet module is being discovered or not by the device.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.