Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How do I know if ION Setup is truely able to adjust CM3 CM4 Waveform Log Configrations

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • How do I know if ION Setup is truely able to adjust CM3 CM4 Waveform Log Configrations
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Yu_Diao
Yu_Diao Leader
Leader

Posted: ‎2016-07-28 06:12 PM . Last Modified: ‎2020-04-22 01:23 AM

0 Likes
1
961
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
‎2016-07-28 06:12 PM

How do I know if ION Setup is truely able to adjust CM3 CM4 Waveform Log Configrations

I am working on a project which has around 100 CM2000, CM3000, CM4000 and PM8 devices on-site, and I could use either SMS or IONSetup to adjust their data/waveform logs as well as on-board alarms. By comparing the meter's "free memory" counter after the same modfiication was made in ION Setup and SMS, I am not sure if ION Setup really makes the change into effect. And here are the details:

 

ION Setup version: 3.0.16182.01

 

Per CM3000/4000 register map, register "403054" is the "Free Log Memory" counter in clusters, and one clusters is 1K (register 403055 = 1024). I started with a CM4000 meter which has 691K free log memory as shown below.

403054 691.png

I then use ION Setup to reduce the max capture number of "Disturbance WFC" log from 13 and 3. After clicked "Send", ION Setup showed me a progress bar to apply and reset the meter, and it indicated the modification was scussed through the message in the status bar at the bottom. I then noticied tha the modbus register "403054" still stayed at the same vaule rather than increased to a larger number (fewer waveform capture should free more log memory...).

IONSetup Adjustment.jpg

 

I then opened up the same meter in SMS. SMS was able to read out that the "captures" was "3" for  "Disturbance WFC" log which means ION Setup defintely did something to the meter. In order to let SMS redo the same change, I just increased the "caputres" to 4 and then reduce it back to "3", SMS then made the "Update" button available. Cliked the "Update" value, after a while, I check the "Free Log Memory" counter again, and this time, it incresed to "3283" as what I expected.

SMS Adjustment.jpgNew Free Log Memory.jpg

 

I have also tried similar test backwards: made the adjustment in SMS first (i.e. increase free log memory) and try to reduce it in ION Setup. The "Free Log Memory" value only changed after the "Update" was done in SMS but NOT in ION Setup.

 

I got a feeling that, while ION Setup was able to write the new configration into the meter, it somehow misses a final "GO" command to let the meter acutally put these configration into effect.

 

Robert Lee

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2016-08-02 04:40 PM

0 Likes
0
934
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
‎2016-08-02 04:40 PM

Hi Yu,

You are correct in that it looks like ION Setup is not properly resizing the allocated # of records when configuring waveforms on the CM/PM devices.  I have actually made a fix and doing some verification testing now and should be able to release a new version which will fix this issue going forward.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.