Dear Community Members,
We are currently experiencing a technical issue that is affecting the ability to create new posts. Our team is actively investigating the root cause and working to resolve it as quickly as possible. We apologize for the inconvenience and appreciate your patience.
SE Community Team!
Installing EcoStruxure IT Gateway on Windows 11 24H2 - WMIC required
What's new in EcoStruxure IT Gateway
Get the latest news, release notes, and other need-to-know information about EcoStruxure IT Gateway
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
The EcoStruxure IT Gateway Windows installer requires the Windows Management Instrumentation Command line (WMIC) utility. WMIC is not preinstalled by default on Windows 11 24H2.
The WMIC utility must be installed on new Windows 11 systems before you install EcoStruxure IT Gateway. Note: Older Windows 11 versions that were updated to 24H2 may already have WMIC installed.
Verify the Windows 11 version
Type system information in the search field on the taskbar.
Verify whether WMIC is installed on your system
Open a command window and type wmic os. If WMIC is not installed or enabled, the command returns:
'wmic’ is not recognized as an internal or external command, operable program, or batch file.
Install WMIC on your Windows 11 system
Type Optional features in the search field on the taskbar.
Note: WMIC will not appear in the Added features list if it is not installed.
In the Add an optional feature section, click View features.
Type WMICin the search field.
Check the box for WMIC and then click Next to install WMIC.
Feel free to add the link to this article to your documentation. Please note that Gateway version 2.0 and newer do not require installing WMIC. Gateway 2.0 is due to be released in June 2025.