Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogic PM5563 Data Log Loss of Precision after 1B Wh

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PowerLogic PM5563 Data Log Loss of Precision after 1B Wh
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic PM5000 series

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2024-07-14 08:15 PM

0 Likes
4
2142
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
‎2024-07-14 08:15 PM

PowerLogic PM5563 Data Log Loss of Precision after 1B Wh

We have come across an unfortunate behavior in the Ion Setup Data Log retrieval for PM5563 meters

 

Up until one shy of a billion on the meter, retrieving the Wh Data Log would produce a listing of 15-minute intervals precise to 1 watt-hours

 

As soon as the meter went over 1B, the log retrieval started using scientific notation precise only to the one-million-th watt hours. If I log into the meter's web interface directly, the wh counter is correct.

 

So for example on the meter web interface:

1006467208 Wh

is only being transmitted to Ion Setup as:

1006000000 Wh

 

How can Ion Setup be configured to retrieve data accurate to 1 Wh again?

 

Thanks in advance

 

  • Thumbnail of PowerLogic PM5000 series
    Schneider Electric
    PowerLogic PM5000 series
View products (1)
Labels
  • Labels:
  • ION Setup
  • PM5000
Tags (5)
  • Tags:
  • Data Log
  • english
  • ion setup
  • Loss of Precision
  • pm5563
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-07-16 09:42 AM . Last Modified: ‎2024-07-16 09:43 AM

1 Like
0
2085
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
‎2024-07-16 09:42 AM

What version of ION Setup are you using?  I suggest downloading the latest version from the following location: ION Setup Latest Release | Schneider Electric

Depending on how long ago the device has been since the data log has been programmed, you may need to reprogram the data log again with the latest version which should permit the UINT64 version of the energy registers and not the FLOAT32 version (which is what I believe is happening).

Below I've reprogrammed my PM556X device data log with the latest version and preset the energy register to the same number as you posted above and it is showing up fine.

Robert_Lee_0-1721147978726.png

 




See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-07-15 02:54 PM

0 Likes
1
2118
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
‎2024-07-15 02:54 PM

Hello @NortheastSolar ,

 

There are a number of factors that can come into play here. One of the big ones is what format for the number is being used. 32-bit float (IEEE 754, also know as Single-precision floating-point format) has limitations on resolution depending how big the number is. 1006467208 cannot be represented as a floating point number, the closes number would be 1006467200. The meter's web page might be using internal features such as int32, 64 bit float or some other method that cannot be used external to the meter.

When numbers get large, there is no way to keep resolution down to 1 kwh and still have large numbers when numbers are encoded with 32-bit floating point.

So short answer is no, not possible to for ION Setup. Why the resolution is that much lower in ION Setup I am not sure.

 

Regards,

Charles 

L4 Prime for Advanced metering and Utilities
Reply
NortheastSolar
NortheastSolar
Explorer

Posted: ‎2024-07-15 11:12 PM

0 Likes
0
2078
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
‎2024-07-15 11:12 PM

Hi Charles, 10 or 100 Wh precision would be workable but as it stands one million Wh precision is essentially unusable for us.

 

So the question becomes if either of the following options are possible:

- Subtract 1B from the total before transmitting to ION, or

- Transmit 10 or 100 Wh precise numbers to ION

 

Alternatively is there an alternative to ION to retrieve 15-minute interval data?

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2024-07-16 09:42 AM . Last Modified: ‎2024-07-16 09:43 AM

1 Like
0
2086
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
‎2024-07-16 09:42 AM

What version of ION Setup are you using?  I suggest downloading the latest version from the following location: ION Setup Latest Release | Schneider Electric

Depending on how long ago the device has been since the data log has been programmed, you may need to reprogram the data log again with the latest version which should permit the UINT64 version of the energy registers and not the FLOAT32 version (which is what I believe is happening).

Below I've reprogrammed my PM556X device data log with the latest version and preset the energy register to the same number as you posted above and it is showing up fine.

Robert_Lee_0-1721147978726.png

 




Reply
Kelster
Kelster
Explorer

Posted: ‎2025-06-09 08:09 AM

0 Likes
0
1216
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
‎2025-06-09 08:09 AM

If I do the software update, does it delete my existing data logs?
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.