Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 – Modbus TCP/IP Node ID

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000 – Modbus TCP/IP Node ID
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Gilbert
Gilbert
Explorer

Posted: ‎2025-06-04 10:48 AM

0 Likes
2
1308
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
‎2025-06-04 10:48 AM

PM8000 – Modbus TCP/IP Node ID

PM8000 – Modbus TCP/IP Node ID

With respect to the PM8244, the clients BMS software (Tridium, Niagara Framework) will not allow a node ID of 0 or 255.

Issue:

Upgrading from PM800 to PM8000 meters (39 meters), each meter has many Modbus RTU slaves (Meter as a Gateway). PM800 allowed to set the Node address to 1-248 for the TCP connection.

If we turn off the gateway function of the meter, the BMS will communicate and read meter data, as soon as we turn on the gateway (Modbus Master, Com1, Node ID 1) all RTU nodes communicate, but the PM8000 data stops.

Question:

Is there a was to set the TCP/IP Node ID between 1-248?

With Firmware V4.6, I see that BACnet can be used. Can the BMS talk to the PM8000 on BacNet and the meter still use the Gateway function (Modbus Master)?

Labels
  • Labels:
  • ION Setup
  • PM8000
  • Power Quality
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-06-05 09:18 AM

0 Likes
0
1293
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
‎2025-06-05 09:18 AM

Hello @Gilbert,
"Is there a was to set the TCP/IP Node ID between 1-248?"

-No, sadly, when gateway function is active, meter will only respond to ID 255.

"With Firmware V4.6, I see that BACnet can be used. Can the BMS talk to the PM8000 on BacNet and the meter still use the Gateway function (Modbus Master)?"

Yes, meter can have multiple protocols talk to the meter at the same time.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-06-05 09:18 AM

0 Likes
0
1293
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
‎2025-06-05 09:18 AM

Hello @Gilbert,
"Is there a was to set the TCP/IP Node ID between 1-248?"

-No, sadly, when gateway function is active, meter will only respond to ID 255.

"With Firmware V4.6, I see that BACnet can be used. Can the BMS talk to the PM8000 on BacNet and the meter still use the Gateway function (Modbus Master)?"

Yes, meter can have multiple protocols talk to the meter at the same time.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Gilbert
Gilbert
Explorer

Posted: ‎2025-06-05 01:10 PM

0 Likes
0
1240
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
‎2025-06-05 01:10 PM

Charles, Thank you for the timely response.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.