Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM5563 IP address resetting to 255.255.255.255 after upgrade to 4.4.1

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM5563 IP address resetting to 255.255.255.255 after upgrade to 4.4.1
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
DCarlson
DCarlson Mentor
Mentor

Posted: ‎2024-11-08 02:07 PM

1 Like
6
2543
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
‎2024-11-08 02:07 PM

PM5563 IP address resetting to 255.255.255.255 after upgrade to 4.4.1

*We have initiated a case already. 

 

I'm posting this here to see if anyone has seen this issue with 4.4.1 or any previous PM5563 firmware version.

 

Some meters *more than one* were upgraded from 4.2.1 to 4.4.1

The meters were able to communicate with PSO. Within a few hours to a few days the meter would stop talking to PSO. The IP settings were found to be as follows IP:255.255.255.255  SUBNET:  255.255.255.255   GATEWAY: 255.255.255.255

It was found that if the meter was power cycled, the IP settings reset back to the previously configured IP and the meter would talk. No changes were made to the meter. Then it was found that a few days later these meters (two of them) once again lost their communication setting. Thus, power cycling isn't a permanent solution. All 4 meters we upgraded lost IP at one point or another within the last 10 days.

The IP was NOT modified around the time frame that the meter was upgraded.

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2025-01-07 08:06 AM

0 Likes
0
2176
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
‎2025-01-07 08:06 AM

Hi @DCarlson 

 

The IP address will display 255.255.255.255 only when the Ethernet connection is not stable between the meter and host, So we need to connect the meter directly with the laptop and check. 

 

See Answer In Context

Reply
Replies 6
Jesus_Diaz
Jesus_Diaz Leader
Leader

Posted: ‎2024-11-12 01:53 PM

0 Likes
3
2488
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
‎2024-11-12 01:53 PM

Hi @DCarlson,

 

Was this ever observed when the meters were running version 4.2.1? Were there any other changes in the network recently, or was there an auxiliary power failure close to the occurrence of the issues?


Do you see anything in the meter's maintenance log from the web pages?


I would suggest contacting your local country support, as this might require a deeper investigation.

 

@Ramasamy_N, do you have any input on this?

 

Best Regards,

JD

Reply
DCarlson
DCarlson Mentor
Mentor

Posted: ‎2024-11-14 08:15 AM

0 Likes
0
2452
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
‎2024-11-14 08:15 AM

My understanding is that these meters were not experiencing this before the upgrade.

I do not believe there was any network changes.

 

However  we are investigating if there was "fluctuations" in the power. We are investigating.

Reply
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2024-11-18 09:19 PM

0 Likes
0
2416
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
‎2024-11-18 09:19 PM

Hi @Jesus_Diaz 

This behavior needs to be investigated.

Can you check if the meter IP address restored when it access directly 1 to 1 with a laptop before the power cycle?

 

Reply
DCarlson
DCarlson Mentor
Mentor

Posted: ‎2024-11-20 08:57 AM

0 Likes
0
2387
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
‎2024-11-20 08:57 AM

So even though the server can see the meter over the network, your suggesting we disconnect it and connect it locally to a meter to see if it works. How does a direct connection to the laptop differ from a serve over the network. In so far as telling us that the meter has "stored" the IP.

Reply
DCarlson
DCarlson Mentor
Mentor

Posted: ‎2024-11-20 09:20 AM . Last Modified: ‎2024-11-20 09:20 AM

0 Likes
0
2386
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
‎2024-11-20 09:20 AM

We have a site in which when using 4.4.1 a power fluctuation on the control power does seem to lead to a high likely hood that the meter "forgets" its stored IP. Resets to 255.255.255.255. A second site has issues only on one set of equipment, but we have not been able to find any correlation to other events which might be triggering the change in IP.

Reply
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2025-01-07 08:06 AM

0 Likes
0
2176
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
‎2025-01-07 08:06 AM

Hi @DCarlson 

 

The IP address will display 255.255.255.255 only when the Ethernet connection is not stable between the meter and host, So we need to connect the meter directly with the laptop and check. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.