Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Need help for ION8600

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Need help for ION8600
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa82148_bridg
sesa82148_bridg Contributor
Contributor

Posted: ‎2019-12-09 05:43 AM . Last Modified: ‎2020-04-22 01:00 AM

1 Like
7
4069
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
‎2019-12-09 05:43 AM

Need help for ION8600

Dear Group,

 

need help o explain the following.

 

  • The ION meter value today is 8,216,743.93 MWH. See attached photo. The value is for MWH export.
  • in the moddus map, If the KWH is composed of 2 registers, should not be their maximum value is
    2 To the power 32 (4,294,967,296 KWH = 4,294,967 MWH )?
  •  

How this can be configured in the ION? Since 4,294,967 < 8,216,743.93.

 

Attachments
Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • ion8600
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa82148_bridg
sesa82148_bridg Contributor
Contributor

Posted: ‎2020-01-01 11:55 PM

2 Likes
1
4040
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
‎2020-01-01 11:55 PM

we got a direction from Anup Surendran Chozhiyattel Thiyyath <anup.surendran@se.com> , to configure the modbus mapping. meaning , to create new 4 registers (4*16 bit = 64 bit).
in this way , the ION will store the values "as is" in these new registers. 

by this way, we can take the full value of the reading, in Watt resolution. 

the max range shall be 2^64 =18446744073709551616 W  = 18,446,744,073,709 MW. that is 2M times grater than the current value. 

 

we shall try this solution and update the case.

See Answer In Context

Reply
Replies 7
Yut
Yut
Leader

Posted: ‎2019-12-12 08:28 PM

0 Likes
1
4061
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
‎2019-12-12 08:28 PM

You mean this register address 40232 ?

 

Label       Address   Module no.     Module label   No. of registers    Format    Scaling   Scaling Enable

kWh rec   40232            9                     kWh/kVArh              2                      INT32       1/1000         No

 

Use ION Setup connect to meter change to Advance option select Modbus Slave module go to module No. 9 then configure it.

Hope this may help.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-12-20 09:30 AM . Last Modified: ‎2019-12-20 09:31 AM

0 Likes
2
4056
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
‎2019-12-20 09:30 AM

Hello,

 

The scaling of the register also needs to be taken into account, 1/1000 means that the value send via modbus will be 1000 times as large as the value in the register so when the modbus value is divided by 1000, the end result is 3 decimal points. With the default scaling and configuration, the maximum MWH to be sent = ((2^32 )/1000 )/1000) = 4,294.967296. There are a few options. A) link MWH to the modbus slave module, B) Reduce the scaling.

L4 Prime for Advanced metering and Utilities
Reply
sesa82148_bridg
sesa82148_bridg Contributor
Contributor

Posted: ‎2019-12-23 04:42 AM

0 Likes
0
4052
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
‎2019-12-23 04:42 AM

Dear Yut,

 

thanks for the reply. 

 

  • the meter displays a value of 8x10^6 MWH and still can increase.
  • note : the meter step up file shows the following :
    1. in ION step up software: the scaling found to be "custom"
    2. in ION meter display : the scaling found to be 1000.

 

so, what is the right scaling to choose in ION step up? in order can show bigger values ? (like the 

  • 8x10^6 MWH)

thanks

Reply
sesa82148_bridg
sesa82148_bridg Contributor
Contributor

Posted: ‎2019-12-23 04:59 AM

0 Likes
1
4051
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
‎2019-12-23 04:59 AM

i agree with you about the maximum value in MWH it can reach with 2 registers.

but the meter now shows this value in its display " 8x10^6 MWH "and still can increase.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2019-12-30 10:05 AM

0 Likes
0
4044
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
‎2019-12-30 10:05 AM

Note that inside the meter, the module in question is Float 64 bit number, only the modbus register is 32 bit integer.

L4 Prime for Advanced metering and Utilities
Reply
sesa82148_bridg
sesa82148_bridg Contributor
Contributor

Posted: ‎2020-01-01 11:55 PM

2 Likes
1
4041
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
‎2020-01-01 11:55 PM

we got a direction from Anup Surendran Chozhiyattel Thiyyath <anup.surendran@se.com> , to configure the modbus mapping. meaning , to create new 4 registers (4*16 bit = 64 bit).
in this way , the ION will store the values "as is" in these new registers. 

by this way, we can take the full value of the reading, in Watt resolution. 

the max range shall be 2^64 =18446744073709551616 W  = 18,446,744,073,709 MW. that is 2M times grater than the current value. 

 

we shall try this solution and update the case.

Reply
Anonymous user
Not applicable

Posted: ‎2020-03-24 03:32 AM

0 Likes
0
4028
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
‎2020-03-24 03:32 AM

Hi @sesa82148_bridg,

 

Did you find your answer to the replies above?

If yes, please click on "Accept as Solution" at the bottom right corner of the answer which helps you.

You can also thank the members who tried to help you by liking their comments!

 

Have a nice day.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.