Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84695members
354073posts

Modify Meter Framework with ION Setup

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Gavin_Bryson
Commander | EcoXpert Master Commander | EcoXpert Master
Commander | EcoXpert Master
0 Likes
4
840

Modify Meter Framework with ION Setup

Hi,

 

Is it possible to modify a specific aspect of a meter framework using ION setup and then apply that change to the meter without wiping the meter configuration?

 

Or can this only be done with Designer?

 

Many thanks,

 

Gavin

Tags (1)

Accepted Solutions
Charles_Murison
Picard Picard
Picard
0 Likes
2
835

Re: Modify Meter Framework with ION Setup

Hello @Gavin_Bryson ,

 

Is it possible to configure specific aspects of a framework using ION Setup - Yes, Advanced configuration.

Is it possible to save just a small section of a framework (framelet) in ION Setup - No.

It is possible to have a framelet from Designer and use ION Setup to paste onto meter - Yes. The framelet is considered a lock paste, existing modules on the will be overwritten from framelet.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Tags (1)
4 Replies 4
Tom_Stevenson
Picard Picard
Picard
0 Likes
0
837

Re: Modify Meter Framework with ION Setup

I believe only Designer - @Rob to confirm if there are any exceptions.

Tags (1)
Charles_Murison
Picard Picard
Picard
0 Likes
2
836

Re: Modify Meter Framework with ION Setup

Hello @Gavin_Bryson ,

 

Is it possible to configure specific aspects of a framework using ION Setup - Yes, Advanced configuration.

Is it possible to save just a small section of a framework (framelet) in ION Setup - No.

It is possible to have a framelet from Designer and use ION Setup to paste onto meter - Yes. The framelet is considered a lock paste, existing modules on the will be overwritten from framelet.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
Tom_Stevenson
Picard Picard
Picard
0 Likes
0
832

Re: Modify Meter Framework with ION Setup

Thanks Charles !

Tags (1)
Gavin_Bryson
Commander | EcoXpert Master Commander | EcoXpert Master
Commander | EcoXpert Master
0 Likes
0
820

Re: Modify Meter Framework with ION Setup

Thanks @Charles_Murison 

Tags (1)