Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84796members
354246posts

Memory PM5560

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
SESA_B
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
3
1148

Memory PM5560

Hi team,

 

My customer using PM5560 for tariff. Now, they just only logging Energy (kWh del). So, with memory 1.1Mb of PM5560.

 

I want know, when will Memory PM5560 full? 1 week, two week, or 1 month? Any document for calculator this logging in memory?

 

Thanks very much.

 

 

Tags (1)

Accepted Solutions
Ramasamy_N
Commander Commander
Commander
1
1137

Re: Memory PM5560

Hello @SESA_B 

 

The size of one data log record will be 20 bytes approximately for one energy parameter (INT64 data format). So the PM5560 can record the maximum of 60000 records when only 2 energy parameters are enabled (maximum 14 parameters can be enabled). This configuration can store the data records for about 21 months when the time interval selected for 15 minutes. 

 

Please refer the attached excel sheet of data log calculator for more information. 

 

Regards, 

Ramasamy N

See Answer In Context

Attachments
Tags (1)
3 Replies 3
Charles_Murison
Picard Picard
Picard
0 Likes
0
1140

Re: Memory PM5560

@Ramasamy_N any thoughts?

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
Ramasamy_N
Commander Commander
Commander
1
1138

Re: Memory PM5560

Hello @SESA_B 

 

The size of one data log record will be 20 bytes approximately for one energy parameter (INT64 data format). So the PM5560 can record the maximum of 60000 records when only 2 energy parameters are enabled (maximum 14 parameters can be enabled). This configuration can store the data records for about 21 months when the time interval selected for 15 minutes. 

 

Please refer the attached excel sheet of data log calculator for more information. 

 

Regards, 

Ramasamy N

Attachments
Tags (1)
SESA_B
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
1130

Re: Memory PM5560

Hi @Charles_Murison , @Ramasamy_N ,

 

Thanks for your information. hihi

 

Tags (1)