Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7400 historical data management

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION7400 historical data management
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
RicardoMiranda
RicardoMiranda
Contributor

Posted: ‎2025-08-13 09:12 AM

0 Likes
3
1401
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
‎2025-08-13 09:12 AM

ION7400 historical data management

Hello everyone, nice to meet you.

From Chile, I have the following question regarding the management of the historical data stored by the ION7400 analyzer. Is it possible to manage this historical information and calculate the maximum value of any recorded variable for the month between specific times? This variable must be reset each month.

 

For example, bring the maximum variable (Current) for the month, which occurred between 10:00 and 11:00.

 

I understand that the meter can be programmed with the ION Setup tool, but I don't know if it has these programming capabilities, as it is a very specific task.

 

Thank you very much.

Labels
  • Labels:
  • ION Setup
  • ION7000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
RobGraham
RobGraham Champion
Champion

Posted: ‎2025-08-13 11:47 AM

1 Like
0
1390
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
‎2025-08-13 11:47 AM

The ION meter doesn't have any meaningful access to its own logged data.  That said, I can picture an ION framework using a Time of Use Module to enable a Maximum Module to store the maximum value during that period, then reset every month using the Clock module.

 

This is a rather advanced task requiring the use of Advanced ION Setup mode (or, better, PME's Designer application).  I recommend you familiarize yourself with that as well as the modules in the ION Reference before attempting this on a production meter.

See Answer In Context

Reply
Replies 3
RobGraham
RobGraham Champion
Champion

Posted: ‎2025-08-13 11:47 AM

1 Like
0
1390
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
‎2025-08-13 11:47 AM

The ION meter doesn't have any meaningful access to its own logged data.  That said, I can picture an ION framework using a Time of Use Module to enable a Maximum Module to store the maximum value during that period, then reset every month using the Clock module.

 

This is a rather advanced task requiring the use of Advanced ION Setup mode (or, better, PME's Designer application).  I recommend you familiarize yourself with that as well as the modules in the ION Reference before attempting this on a production meter.

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-08-13 12:57 PM

1 Like
0
1389
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
‎2025-08-13 12:57 PM

Hi @RicardoMiranda 

 

You can also refer to the following existing topic in the Exchange Community on a similar subject, I hope it helps:

how to find the maximum current draw in a month in PM8000

 

As for retrieving the maximum value of a variable (Current) for the month, specifically between 10:00 and 11:00, other modules such as Time Of Use or Arithmetic Modules are needed to configure frameworks that measure for example the demand values for that specific time periods.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Yut
Yut
Leader

Posted: ‎2025-08-18 01:55 AM

1 Like
0
1332
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
‎2025-08-18 01:55 AM

Get into the ION Reference study the Scheduler Module, Maximum module.

You may use ION Setup Advance mode or Designer, for me I prefer Designer.

The TOU can be use but it might interfere the TOU setting. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.