Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
how to check maximum current drawn in a month in PM 8000 pmu meter ??
Link copied. Please paste this link to share this article on your social media post.
Hello @hariqatar80 ,
The answer depends if you are trying to setup the meter to collect this information or if you have a meter already in the field and you are trying to determine this information from the collected data.
If new setup, you can use a maximum module, data recorder and feedback module. The maximum module would be linked to the measurement desired, a maximum module can only have 1 input so if you need for each phase you will need 3 maximum modules. The data recorder would have the maximum module's output as a source and the clock module's new month pulse as the record input. Link the record complete pulse output from data recorder to input of the feedback module. The output of the feedback module would link to reset input of the maximum module.
At the start of each month, the data recorder would record the maximum value for the month, then reset the maximum module. The feedback module is required to prevent logical looping inside the meter between data recorder and maximum module.
If you already have a meter in the field and has a moth of data collected, you can look at the HIST log log in ION setup to see the last 35ish days. This logs the maximum current every 15 minutes. You can take the maximum of the individual intervals to get the maximum for the 35 days.
If you are using software like PME to collect the logs you could look into the database to go back further is time than last 35 days.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @hariqatar80 ,
The answer depends if you are trying to setup the meter to collect this information or if you have a meter already in the field and you are trying to determine this information from the collected data.
If new setup, you can use a maximum module, data recorder and feedback module. The maximum module would be linked to the measurement desired, a maximum module can only have 1 input so if you need for each phase you will need 3 maximum modules. The data recorder would have the maximum module's output as a source and the clock module's new month pulse as the record input. Link the record complete pulse output from data recorder to input of the feedback module. The output of the feedback module would link to reset input of the maximum module.
At the start of each month, the data recorder would record the maximum value for the month, then reset the maximum module. The feedback module is required to prevent logical looping inside the meter between data recorder and maximum module.
If you already have a meter in the field and has a moth of data collected, you can look at the HIST log log in ION setup to see the last 35ish days. This logs the maximum current every 15 minutes. You can take the maximum of the individual intervals to get the maximum for the 35 days.
If you are using software like PME to collect the logs you could look into the database to go back further is time than last 35 days.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.