Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8240 using optical port for daisy chain

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PM8240 using optical port for daisy chain
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
RWG924
RWG924 Explorer
Explorer

Posted: ‎2025-08-12 02:22 AM . Last Modified: ‎2025-08-12 02:22 AM

0 Likes
1
691
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
‎2025-08-12 02:22 AM

PM8240 using optical port for daisy chain

When using PM8240 with Optical port , what is the architecture to daisy chain PM8240 at muliple locations?

Can we just link up the meter without using optical ethernet converters?

 

 

Labels
  • Labels:
  • ION8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-08-12 09:07 AM

1 Like
0
677
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
‎2025-08-12 09:07 AM

Hi @RWG924 

 

If I'm not mistaken, you're referring to fiber optic SC-duplex connectivity, which is converted from the meter's onboard Ethernet port:

Mehran_Mehrnia_0-1755009954183.png

 

The optical port located on the front panel of the meter—used primarily for local communication or configuration—is not supported by the PM8000 series. Only the ION7400 and ION9000 meters include an optical port.

 

PM8240 supports dual Ethernet ports for daisy-chaining and redundancy which is not practical for multiple locations are far apart(more than 100 meters), however, linking the meters using fiber—capable of spanning up to 2000 meters— requires industrial fiber switches or media converters that support daisy-chaining or ring topology.

For example:
[PM8240 + Fiber Module] <--fiber--> [Managed Switch] <--fiber--> [PM8240 + Fiber Module] <--fiber--> [Managed Switch] ...

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Reply 1
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-08-12 09:07 AM

1 Like
0
678
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
‎2025-08-12 09:07 AM

Hi @RWG924 

 

If I'm not mistaken, you're referring to fiber optic SC-duplex connectivity, which is converted from the meter's onboard Ethernet port:

Mehran_Mehrnia_0-1755009954183.png

 

The optical port located on the front panel of the meter—used primarily for local communication or configuration—is not supported by the PM8000 series. Only the ION7400 and ION9000 meters include an optical port.

 

PM8240 supports dual Ethernet ports for daisy-chaining and redundancy which is not practical for multiple locations are far apart(more than 100 meters), however, linking the meters using fiber—capable of spanning up to 2000 meters— requires industrial fiber switches or media converters that support daisy-chaining or ring topology.

For example:
[PM8240 + Fiber Module] <--fiber--> [Managed Switch] <--fiber--> [PM8240 + Fiber Module] <--fiber--> [Managed Switch] ...

 

Best Regards,

-Mehran

L3 Expert Advanced metering
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.