Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2015-05-0409:22 AM
ION 7550 Readings
After installing an ION 7550 meter i have differnt reading on the PF parameter.
one phase of the meter is giving out a low power factor which is affecting the KILOWATT output from this phase and as well the total kilowatt output of the meter in general.
See attached the screen shots of the reading on the meter.
What could have caused this disparity in the readings. I have checked the installation and seems all is fine.