Posted: 2020-07-03 11:25 PM . Last Modified: 2024-04-05 04:56 AM
SxOnGW1.1.0.43 and early: default file transfer settings do not apply?
Hi all!
I found another bug in SxOn GW 1.1.0.43, which moved from earlier versions of SxOn GW: default file transfer settings do not apply. I.e., in SxOn GW I configured Device File Transfer Settings like this (the password is not visible, but it's entered there):
After applying these settings, I still see unauthorized FTP access attempts every day in the logs of my devices.
If you disable these Default Device Settings and create your own settings, then the problem disappears and errors in the device logs no longer occur.
Very thanks for the support.
(CID:125208534)
- Labels:
-
Asset Advisor
-
IT Expert
- Tags:
- bug
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
Posted: 2020-07-03 11:25 PM . Last Modified: 2024-04-05 04:56 AM
Hi all!
From What is new in EcoStruxure IT:
StruxureOn Gateway 1.1.2.25
- The console log no longer displays an error when the Symmetra PX250 is polled.
- The password now updates as expected after the default or a user created file transfer configuration is modified.
- The service log posted by Symmetra PX250 now shows data as expected.
- Samsung BMS and Uniflair CRACs are now supported.
I can confirm, that the above problem is already fixed in the new version of SxOn GW 1.1.2.25.
Very thanks for the support 😀.
(CID:126175351)
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
Posted: 2020-07-03 11:25 PM . Last Modified: 2024-04-05 04:56 AM
Thanks for sharing 😀
(CID:125212614)
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
Posted: 2020-07-03 11:25 PM . Last Modified: 2024-04-05 04:56 AM
Hi Ditte Drewer Mathiasen,
Unfortunately, this bug is also present in the current version of SxOn GW 1.1.1.16. This is not good...
Very thanks for the support.
(CID:125212728)
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
Posted: 2020-07-03 11:25 PM . Last Modified: 2024-04-05 04:56 AM
Hi all!
From What is new in EcoStruxure IT:
StruxureOn Gateway 1.1.2.25
- The console log no longer displays an error when the Symmetra PX250 is polled.
- The password now updates as expected after the default or a user created file transfer configuration is modified.
- The service log posted by Symmetra PX250 now shows data as expected.
- Samsung BMS and Uniflair CRACs are now supported.
I can confirm, that the above problem is already fixed in the new version of SxOn GW 1.1.2.25.
Very thanks for the support 😀.
(CID:126175351)
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
Posted: 2020-07-03 11:25 PM . Last Modified: 2023-10-22 04:04 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.