Posted: 2020-07-04 08:17 PM . Last Modified: 2024-04-04 04:15 AM
Netbotz - Disable SMS but still receive e-mails
Good day
Please assist
We need to disable SMS notifications but e-mail notification need to be enabled.
Background - I have a netbotz 450 monitoring various access, exit and emergency doors via dry contacts. I am receiving sms and e-mails as soon as these doors open and close which is brilliant. I have edited the Default Alert Profile which enables SMS and e-mail notification.
Given the amount of traffic of the entrance doors, i now need to disable the sms but still want to receive e-mails for these doors.
Is there any way to disable the sms functionality without creating another alert profile for a few selected doors ?
Thanking you in Advance
Gamie.
(CID:132665526)
- Labels:
-
NetBotz
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
Posted: 2020-07-04 08:17 PM . Last Modified: 2024-04-04 04:15 AM
Dear gamie,
If you want to do this for all your doors, then in APC Advanced View go to Alert Profile -> select Default profile -> Edit... -> in tab Alert Sequences select the required alert -> Edit... -> in field Actions leave only E-mail Notifications.
If you want to do this only for some of your doors (not for all), then you will need to create a separate Alert Profile and configure it properly with the necessary Alert Action.
I hope this helps you.
With respect.
(CID:132665543)
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
Posted: 2020-07-04 08:17 PM . Last Modified: 2024-04-04 04:15 AM
Dear Gamie,
i am also interested to know if you found an alternative solution.
Thanks
(CID:132666068)
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
Posted: 2020-07-04 08:17 PM . Last Modified: 2024-04-04 04:15 AM
Dear gamie,
Tell us, please, did you solve your question or not?
With respect.
(CID:132670098)
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
Posted: 2020-07-04 08:18 PM . Last Modified: 2023-10-22 03:22 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.